Mixing Electronics & Water
  • Challenges & Projects
  • Project14
  • Mixing Electronics & Water
  • More
  • Cancel
Mixing Electronics & Water
Blog (Semi)Automated Plant Irrigation System
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Mixing Electronics & Water to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: urkraft
  • Date Created: 1 Feb 2018 9:50 PM Date Created
  • Views 10045 views
  • Likes 17 likes
  • Comments 81 comments
  • ardintermediate
  • arduino_projects
  • conservation_projects
  • mixewaterch
  • openarduinoch
Related
Recommended

(Semi)Automated Plant Irrigation System

urkraft
urkraft
1 Feb 2018

Semi-automated Plant Irrigation System

Summary

This is an automated system for watering my olive tree.

 

The main components are:

  • A soil moisture sensor
  • A 10 gallon bucket of water with a water level sensor
  • An Adafruit Feather HUZZAH ESP8266 microcontroller (hereafter referred to as “feather”)
  • A peristaltic water pump

 

The two sensors are connected to inputs of the feather, and the water pump is controlled by an output signal from the feather. There are two built in LED’s on the feather:

  • Red: used to indicate that the soil is dry enough to warrant watering
  • Blue: Used to indicate that the bucket is empty (requires a refill of water)

 

There are three criteria which all have to be met in order to turn on the pump (and water the plant):

  1. There must be water in the bucket
  2. The lack of moisture in the soil must be greater than a specified threshold value
  3. A specified minimum amount of time must have elapsed since the pump was last turned off while watering.

 

Any one of the following criteria will cause the pump to be turned off:

  • No water left in the bucket
  • The moisture level of the soil is higher than a specified threshold value (this criteria also triggers starting of the timer which keeps track of the amount of time that has elapsed since the pump was turned off).

 

Basically, the feather just goes in a loop checking the criteria above and taking the necessary action. Each loop iteration takes approximately 20-30 seconds to complete.

 

A feature that I would also like to implement is to have the system send me a message whenever it detects that the water bucket is empty (and possibly send a new reminder each day for a week before giving up). Unfortunately I have not found any official libraries with SMTP capabilities that I can use to accomplish this, so I do not know when or if I will be able to accomplish this goal.

 

I have tested the system quite a bit while implementing it (during the last 2 days) and feel confident that I have found and fixed all of the problems I have encountered along the way, but experience has taught me that the test of time is a very important test – and that test has only just begun.

 

Parts used

  • 1 Adafruit Feather HUZZAH ESP8266 (https://learn.adafruit.com/adafruit-feather-huzzah-esp8266/overview)
  • 1 5v 2.1A DC power supply w/micro usb contact (for the HUZZAH)
  • 1 12v 1A DC power supply (https://www.kjell.com/no/produkter/elektro-og-verktoy/stromforsyning/stromforsyning/ac-dc/fast-utgangsspenning/ac-dc-stromadapter-12-v-(dc)-12-w-p44382)
  • 1 power jack for the 12v power supply
  • 1 soil moisture sensor (https://www.kjell.com/no/produkter/elektro-og-verktoy/arduino/moduler/luxorparts-jordfuktmaler-p87941)
  • 1 water level switch NC (https://www.kjell.com/no/produkter/elektro-og-verktoy/elektronikk/electromechanics/strombrytere/nivabrytere/nivastrombryter-nc-p36037)
  • 1 22k ohm 1/8w resistor
  • 2 10k 1/8w resistor
  • 1 33 ohm 1/4w resistor
  • 2 1N4001 diodes
  • 1 Peristaltic Pump (https://www.kjell.com/no/produkter/elektro-og-verktoy/elektronikk/electromechanics/motorer/luxorparts-vaeskepumpe-peristaltisk-p90782)
  • 1 VR05R241A single pole DIL relay (https://www.kjell.com/no/produkter/elektro-og-verktoy/elektronikk/electromechanics/releer/1-polet-dil-rele-5-v-dc-0-5-a-30-v-p36110)
  • 1 Breadboard
  • Assorted jumper wires

 

Schematic Drawing

image

Breadboard

image

Code

#include 

//==========
// CONSTANTS
//==========

// wifi
const char* MY_SSID     = "";
const char* PASSWORD = "";

// I/O
const int LED = 0;  // (Output) indicates pump status (pump ON => LOW signal => lit)
const int PUMP = 4; // (Output) turns water pump on (set LOW) and off (set HIGH)
const int WATER_EMPTY_LED = 2;  // (Output) indicates water reservoir status 
                                // (empty => LOW signal => lit)
const int WATER_LEVEL = 14;  // (Input) to detect water in reservoir (water => HIGH)

// A0 : ADC (Analog Input) used to read soil humidity: high value => dry, low value => wet 
// Max value is approx. 825 - bone dry
// Min value is approx. 470 - drowning in water
const int PUMP_ON_THRESHOLD = 700;  // ADC input value >= this value => Turn on water pump
const int PUMP_OFF_THRESHOLD = 650; // ADC input value <= this value => Turn off water pump
                                    // (and do not turn on again for at least a day)
const long MINIMUM_TIME = 1000 * 60 * 60 * 24; // minimum time between watering (1 day)

//==========
// VARIABLES
//==========

// timing
unsigned long previousMillis = 0;
unsigned long currentMillis = 0;

// soil moisture reading
int moisture = 800; // previous 
int tmpMoisture = 0;  //  new (temporary)

//======
// SETUP
//======

void setup() {
  // initialize Serial
  Serial.begin(115200);
  delay(100);

  Serial.println();
  Serial.println();
  Serial.print("Connecting to ");
  Serial.println(MY_SSID);

  // initialize info
  WiFi.begin(MY_SSID, PASSWORD);
  WiFi.config(IPAddress(192, 168, 33, 95), IPAddress(192, 168, 33, 1), IPAddress(192, 168, 33, 1));
  
  while (WiFi.status() != WL_CONNECTED) {
    delay(500);
    Serial.print(".");
  }

  Serial.println("");
  Serial.println("WiFi connected");  
  Serial.println("IP address: ");
  Serial.println(WiFi.localIP());

  Serial.println();
  Serial.println();

  Serial.println("Soil moisture sensor");

  // initialize IO
  pinMode(WATER_LEVEL, INPUT);
  pinMode(PUMP, OUTPUT);
  digitalWrite(PUMP, HIGH);
  pinMode(LED, OUTPUT);
  digitalWrite(LED, HIGH);
  pinMode(WATER_EMPTY_LED, OUTPUT);
  digitalWrite(WATER_EMPTY_LED, HIGH);
  delay(2000); // give soil moisture sensor a chance to stabilize
}

void loop() {
  
  // check water reservoir
  while (digitalRead(WATER_LEVEL) == LOW) {  // water reservoir is empty 
    digitalWrite(WATER_EMPTY_LED, LOW);  // turn on the WATER_EMPTY_LED
    digitalWrite(PUMP, HIGH);  // make sure the water pump is turned off
    Serial.println("No water in reservoir => fill it up!");
    soil_moisture(false); // get soil moisture reading and update the soil moisture indicator LED
    // future code to send message at appropriate intervals goes here ...
    delay(10000); // allow moisture sensor to stabilize before next reading
  }
  digitalWrite(WATER_EMPTY_LED, HIGH); // The reservoir has water => turn off the WATER_EMPTY_LED
  soil_moisture(true);  // get the soil moisture reading and do appropriate actions
  delay(10000); // make sure that the moisture sensor gets time to stabilize before next reading
}


void soil_moisture(bool waterAvailable) {
  tmpMoisture = analogRead(A0); // take a soil moisture reading
  if (tmpMoisture != moisture) {  
    // only do the following if the moisture level has changed
    moisture = tmpMoisture;
    // print the moisture data to the serial interface ...
    Serial.print("moisture = ");
    Serial.println(moisture);
    if (moisture >= PUMP_ON_THRESHOLD) { // soil is dry enough for watering ...
      digitalWrite(LED, LOW); // turn on the indicator LED ...
      Serial.print("Dry threshold reached - ");
      if (waterAvailable) { // water is in the reservoir => OK to continue ...
        Serial.print("and water is available - ");
        currentMillis = millis();
        if ((previousMillis == 0) or (currentMillis - previousMillis >= MINIMUM_TIME)) {
          // the appropriate amount of time has transpired since the last watering => OK to water
          digitalWrite(PUMP, LOW);  // turn on pump
          Serial.println("water the plant!");
        } else {
          // not enough time has transpired since last watering => need to wait before watering
          Serial.println("but wait a bit longer.");
        }
      } else {
        // water reservoir is empty ...
        Serial.println("but the water reservoir is empty - fill it up!");
      }
    } else if (moisture <= PUMP_OFF_THRESHOLD) {
        // soil is moist enough ...
        digitalWrite(LED, HIGH);  // turn off the indicator LED
        digitalWrite(PUMP, HIGH); // make sure the water pump is off
        // update previousMillis. Want to wait at least MINIMUM_TIME before next watering
        previousMillis = millis();
        Serial.println("The soil moisture level is high - turning off the water pump.");
    } else {
      // moisture level between thresholds - no action necessary
      Serial.println("The soil moisture level is adequate - no action is being taken.");
    }
  }
}

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • urkraft
    urkraft over 8 years ago +7
    Status update: Here is a picture of the latest breadboard configuration (although i would be amazed if it would be helpful to anyone as it looks like a rats nest). It is now connected to all the sensors…
  • ntewinkel
    ntewinkel over 8 years ago in reply to urkraft +5
    Thanks Raymond! Hey I just found a case - it fits inside a TicTac container! -Nico
  • ntewinkel
    ntewinkel over 8 years ago in reply to urkraft +5
    What if you replaced the corroded prongs with copper (or copper plated) nails ($5 for a bag here at Home Depot)? Or you could probably use a few cutoff bits of copper house wiring (likely free even at…
Parents
  • urkraft
    urkraft over 8 years ago

    Status:

    I have just finished a new revision of my code in preparation for implement messaging using the ESP-01. The next steps are as follows:

     

    1. Upload the new sketch for the ESP-01. (Status: Done)
    2. Make a schematic of the changes that need to be made in order to integrate the ESP-01 into the existing design. (Done)
    3. Power down the irrigation system presently being used to water my olive tree. (Done)
    4. Connect the ESP-01 and necessary circuitry to the existing design (as per step 2). (Done)
    5. Upload the new sketch for the Uno. (Done)
    6. Test that everything appears to be functioning as it should. (Done)
    7. Install the new system at the olive tree. (Done)
    8. Test that everything appears to be functioning as it should. (Done)
    9. Document my work. (Done)
    10. Publish. (Done)

     

    -raymond

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 8 years ago in reply to urkraft

    Hi Raymond,

    After steps 9 and 10, you might want to enter your project into the newest Project14 contest: Mixing Electronics & Water

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 8 years ago in reply to urkraft

    >I believe that project cost would be much lower using a Sonoff device instead of en ESP-01.

     

    I think you might be right. For some reason I assumed these units would be much more expensive, but at $5.50 US it's only about $1.50 more than a Witty or Wemos! And as you say, that includes the enclosure and power supply and a bonus relay, a much better deal overall.

    I also wasn't aware of the 2 GPIO pins, I thought it was just a remote switch.

     

    I've gone ahead and bought one image  If my wife asks, I'll blame you image

     

    -Nico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • urkraft
    urkraft over 8 years ago in reply to ntewinkel

    image Funny, Nico! But really - check out that video in the link i posted. It is a long one, but he gives a lot of interesting tips and info about the Sonoff devices and what can be done with them. I am sure you will enjoy the video.

     

    Regards,

    -raymond

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • urkraft
    urkraft over 8 years ago in reply to ntewinkel

    Hello Nico,

    Please keep me updated about your experience with the Sonoff device. I am interested in finding out more about them, but need to wait until my economical situation changes before i can make any further expenditures of this type.

    -raymond

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 8 years ago in reply to urkraft

    Hi Raymond!

    Funny you happened to message today, as just a half hour ago I finally finished watching the video you recommended!

    He gives some really good advice. I also learned that the cheaper Sonoff I bought (I think) only has one GPIO available (+1 that's already in use for the relay), but that's probably fine for my uses.

     

    My Sonoff is coming from China, so I don't expect it'll be here before the end of the month. I think it may have also been delayed by Chinese New Year. I'm also still waiting for the WeMos and Witty.

     

    The ESP-01 data logging is going really well though. Here's the live graph: http://mulberryland.com/sensors/sensorgraph.html

    It's giving me lots of insight on how my temperature switch works in real life. (the spike is when I was changing things). Outside temperature is dropping to about 3C at night, up to about 7C in the day, so I know the heater is working.

     

    And I know what you mean about project expenditures - for me it has generally been that I either had the time or the money for these projects, but rarely both at the same time image

    Hope you find a really excellent job soon. What is it you do for a living?

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • urkraft
    urkraft over 8 years ago in reply to ntewinkel

    Hello again Nico,

     

    This system can be VERY frustrating. Just spent a long time writing a reply to you only to loose it all when i attempted to upload a picture of a graph of my own. I have lost my work here quite often and it is frustrating every time.

    Thank you for your response. Sorry for not being specific enough about the Sonoff devices - in particular about pointing out that not all of them have that extra IO pin available. Anyway, i hope that the one you ordered is good enough for your requirements.

    Here is a graph of the temperature and air pollution in my bedroom the past 24 hours:

    image

    I use a couple of my Raspberry Pi's to record temperature, humidity, and air pollution levels in my bedroom and living room. I made this system about 4 years ago when my circumstances changed radically resulting in me having to reduce expenses - also with regards to rent. The result is that i can only afford to live in places densely populated by heavy smokers. Being forced to become a heavy passive smoker i naively tried to document my situation for the health authorities hoping to find some way of escaping it. But it turns out that (at least in Norway) smokers "right" to smoke in their home is incontestable and outweighs their neighbors need for fresh air. The "solution" recommended for me is to move. After 3 failed attempts at this "solutions" i no longer have the resources to make any further attempts of escape. You can see from my graph when my neighbors are at home - the pollution levels increase dramatically.

     

    I really do wish that it was possible for me to get a job which would enable me to at least search for solutions, but i do not believe there is any chance of that. I have lived in Norway for over 30 years and have always had great difficulties finding work. It was a bit easier to get by when i was younger and was able to compete for jobs that Norwegians were not interested in, but i am 62 years old now. Of the more than 250 jobs that i have applied for there was only one of them that did not require me to state my date of birth.

     

    Anyway, everything has an end in some way or another - also this. So i just have to focus on one day at a time and on the things that give me strength.

     

    -raymond

    ludo ergo sum

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • urkraft
    urkraft over 8 years ago in reply to ntewinkel

    Hello again Nico,

     

    This system can be VERY frustrating. Just spent a long time writing a reply to you only to loose it all when i attempted to upload a picture of a graph of my own. I have lost my work here quite often and it is frustrating every time.

    Thank you for your response. Sorry for not being specific enough about the Sonoff devices - in particular about pointing out that not all of them have that extra IO pin available. Anyway, i hope that the one you ordered is good enough for your requirements.

    Here is a graph of the temperature and air pollution in my bedroom the past 24 hours:

    image

    I use a couple of my Raspberry Pi's to record temperature, humidity, and air pollution levels in my bedroom and living room. I made this system about 4 years ago when my circumstances changed radically resulting in me having to reduce expenses - also with regards to rent. The result is that i can only afford to live in places densely populated by heavy smokers. Being forced to become a heavy passive smoker i naively tried to document my situation for the health authorities hoping to find some way of escaping it. But it turns out that (at least in Norway) smokers "right" to smoke in their home is incontestable and outweighs their neighbors need for fresh air. The "solution" recommended for me is to move. After 3 failed attempts at this "solutions" i no longer have the resources to make any further attempts of escape. You can see from my graph when my neighbors are at home - the pollution levels increase dramatically.

     

    I really do wish that it was possible for me to get a job which would enable me to at least search for solutions, but i do not believe there is any chance of that. I have lived in Norway for over 30 years and have always had great difficulties finding work. It was a bit easier to get by when i was younger and was able to compete for jobs that Norwegians were not interested in, but i am 62 years old now. Of the more than 250 jobs that i have applied for there was only one of them that did not require me to state my date of birth.

     

    Anyway, everything has an end in some way or another - also this. So i just have to focus on one day at a time and on the things that give me strength.

     

    -raymond

    ludo ergo sum