Mixing Electronics & Water
  • Challenges & Projects
  • Project14
  • Mixing Electronics & Water
  • More
  • Cancel
Mixing Electronics & Water
Blog (Semi)Automated Plant Irrigation System
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Mixing Electronics & Water to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: urkraft
  • Date Created: 1 Feb 2018 9:50 PM Date Created
  • Views 10087 views
  • Likes 17 likes
  • Comments 81 comments
  • ardintermediate
  • arduino_projects
  • conservation_projects
  • mixewaterch
  • openarduinoch
Related
Recommended

(Semi)Automated Plant Irrigation System

urkraft
urkraft
1 Feb 2018

Semi-automated Plant Irrigation System

Summary

This is an automated system for watering my olive tree.

 

The main components are:

  • A soil moisture sensor
  • A 10 gallon bucket of water with a water level sensor
  • An Adafruit Feather HUZZAH ESP8266 microcontroller (hereafter referred to as “feather”)
  • A peristaltic water pump

 

The two sensors are connected to inputs of the feather, and the water pump is controlled by an output signal from the feather. There are two built in LED’s on the feather:

  • Red: used to indicate that the soil is dry enough to warrant watering
  • Blue: Used to indicate that the bucket is empty (requires a refill of water)

 

There are three criteria which all have to be met in order to turn on the pump (and water the plant):

  1. There must be water in the bucket
  2. The lack of moisture in the soil must be greater than a specified threshold value
  3. A specified minimum amount of time must have elapsed since the pump was last turned off while watering.

 

Any one of the following criteria will cause the pump to be turned off:

  • No water left in the bucket
  • The moisture level of the soil is higher than a specified threshold value (this criteria also triggers starting of the timer which keeps track of the amount of time that has elapsed since the pump was turned off).

 

Basically, the feather just goes in a loop checking the criteria above and taking the necessary action. Each loop iteration takes approximately 20-30 seconds to complete.

 

A feature that I would also like to implement is to have the system send me a message whenever it detects that the water bucket is empty (and possibly send a new reminder each day for a week before giving up). Unfortunately I have not found any official libraries with SMTP capabilities that I can use to accomplish this, so I do not know when or if I will be able to accomplish this goal.

 

I have tested the system quite a bit while implementing it (during the last 2 days) and feel confident that I have found and fixed all of the problems I have encountered along the way, but experience has taught me that the test of time is a very important test – and that test has only just begun.

 

Parts used

  • 1 Adafruit Feather HUZZAH ESP8266 (https://learn.adafruit.com/adafruit-feather-huzzah-esp8266/overview)
  • 1 5v 2.1A DC power supply w/micro usb contact (for the HUZZAH)
  • 1 12v 1A DC power supply (https://www.kjell.com/no/produkter/elektro-og-verktoy/stromforsyning/stromforsyning/ac-dc/fast-utgangsspenning/ac-dc-stromadapter-12-v-(dc)-12-w-p44382)
  • 1 power jack for the 12v power supply
  • 1 soil moisture sensor (https://www.kjell.com/no/produkter/elektro-og-verktoy/arduino/moduler/luxorparts-jordfuktmaler-p87941)
  • 1 water level switch NC (https://www.kjell.com/no/produkter/elektro-og-verktoy/elektronikk/electromechanics/strombrytere/nivabrytere/nivastrombryter-nc-p36037)
  • 1 22k ohm 1/8w resistor
  • 2 10k 1/8w resistor
  • 1 33 ohm 1/4w resistor
  • 2 1N4001 diodes
  • 1 Peristaltic Pump (https://www.kjell.com/no/produkter/elektro-og-verktoy/elektronikk/electromechanics/motorer/luxorparts-vaeskepumpe-peristaltisk-p90782)
  • 1 VR05R241A single pole DIL relay (https://www.kjell.com/no/produkter/elektro-og-verktoy/elektronikk/electromechanics/releer/1-polet-dil-rele-5-v-dc-0-5-a-30-v-p36110)
  • 1 Breadboard
  • Assorted jumper wires

 

Schematic Drawing

image

Breadboard

image

Code

#include 

//==========
// CONSTANTS
//==========

// wifi
const char* MY_SSID     = "";
const char* PASSWORD = "";

// I/O
const int LED = 0;  // (Output) indicates pump status (pump ON => LOW signal => lit)
const int PUMP = 4; // (Output) turns water pump on (set LOW) and off (set HIGH)
const int WATER_EMPTY_LED = 2;  // (Output) indicates water reservoir status 
                                // (empty => LOW signal => lit)
const int WATER_LEVEL = 14;  // (Input) to detect water in reservoir (water => HIGH)

// A0 : ADC (Analog Input) used to read soil humidity: high value => dry, low value => wet 
// Max value is approx. 825 - bone dry
// Min value is approx. 470 - drowning in water
const int PUMP_ON_THRESHOLD = 700;  // ADC input value >= this value => Turn on water pump
const int PUMP_OFF_THRESHOLD = 650; // ADC input value <= this value => Turn off water pump
                                    // (and do not turn on again for at least a day)
const long MINIMUM_TIME = 1000 * 60 * 60 * 24; // minimum time between watering (1 day)

//==========
// VARIABLES
//==========

// timing
unsigned long previousMillis = 0;
unsigned long currentMillis = 0;

// soil moisture reading
int moisture = 800; // previous 
int tmpMoisture = 0;  //  new (temporary)

//======
// SETUP
//======

void setup() {
  // initialize Serial
  Serial.begin(115200);
  delay(100);

  Serial.println();
  Serial.println();
  Serial.print("Connecting to ");
  Serial.println(MY_SSID);

  // initialize info
  WiFi.begin(MY_SSID, PASSWORD);
  WiFi.config(IPAddress(192, 168, 33, 95), IPAddress(192, 168, 33, 1), IPAddress(192, 168, 33, 1));
  
  while (WiFi.status() != WL_CONNECTED) {
    delay(500);
    Serial.print(".");
  }

  Serial.println("");
  Serial.println("WiFi connected");  
  Serial.println("IP address: ");
  Serial.println(WiFi.localIP());

  Serial.println();
  Serial.println();

  Serial.println("Soil moisture sensor");

  // initialize IO
  pinMode(WATER_LEVEL, INPUT);
  pinMode(PUMP, OUTPUT);
  digitalWrite(PUMP, HIGH);
  pinMode(LED, OUTPUT);
  digitalWrite(LED, HIGH);
  pinMode(WATER_EMPTY_LED, OUTPUT);
  digitalWrite(WATER_EMPTY_LED, HIGH);
  delay(2000); // give soil moisture sensor a chance to stabilize
}

void loop() {
  
  // check water reservoir
  while (digitalRead(WATER_LEVEL) == LOW) {  // water reservoir is empty 
    digitalWrite(WATER_EMPTY_LED, LOW);  // turn on the WATER_EMPTY_LED
    digitalWrite(PUMP, HIGH);  // make sure the water pump is turned off
    Serial.println("No water in reservoir => fill it up!");
    soil_moisture(false); // get soil moisture reading and update the soil moisture indicator LED
    // future code to send message at appropriate intervals goes here ...
    delay(10000); // allow moisture sensor to stabilize before next reading
  }
  digitalWrite(WATER_EMPTY_LED, HIGH); // The reservoir has water => turn off the WATER_EMPTY_LED
  soil_moisture(true);  // get the soil moisture reading and do appropriate actions
  delay(10000); // make sure that the moisture sensor gets time to stabilize before next reading
}


void soil_moisture(bool waterAvailable) {
  tmpMoisture = analogRead(A0); // take a soil moisture reading
  if (tmpMoisture != moisture) {  
    // only do the following if the moisture level has changed
    moisture = tmpMoisture;
    // print the moisture data to the serial interface ...
    Serial.print("moisture = ");
    Serial.println(moisture);
    if (moisture >= PUMP_ON_THRESHOLD) { // soil is dry enough for watering ...
      digitalWrite(LED, LOW); // turn on the indicator LED ...
      Serial.print("Dry threshold reached - ");
      if (waterAvailable) { // water is in the reservoir => OK to continue ...
        Serial.print("and water is available - ");
        currentMillis = millis();
        if ((previousMillis == 0) or (currentMillis - previousMillis >= MINIMUM_TIME)) {
          // the appropriate amount of time has transpired since the last watering => OK to water
          digitalWrite(PUMP, LOW);  // turn on pump
          Serial.println("water the plant!");
        } else {
          // not enough time has transpired since last watering => need to wait before watering
          Serial.println("but wait a bit longer.");
        }
      } else {
        // water reservoir is empty ...
        Serial.println("but the water reservoir is empty - fill it up!");
      }
    } else if (moisture <= PUMP_OFF_THRESHOLD) {
        // soil is moist enough ...
        digitalWrite(LED, HIGH);  // turn off the indicator LED
        digitalWrite(PUMP, HIGH); // make sure the water pump is off
        // update previousMillis. Want to wait at least MINIMUM_TIME before next watering
        previousMillis = millis();
        Serial.println("The soil moisture level is high - turning off the water pump.");
    } else {
      // moisture level between thresholds - no action necessary
      Serial.println("The soil moisture level is adequate - no action is being taken.");
    }
  }
}

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • urkraft
    urkraft over 8 years ago +7
    Status update: Here is a picture of the latest breadboard configuration (although i would be amazed if it would be helpful to anyone as it looks like a rats nest). It is now connected to all the sensors…
  • ntewinkel
    ntewinkel over 8 years ago in reply to urkraft +5
    Thanks Raymond! Hey I just found a case - it fits inside a TicTac container! -Nico
  • ntewinkel
    ntewinkel over 8 years ago in reply to urkraft +5
    What if you replaced the corroded prongs with copper (or copper plated) nails ($5 for a bag here at Home Depot)? Or you could probably use a few cutoff bits of copper house wiring (likely free even at…
Parents
  • urkraft
    urkraft over 8 years ago

    Status:

    Been experimenting with solutions for messaging today. Really tired and sleep deprived now, so i have wasted lots of time because of trivial stupid mistakes (typos). I have been playing around with the Adafruit Feather HUZZAH ESP8266 again, but this time without any extra circuitry and only WiFi code. My idea was to use it to send a message to one of my raspi's and get it to send me an e-mail. I have a Python script on one of my raspi's that i use to take a picture and send it to me as an emails attachment if movement is detected via a PIR that is connected to it. It works quite well, but i could not find a way to trigger a Python script remotely automatically. Nico recently suggested using a PHP script to get it done, but i had never configured the mail server on any of my raspi's. After googling around a bit i found this link about configuring postfix to send mail using gmail. I had to struggle to get it to work because of a couple of typos that i managed to make along the way, but i finally got it to work! This is the PHP script that i have on the raspi:

     

    (/var/www/irrigation.php)

     

    <?php     //the formatting keeps either eliminating this line or the last line of the code - go figure!

         $msg = "The water reservoir is empty"";
         $to_email = "myEmail@myDomain.com";
         $subject = "Irrigation System Status";
         if (mail($to_email, $subject, $msg)) {
              echo "Done!";
         } else {
              echo "Failed!";
         }
    ?>

    I tested it by just entering the url for the raspi in a browser followed by the file name like so:

     

    http://192.198.1.12/irrigation.php

     

    and shortly after i received the e-mail.

     

    Next, i just modified the some Adafruit test code for the feather:

     

    /*
     *  Simple HTTP get webclient test
     */
    
    
    #include 
    
    
    const char* ssid     = "mySSID";
    const char* password = "myPassword";
    
    
    const char* host = "";
    
    
    void setup() {
      Serial.begin(115200);
      delay(100);
    
    
      // We start by connecting to a WiFi network
    
    
      Serial.println();
      Serial.println();
      Serial.print("Connecting to ");
      Serial.println(ssid);
      
      WiFi.begin(ssid, password);
      WiFi.config(IPAddress(192, 168, 1, 13), IPAddress(192, 168, 1, 1), IPAddress(192, 168, 1, 1));  // replace with yours
      
      while (WiFi.status() != WL_CONNECTED) {
        delay(500);
        Serial.print(".");
      }
    
    
      Serial.println("");
      Serial.println("WiFi connected");  
      Serial.println("IP address: ");
      Serial.println(WiFi.localIP());
      
      delay(5000);
    
    
      Serial.print("connecting to ");
      Serial.println(host);
      
      // Use WiFiClient class to create TCP connections
      WiFiClient client;
      const int httpPort = 80;
      if (!client.connect(host, httpPort)) {
        Serial.println("connection failed");
        return;
      }
      
      // We now create a URI for the request
      String url = "/irrigation.php";
      Serial.print("Requesting URL: ");
      Serial.println(url);
      
      // This will send the request to the server
      client.print(String("GET ") + url + " HTTP/1.1\r\n" +
                   "Host: " + host + "\r\n" + 
                   "Connection: close\r\n\r\n");
      delay(500);
      
      // Read all the lines of the reply from server and print them to Serial
      while(client.available()){
        String line = client.readStringUntil('\r');
        Serial.print(line);
      }
      
      Serial.println();
      Serial.println("closing connection");
      delay(50000);
    }
    
    
    
    
    void loop() {
    }

     

    The above code just does what i did manually to test the PHP script (after configuring the WiFi on the feather) - and it worked!

     

    I also made a trip into Oslo to buy a ESP8266, so the next step is to try to get that working with an UNO.

     

    -raymond

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • urkraft
    urkraft over 8 years ago

    Status:

    Been experimenting with solutions for messaging today. Really tired and sleep deprived now, so i have wasted lots of time because of trivial stupid mistakes (typos). I have been playing around with the Adafruit Feather HUZZAH ESP8266 again, but this time without any extra circuitry and only WiFi code. My idea was to use it to send a message to one of my raspi's and get it to send me an e-mail. I have a Python script on one of my raspi's that i use to take a picture and send it to me as an emails attachment if movement is detected via a PIR that is connected to it. It works quite well, but i could not find a way to trigger a Python script remotely automatically. Nico recently suggested using a PHP script to get it done, but i had never configured the mail server on any of my raspi's. After googling around a bit i found this link about configuring postfix to send mail using gmail. I had to struggle to get it to work because of a couple of typos that i managed to make along the way, but i finally got it to work! This is the PHP script that i have on the raspi:

     

    (/var/www/irrigation.php)

     

    <?php     //the formatting keeps either eliminating this line or the last line of the code - go figure!

         $msg = "The water reservoir is empty"";
         $to_email = "myEmail@myDomain.com";
         $subject = "Irrigation System Status";
         if (mail($to_email, $subject, $msg)) {
              echo "Done!";
         } else {
              echo "Failed!";
         }
    ?>

    I tested it by just entering the url for the raspi in a browser followed by the file name like so:

     

    http://192.198.1.12/irrigation.php

     

    and shortly after i received the e-mail.

     

    Next, i just modified the some Adafruit test code for the feather:

     

    /*
     *  Simple HTTP get webclient test
     */
    
    
    #include 
    
    
    const char* ssid     = "mySSID";
    const char* password = "myPassword";
    
    
    const char* host = "";
    
    
    void setup() {
      Serial.begin(115200);
      delay(100);
    
    
      // We start by connecting to a WiFi network
    
    
      Serial.println();
      Serial.println();
      Serial.print("Connecting to ");
      Serial.println(ssid);
      
      WiFi.begin(ssid, password);
      WiFi.config(IPAddress(192, 168, 1, 13), IPAddress(192, 168, 1, 1), IPAddress(192, 168, 1, 1));  // replace with yours
      
      while (WiFi.status() != WL_CONNECTED) {
        delay(500);
        Serial.print(".");
      }
    
    
      Serial.println("");
      Serial.println("WiFi connected");  
      Serial.println("IP address: ");
      Serial.println(WiFi.localIP());
      
      delay(5000);
    
    
      Serial.print("connecting to ");
      Serial.println(host);
      
      // Use WiFiClient class to create TCP connections
      WiFiClient client;
      const int httpPort = 80;
      if (!client.connect(host, httpPort)) {
        Serial.println("connection failed");
        return;
      }
      
      // We now create a URI for the request
      String url = "/irrigation.php";
      Serial.print("Requesting URL: ");
      Serial.println(url);
      
      // This will send the request to the server
      client.print(String("GET ") + url + " HTTP/1.1\r\n" +
                   "Host: " + host + "\r\n" + 
                   "Connection: close\r\n\r\n");
      delay(500);
      
      // Read all the lines of the reply from server and print them to Serial
      while(client.available()){
        String line = client.readStringUntil('\r');
        Serial.print(line);
      }
      
      Serial.println();
      Serial.println("closing connection");
      delay(50000);
    }
    
    
    
    
    void loop() {
    }

     

    The above code just does what i did manually to test the PHP script (after configuring the WiFi on the feather) - and it worked!

     

    I also made a trip into Oslo to buy a ESP8266, so the next step is to try to get that working with an UNO.

     

    -raymond