Mixing Electronics & Water
  • Challenges & Projects
  • Project14
  • Mixing Electronics & Water
  • More
  • Cancel
Mixing Electronics & Water
Blog (Semi)Automated Plant Irrigation System
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Mixing Electronics & Water to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: urkraft
  • Date Created: 1 Feb 2018 9:50 PM Date Created
  • Views 10065 views
  • Likes 17 likes
  • Comments 81 comments
  • ardintermediate
  • arduino_projects
  • conservation_projects
  • mixewaterch
  • openarduinoch
Related
Recommended

(Semi)Automated Plant Irrigation System

urkraft
urkraft
1 Feb 2018

Semi-automated Plant Irrigation System

Summary

This is an automated system for watering my olive tree.

 

The main components are:

  • A soil moisture sensor
  • A 10 gallon bucket of water with a water level sensor
  • An Adafruit Feather HUZZAH ESP8266 microcontroller (hereafter referred to as “feather”)
  • A peristaltic water pump

 

The two sensors are connected to inputs of the feather, and the water pump is controlled by an output signal from the feather. There are two built in LED’s on the feather:

  • Red: used to indicate that the soil is dry enough to warrant watering
  • Blue: Used to indicate that the bucket is empty (requires a refill of water)

 

There are three criteria which all have to be met in order to turn on the pump (and water the plant):

  1. There must be water in the bucket
  2. The lack of moisture in the soil must be greater than a specified threshold value
  3. A specified minimum amount of time must have elapsed since the pump was last turned off while watering.

 

Any one of the following criteria will cause the pump to be turned off:

  • No water left in the bucket
  • The moisture level of the soil is higher than a specified threshold value (this criteria also triggers starting of the timer which keeps track of the amount of time that has elapsed since the pump was turned off).

 

Basically, the feather just goes in a loop checking the criteria above and taking the necessary action. Each loop iteration takes approximately 20-30 seconds to complete.

 

A feature that I would also like to implement is to have the system send me a message whenever it detects that the water bucket is empty (and possibly send a new reminder each day for a week before giving up). Unfortunately I have not found any official libraries with SMTP capabilities that I can use to accomplish this, so I do not know when or if I will be able to accomplish this goal.

 

I have tested the system quite a bit while implementing it (during the last 2 days) and feel confident that I have found and fixed all of the problems I have encountered along the way, but experience has taught me that the test of time is a very important test – and that test has only just begun.

 

Parts used

  • 1 Adafruit Feather HUZZAH ESP8266 (https://learn.adafruit.com/adafruit-feather-huzzah-esp8266/overview)
  • 1 5v 2.1A DC power supply w/micro usb contact (for the HUZZAH)
  • 1 12v 1A DC power supply (https://www.kjell.com/no/produkter/elektro-og-verktoy/stromforsyning/stromforsyning/ac-dc/fast-utgangsspenning/ac-dc-stromadapter-12-v-(dc)-12-w-p44382)
  • 1 power jack for the 12v power supply
  • 1 soil moisture sensor (https://www.kjell.com/no/produkter/elektro-og-verktoy/arduino/moduler/luxorparts-jordfuktmaler-p87941)
  • 1 water level switch NC (https://www.kjell.com/no/produkter/elektro-og-verktoy/elektronikk/electromechanics/strombrytere/nivabrytere/nivastrombryter-nc-p36037)
  • 1 22k ohm 1/8w resistor
  • 2 10k 1/8w resistor
  • 1 33 ohm 1/4w resistor
  • 2 1N4001 diodes
  • 1 Peristaltic Pump (https://www.kjell.com/no/produkter/elektro-og-verktoy/elektronikk/electromechanics/motorer/luxorparts-vaeskepumpe-peristaltisk-p90782)
  • 1 VR05R241A single pole DIL relay (https://www.kjell.com/no/produkter/elektro-og-verktoy/elektronikk/electromechanics/releer/1-polet-dil-rele-5-v-dc-0-5-a-30-v-p36110)
  • 1 Breadboard
  • Assorted jumper wires

 

Schematic Drawing

image

Breadboard

image

Code

#include 

//==========
// CONSTANTS
//==========

// wifi
const char* MY_SSID     = "";
const char* PASSWORD = "";

// I/O
const int LED = 0;  // (Output) indicates pump status (pump ON => LOW signal => lit)
const int PUMP = 4; // (Output) turns water pump on (set LOW) and off (set HIGH)
const int WATER_EMPTY_LED = 2;  // (Output) indicates water reservoir status 
                                // (empty => LOW signal => lit)
const int WATER_LEVEL = 14;  // (Input) to detect water in reservoir (water => HIGH)

// A0 : ADC (Analog Input) used to read soil humidity: high value => dry, low value => wet 
// Max value is approx. 825 - bone dry
// Min value is approx. 470 - drowning in water
const int PUMP_ON_THRESHOLD = 700;  // ADC input value >= this value => Turn on water pump
const int PUMP_OFF_THRESHOLD = 650; // ADC input value <= this value => Turn off water pump
                                    // (and do not turn on again for at least a day)
const long MINIMUM_TIME = 1000 * 60 * 60 * 24; // minimum time between watering (1 day)

//==========
// VARIABLES
//==========

// timing
unsigned long previousMillis = 0;
unsigned long currentMillis = 0;

// soil moisture reading
int moisture = 800; // previous 
int tmpMoisture = 0;  //  new (temporary)

//======
// SETUP
//======

void setup() {
  // initialize Serial
  Serial.begin(115200);
  delay(100);

  Serial.println();
  Serial.println();
  Serial.print("Connecting to ");
  Serial.println(MY_SSID);

  // initialize info
  WiFi.begin(MY_SSID, PASSWORD);
  WiFi.config(IPAddress(192, 168, 33, 95), IPAddress(192, 168, 33, 1), IPAddress(192, 168, 33, 1));
  
  while (WiFi.status() != WL_CONNECTED) {
    delay(500);
    Serial.print(".");
  }

  Serial.println("");
  Serial.println("WiFi connected");  
  Serial.println("IP address: ");
  Serial.println(WiFi.localIP());

  Serial.println();
  Serial.println();

  Serial.println("Soil moisture sensor");

  // initialize IO
  pinMode(WATER_LEVEL, INPUT);
  pinMode(PUMP, OUTPUT);
  digitalWrite(PUMP, HIGH);
  pinMode(LED, OUTPUT);
  digitalWrite(LED, HIGH);
  pinMode(WATER_EMPTY_LED, OUTPUT);
  digitalWrite(WATER_EMPTY_LED, HIGH);
  delay(2000); // give soil moisture sensor a chance to stabilize
}

void loop() {
  
  // check water reservoir
  while (digitalRead(WATER_LEVEL) == LOW) {  // water reservoir is empty 
    digitalWrite(WATER_EMPTY_LED, LOW);  // turn on the WATER_EMPTY_LED
    digitalWrite(PUMP, HIGH);  // make sure the water pump is turned off
    Serial.println("No water in reservoir => fill it up!");
    soil_moisture(false); // get soil moisture reading and update the soil moisture indicator LED
    // future code to send message at appropriate intervals goes here ...
    delay(10000); // allow moisture sensor to stabilize before next reading
  }
  digitalWrite(WATER_EMPTY_LED, HIGH); // The reservoir has water => turn off the WATER_EMPTY_LED
  soil_moisture(true);  // get the soil moisture reading and do appropriate actions
  delay(10000); // make sure that the moisture sensor gets time to stabilize before next reading
}


void soil_moisture(bool waterAvailable) {
  tmpMoisture = analogRead(A0); // take a soil moisture reading
  if (tmpMoisture != moisture) {  
    // only do the following if the moisture level has changed
    moisture = tmpMoisture;
    // print the moisture data to the serial interface ...
    Serial.print("moisture = ");
    Serial.println(moisture);
    if (moisture >= PUMP_ON_THRESHOLD) { // soil is dry enough for watering ...
      digitalWrite(LED, LOW); // turn on the indicator LED ...
      Serial.print("Dry threshold reached - ");
      if (waterAvailable) { // water is in the reservoir => OK to continue ...
        Serial.print("and water is available - ");
        currentMillis = millis();
        if ((previousMillis == 0) or (currentMillis - previousMillis >= MINIMUM_TIME)) {
          // the appropriate amount of time has transpired since the last watering => OK to water
          digitalWrite(PUMP, LOW);  // turn on pump
          Serial.println("water the plant!");
        } else {
          // not enough time has transpired since last watering => need to wait before watering
          Serial.println("but wait a bit longer.");
        }
      } else {
        // water reservoir is empty ...
        Serial.println("but the water reservoir is empty - fill it up!");
      }
    } else if (moisture <= PUMP_OFF_THRESHOLD) {
        // soil is moist enough ...
        digitalWrite(LED, HIGH);  // turn off the indicator LED
        digitalWrite(PUMP, HIGH); // make sure the water pump is off
        // update previousMillis. Want to wait at least MINIMUM_TIME before next watering
        previousMillis = millis();
        Serial.println("The soil moisture level is high - turning off the water pump.");
    } else {
      // moisture level between thresholds - no action necessary
      Serial.println("The soil moisture level is adequate - no action is being taken.");
    }
  }
}

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • urkraft
    urkraft over 8 years ago +7
    Status update: Here is a picture of the latest breadboard configuration (although i would be amazed if it would be helpful to anyone as it looks like a rats nest). It is now connected to all the sensors…
  • ntewinkel
    ntewinkel over 8 years ago in reply to urkraft +5
    Thanks Raymond! Hey I just found a case - it fits inside a TicTac container! -Nico
  • ntewinkel
    ntewinkel over 8 years ago in reply to urkraft +5
    What if you replaced the corroded prongs with copper (or copper plated) nails ($5 for a bag here at Home Depot)? Or you could probably use a few cutoff bits of copper house wiring (likely free even at…
Parents
  • urkraft
    urkraft over 8 years ago

    Very strange, but i can get the Adafruit Feather HUZZAH ESP8266 to connect to my SSID (even though it is hidden), but no matter what i do i cannot get the ESP-01 to connect - not even to another WiFi that i have that broadcasts its SSID. I know that i have managed to upload the code successfully and that the code is actually running because i get the "uploading" message in the status area of the Arduino IDE as well as the dots indicating that uploading is in progress (and the blue light on the ESP-01 blinks while this is happening), followed by the "Done uploading" message without any error messages. My code also blinks the blue LED while it is in the loop where it trying to connect to the WiFi - and that is exactly where it is stuck. I have tried a variety of different code examples but have not been able to get anything to work so far. Anyone have any tips for me as to what is wrong? Here is the code i have made (but i have replaced all the sensitive stuff with '*'):

     

    #include 
    
    
    const char* MY_SSID     = "*********";
    const char* PASSWORD = "***********";
    
    
    const String HOST = "***.***.**.**";
    const int HTTP_PORT = 80;
    const String URL = "/fillReservoir.php";
    
    
    const int RESERVOIR = 0;
    const int BLUE_LED = 2;
    
    
    int reservoirLevel = HIGH;
    int ledStatus = HIGH;
    
    
    void setup() {  
      delay(100);  
    
    
      pinMode(BLUE_LED, OUTPUT);
      digitalWrite(BLUE_LED, ledStatus);
    
    
      WiFi.mode(WIFI_STA);
      WiFi.begin(MY_SSID, PASSWORD);  
        
      while (WiFi.status() != WL_CONNECTED) {  
        delay(500);
        if (ledStatus == HIGH) {
          ledStatus = LOW;
        } else {
          ledStatus = HIGH; 
        }
        digitalWrite(BLUE_LED, ledStatus);
      }
      ledStatus = HIGH;
      digitalWrite(BLUE_LED, ledStatus);
      
      delay(100);  
      
      sendMessage();
      delay(500);  
      pinMode(RESERVOIR, INPUT);
      delay(100);
    }  
      
    void loop() {
      if (LOW == (reservoirLevel = digitalRead(RESERVOIR))) {
        sendMessage();
        delay(1000UL * 60UL * 24UL);
      }
    }
    
    
    void sendMessage() {
      WiFiClient client;  
        
      if (!client.connect(HOST, HTTP_PORT)) {  
        //Serial.println("connection failed");  
        return;  
      }  
        
      // We now create a URI for the request  
        
      //Serial.print("Requesting URL: ");  
      //Serial.println(URL);  
        
      // This will send the request to the server  
      client.print(String("GET ") + URL + " HTTP/1.1\r\n" +  
                   "Host: " + HOST + "\r\n" +   
                   "Connection: close\r\n\r\n");  
      delay(500);  
        
      // Read all the lines of the reply from server and print them to Serial  
      /*while(client.available()){  
        String line = client.readStringUntil('\r');  
      }  */
    }

    -raymond

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 8 years ago in reply to urkraft

    I wonder why it would be any different. And your code doesn't look fundamentally different than mine.

     

    This code below is what is working for my ESP-01. If you want to update my server, I can let you know the secretlocation and the url to monitor the updates.

    It basically just sends the values from 0 through 49 to the server, and blinks an LED while doing it (on while sending, off while waiting, or the reverse depending on the way the LED is hooked up).

    (I've also added it to my Github: https://github.com/ntewinkel/electronics )

     

    Using the USB-serial connection I'm also able to use the Arduino serial monitor to see the progress.

     

    /*
      ESP_sensor
      Reads the sensor value and updates the server with it
     
      The server call looks like:
      http://www.mulberryland.com/secretlocation/updateSensorValue.php?sensorID=002&value=77
     */
    
    
    #include 
    
    
    const char* ssid     = "mulBerryLand";
    const char* password = "secretpasswrd";
     
    const char* host = "www.mulberryland.com";
    const char* url = "/secretlocation/updateSensorValue.php";
    
    
    // Use WiFiClient class to create TCP connections
    WiFiClient client;
    const int httpPort = 80;
    
    
    // Set how long to sleep between sensor readings, to save battery life
    const int sleepTimeSecs = 10;  // in seconds
    
    
    // identify this specific sensor with a unique ID
    String sensorID = "001";
    
    
    void setup() {
      Serial.begin(115200);
      delay(100);
    
    
      Serial.println();
      Serial.println();
      Serial.print("Connecting to ");
      Serial.println(ssid);
      
      WiFi.begin(ssid, password);
      
      while (WiFi.status() != WL_CONNECTED) {
        delay(500);
        Serial.print(".");
      }
     
      Serial.println("");
      Serial.println("WiFi connected");  
      Serial.println("IP address: ");
      Serial.println(WiFi.localIP());
      Serial.print("Netmask: ");
      Serial.println(WiFi.subnetMask());
      Serial.print("Gateway: ");
      Serial.println(WiFi.gatewayIP());
    
    
      // initialize the digital pin as an output.
      pinMode(2, OUTPUT); // GPIO2 on ESP-01 is the only fully free pin available (GPIO0 should be available too with some extra work)
    }
    
    
    // the loop routine runs over and over again forever:
    void loop() {
    
    
      for (int sensorValue=0; sensorValue<50; sensorValue++) {
        digitalWrite(2, HIGH);
    
    
        // connect to the host
        Serial.println("Making the connection to the host...");
        if (!client.connect(host, httpPort)) {
          Serial.println("connection failed");
          return;
        }
    
    
        String label = "Sending request with new sensorValue: ";
        Serial.println(label + sensorValue);
            
        // This will send the request to the server
        client.print(String("GET ") + url + "?sensorID=" + sensorID + "&value=" + sensorValue +  " HTTP/1.1\r\n" +
                   "Host: " + host + "\r\n" + 
                   "Connection: close\r\n\r\n");
        delay(500);
      
        // Read all the lines of the reply from server and print them to Serial
        while(client.available()){
          String line = client.readStringUntil('\r');
          Serial.print(line);
        }
      
        Serial.println();
        Serial.println("closing connection");
        
        digitalWrite(2, LOW); 
        delay(1000); // wait for a second
    
    
        // sleep until the next reading
    //    Serial.println("ESP8266 is sleeping...");
    //    ESP.deepSleep(sleepTimeSecs * 1000000);
    //    Serial.println("ESP8266 is awake.");
      }
      
      // When done, just blink the LED
      while(true) {
        digitalWrite(2, HIGH);
        delay(1000);               // wait for a second
        digitalWrite(2, LOW); 
        delay(1000);               // wait for a second
      }
    }

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • urkraft
    urkraft over 8 years ago in reply to ntewinkel

    Thank you Nico, but it will not help me to have access to your server when i cannot connect to any WiFi - not even the one that is broadcasting its SSID. Since posting my code i have found indications that the WiFi object may be dependent on on a Serial object, but i have just tested code with a Serial object and that is not working either image! I just went through the code you have posted but cannot see any other fundamental differences.

     

    As i stated earlier, it appears as though the ESP-01 is stuck in the loop where it is waiting for a change in connection status. I will try changing the code so that it makes a few attempts to connect after waiting unsuccessfully for connection confirmation and see if that helps. I will also continue a while longer investigating how the ESP8266WiFi library is intended to be used before giving up for today.

     

    Thanks again for your assistance!

     

    Regards,

    raymond

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 8 years ago in reply to urkraft

    >when i cannot connect to any WiFi

    I'd offer you use of my WiFi network too, but that would require some travel on your part image

     

    I know, the code for the initial connection does look nearly identical, but I thought I'd share my code just in case there's a detail different. And maybe the serial debug will help.

     

    And I find it sometimes helps to have a full solution to play with while implementing my own version of things.

     

    Hope you get it figured out soon image

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • urkraft
    urkraft over 8 years ago in reply to ntewinkel

    Thank you very much for the offer Nico, but i have resolved the problems now. Just posted some of my findings.

     

    Regards,

    -raymond

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • urkraft
    urkraft over 8 years ago in reply to ntewinkel

    Thank you very much for the offer Nico, but i have resolved the problems now. Just posted some of my findings.

     

    Regards,

    -raymond