Month of Robots
  • Challenges & Projects
  • Project14
  • Month of Robots
  • More
  • Cancel
Month of Robots
Blog SuperRobot #1 : Getting Started
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Month of Robots to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dubbie
  • Date Created: 18 Apr 2019 3:48 PM Date Created
  • Views 1456 views
  • Likes 10 likes
  • Comments 2 comments
  • robot
  • morobotsch
  • mobile robot
  • superrobot
Related
Recommended

SuperRobot #1 : Getting Started

dubbie
dubbie
18 Apr 2019
image

Month of Robots

Enter Your Project for a chance to win robot prizes for your robot builds and a $200 shopping cart!  The Birthday Special: Robot Prizes for Robot Projects!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

I wanted to have a go at the Month of Robots for two main reasons. Mostly is that I really like making robots and secondly that it is a year since I started joining in the Project14 activities. The problem I was having was thinking of a robot that I could create that would be different to all my other robots, still be a fun robot, and that I could make it within the timescale available. For many days and nights I pondered what sort of robot I could make without much success and then I thought, why not make a robot that has many other robots within it, a SuperRobot. Obviously it would have to mainly be a mobile robot (just because they are the best) and I wanted something bigger than my usual ones, so a large base seemed like a good idea. I have some spare MDF so that sorted that. Then I just have to think of as many other robots as I might be able to make within the timescale. To make this easier I decided to take some existing products, mainly children's toys as these come with good external covers and hack them about until they do something robot like. I have two trains that run on the well known wooden rails, plus some talking farm animals. I also want to make some actual robots as well so hopefully at least one robot arm, and possibly another smaller mobile robot as well - which would be as good a small mobile robot as I can make. See below for the components that I was able to gather together to start with.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The first thing to do was to make the base move about. I wanted it to be simple to I have decided on two plastic casters at the front (cheap) and two small DC motors with gearboxes and tyres at the back (because I had them). I wanted to have some  significant ground clearance underneath the platform, just in case I decided to put some other robots underneath,  plus I didn't want to cut notches into the base board for the wheels. So the DC motors had to be upright and hence required a 3D printed holder. After several attempts I managed to design something that actually seemed to work (thanks for the advice from other Element14 participants on reducing the infill on 3D printed - it did seem to work better). I also had to 3D print some blocks for the castor wheels to lift up the front end to the same height as the back. I got those right first time!

 

Then it was just a matter of drilling some holes in the base board (not as easy as it sounds as the board is quite big and difficult to move, but I did manage to get it onto my pillar drill for the big holes -- just! Then it was off to the shops to buy some M3 and M4 screws as I just didn't have any of the required length and it all went together. See video below.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

There was a problem with the battery and the two DC motors in that the weight of the base board was just too much for 6 Volts. I did have a 12 V lead acid battery lying around so I tried that. It zoomed away with a distinct ozone/heating smell. I think 12Volts might be too much so I cobbled together a 9 Volt supply from a 6 V (4xAA) and a 3V (2xAA) just to see if it would work. Which, as you can see in the video, it does, mostly. When a reasonable load is added to the base plate then it struggles to get going. Much of this is down to the carpet it is travelling on but this is my test room so it has to work in here. And, if it works with this carpet it will work in most other areas as well.

 

So the base board is working, but with some limitations, but it is good enough so that I can start adding some other robots. I may have to replace the motors with something more powerful and mechanically stronger at a later date.

 

Dubbie

  • Sign in to reply

Top Comments

  • beacon_dave
    beacon_dave over 7 years ago +3
    Hmmm... looking at that train set... and if you are up for an additional challenge... https://www.youtube.com/watch?v=_ItWevaF2Ag https://www.youtube.com/watch?v=8qy0KbQVzfg Outtakes: https://www.youtube…
  • dubbie
    dubbie over 7 years ago in reply to beacon_dave +3
    Dave, A funny video, especially the outtakes - which I think are the more likely outcome if I tried this. Maybe something a lot simpler might be possible, not sure what at present, maybe turning the train…
  • dubbie
    dubbie over 7 years ago in reply to beacon_dave

    Dave,

     

    A funny video, especially the outtakes - which I think are the more likely outcome if I tried this. Maybe something a lot simpler might be possible, not sure what at present, maybe turning the train on and off?

     

    Dubbie

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 7 years ago

    Hmmm... looking at that train set... and if you are up for an additional challenge...    image

    https://www.youtube.com/watch?v=_ItWevaF2Ag

    https://www.youtube.com/watch?v=8qy0KbQVzfg

     

    Outtakes:

    https://www.youtube.com/watch?v=7ZZCOa9Mhw4

    • Cancel
    • Vote Up +3 Vote Down