Movers and Shakers
  • Challenges & Projects
  • Project14
  • Movers and Shakers
  • More
  • Cancel
Movers and Shakers
Blog Walky the Biped Robot - A new hope (actually a new body and battery)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Movers and Shakers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: genebren
  • Date Created: 9 Jul 2018 3:23 PM Date Created
  • Views 3665 views
  • Likes 14 likes
  • Comments 13 comments
  • 3d pritning
  • fusion 360
  • robotics
  • moversshakersch
  • panasonic batteries
Related
Recommended

Walky the Biped Robot - A new hope (actually a new body and battery)

genebren
genebren
9 Jul 2018
image

Movers and Shakers

Enter Your Electronics & Design Project for Your Chance to Win a $100 Shopping Cart!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

Previous post in the sequence:

Walky the Biped Robot - The prequel

Walky the Biped Robot - Power pack

Walky the Biped Robot - Oops, Walky has an accident!

 

Walky is not quite ready to walk, but still moving in the right direction.  I have redesigned the main body of Walky, opting for a two piece structure. While I had Fusion360 open, I also designed new feet, legs and accessory mounts that I will be printing over the next few days.

imageimageimage

Here is are multiple views of the body with power pack and servos installed.  The parting line between the two halves is barely visible (first image) and the recessed holes for the joining screws worked out wonderfully (second and third images). That shiny red battery is new too. Earlier testing of UltraFire (not!) batteries was disappointing.  These batteries over promised and under delivered, yielding a capacity around 250-350mAh as opposed to their advertised capacity of 1200mAh.  The new Panasonic batteries (UR14500P) did not disappoint.  Here are the results from the first charge/discharge test:

imageimage

In both tests, the accumulated capacity calculations were extremely close to the advertised capacity, most likely varying only due to forced discharge stop of 2.7Volts.  Now we are cooking!  With a steady state load of 500mA on the 5Volt boost supply, this battery will give me over an hour of play time with Walky (although I expect that in normal operation the load will be less that 500mA).  The charge rate is conservative, at ~.6C, while taking ~2.5 hours.  The discharge rate varied from ~.8C to ~1.2C throughout the test, while lasting ~70minutes. Once again, thanks shabaz for the great battery recommendation!

 

Thanks for reading along. Hopefully, with a bit of 3D printing time I hope to have Walky back on his new feet soon!

Gene

  • Sign in to reply

Top Comments

  • DAB
    DAB over 8 years ago +3
    Nice update. I look forward to seeing if the batteries hold up in real use. DAB
  • three-phase
    three-phase over 8 years ago +3
    Good to see the progress being made, looking forward to see you producing the items with your 3D printer. Kind regards
  • jw0752
    jw0752 over 8 years ago in reply to genebren +3
    Hi Gene, You are assuming that you are going to be there when the power fails. Take a trip to the store and by the time you get back it might be too late. Here is my main lab backup battery. I used a cheap…
Parents
  • jw0752
    jw0752 over 8 years ago

    Hi Gene,

    Your printer did a really nice job on the body pieces. I am glad that the battery hurdle has been overcome.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 8 years ago in reply to jw0752

    John,

     

    I am having a lot of fun using the 3D printer.  I only wish that some of these prints did not take so long.  Each half of the body was a 5+ hour print.  I had a failure on my first attempt of printing the second half, stopping almost halfway through the print.  I was worried that I might be having some hardware/software issues with the printer, so I was nervously waiting as the second attempt ran.  In the meantime, I purchased and installed a beefy UPS system, in the event that the failure occurred due to a weather induced power glitch.

     

    I am starting to run down the list of remaining parts to printed, trying to get a 5+ hour run done tonight.

     

    Take care,

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 8 years ago in reply to genebren

    Hi Gene,

     

    I have picked up UPS systems from various sources that were failed. It is almost always just the battery. In my critical situations I have replaced the little battery that they come with, with a regular car battery so that my power down protection can extend for well over an hour. I don't know what the wattage is on your 3D printer but if you may need power for more than a short time you might want to consider a backup battery.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 8 years ago in reply to jw0752

    John,

     

    I really like the way that you jump in and fix and/or enhance anything.  I currently have almost 2000 Watts of backup power in the office.  I like the idea of adding more capacity to the systems with an additonal battery, but my initial plan is just to have enough power to safely stop the printer (pause) and be able to wait out the restoration of power in a low-drain state.

     

    Gene

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 8 years ago in reply to genebren

    Hi Gene,

    You are assuming that you are going to be there when the power fails. Take a trip to the store and by the time you get back it might be too late. Here is my main lab backup battery.

     

    image

     

    I used a cheap Chinese Volt / Ammeter so that I can monitor current consumption and voltage level. It is also magic as there hasn't been a significant power failure since I put it together.

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 8 years ago in reply to genebren

    Some of the UPS have a serial output, or relay.

    Many nowdays have SNMP that you could use to detect that it's running on battery and send the appropriate signal to the printer.

     

    My only caution with adding more battery power is the temperature of the UPS when delivering full load for extended periods.

     

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mcb1
    mcb1 over 8 years ago in reply to genebren

    Some of the UPS have a serial output, or relay.

    Many nowdays have SNMP that you could use to detect that it's running on battery and send the appropriate signal to the printer.

     

    My only caution with adding more battery power is the temperature of the UPS when delivering full load for extended periods.

     

    Mark