Movers and Shakers
  • Challenges & Projects
  • Project14
  • Movers and Shakers
  • More
  • Cancel
Movers and Shakers
Blog Walky the Biped Robot - Oops, Walky has an accident!
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Movers and Shakers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: genebren
  • Date Created: 6 Jul 2018 3:36 PM Date Created
  • Views 2420 views
  • Likes 16 likes
  • Comments 7 comments
  • 3d pritning
  • moversshakersch
  • li-ionlinearbatterycharger
  • 3d design
Related
Recommended

Walky the Biped Robot - Oops, Walky has an accident!

genebren
genebren
6 Jul 2018
image

Movers and Shakers

Enter Your Electronics & Design Project for Your Chance to Win a $100 Shopping Cart!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

Previous post in the sequence:

Walky the Biped Robot - The prequel

Walky the Biped Robot - Power pack

 

Walky has always had a prominent place around my workspace since it was created.

image

Unfortunately, yesterday afternoon Walky suffered a pretty major accident.  I was in the process of adding a couple of holes to assist in cable routing, when the drill stuck and 'crack', Walky was in pieces (I know that I should have been using my 'plastic' drill bits, but I was sure I could go slow enough to get a clean cut).  At first I thought, I will be able to re-glue him, but after a bit of reflection, I decided that maybe it is time for Walky II.  'Rest in Pieces Walky'.

imageimage

I had been working on building a mounting board for attaching the new controller board (adapting the existing hole patter on Walky's top to the new board), when I noticed that the servo wires were going to making some tight bends.  So a couple of side holes seemed like a good idea.  This is where having a 3D printer is so cool.

imageimage

 

 

Here is the new servo controller (blank) attached to the mounting bracket and mated to the power pack board (gently positioned around Walky's broken body.  You might noticed that the power pack is sans battery.  Another interesting story there.  I had attached a 'flying lead' to the positive terminal of the battery on the power pack to allow me to externally monitor the battery voltage during charge/discharge testing.  While I was designing the mounting bracket for the servo controller board, I was using the power pack to capture some dimensional measurements.  At one point in the process I began to smell smoldering plastic.  At first I thought it was the 3D printer.  No, not there.  I kept looking around until I noticed that power pack under my note pad.  Digging it out I noticed the outer sheath of the battery was split and discolored.  Not to mention that the battery was smoking hot!  I found the 'flying lead' welded to the metal housing of the USB connector (ground) and quickly removed it.  I then quickly took the power pack out to the garage where I was able to extract the battery from the power pack (with pliers). Don't do this at home folks.  I later had to explain the burnt smells coming from the office to my wife (who was currently doing a little burning of her own, while roasting some vegetables.  I guess that family that burns together stays together.

 

 

 

 

 

Now it was time to start on the body of Walky II.  I ended up with a split case design for the body.

 

image

It is kind of cool that I can simply mirror the design of this side to create the other side.  I added some through hole mounting holes inside of bosses to join the two halves.  In retrospect it would have been nice to add some alignment pins/holes to the edges to help keep the case halves together.  I am currently printing the first half, so time will tell as to the correctness of this design. (We have been having some thunderstorms lately and lost power a couple of times.  Since my 3D printer is not on the UPS, I will have to hope that I can couple the 4 hour prints without power interruptions)

 

I still have not decided if I will continue to re-design Walky, i.e. new legs and feet.  I guess that it will look a little better (more color coordinated) if I do.

 

Thanks for reading along.  More to come.

Gene

  • Sign in to reply

Top Comments

  • three-phase
    three-phase over 8 years ago +7
    Hopefully you can utilise a small part of Walky within the next generation, so he lives on for a while yet. Kind regards
  • genebren
    genebren over 8 years ago in reply to three-phase +6
    Donald, I do plan to at least use the servos and the associated linkages. So there will be a small piece of the original. Gene
  • jw0752
    jw0752 over 8 years ago +6
    Every time I crack important plastic with my drill I swear I have learned my lesson. Unfortunately time has proven me wrong. John
Parents
  • jw0752
    jw0752 over 8 years ago

    Every time I crack important plastic with my drill I swear I have learned my lesson. Unfortunately time has proven me wrong.

    John

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jw0752
    jw0752 over 8 years ago

    Every time I crack important plastic with my drill I swear I have learned my lesson. Unfortunately time has proven me wrong.

    John

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • genebren
    genebren over 8 years ago in reply to jw0752

    Yeah, I know what you mean.  I have a collection of plastic cutting drill bits (but not quite as large as the whole I was hoping to drill), but I grabbed the first available drill index and a rather large step up from the existing hole and went to town on the holes.  The bit had already grabbed once (without damage), and I was retrying (without clearing out the hole), so I got what I asked for, a mess.  Impatience is not my normal mode, but I was doing a lot of jumping back and forth between tasks, which is never my best approach (not really a good multi-tasker).

     

    Oh well, live and learn (hopefully).

    Gene