NFC/RFID
  • Challenges & Projects
  • Project14
  • NFC/RFID
  • More
  • Cancel
NFC/RFID
Blog LockNFC - Does the PCB work?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join NFC/RFID to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Fred27
  • Date Created: 28 Apr 2019 7:55 PM Date Created
  • Views 2483 views
  • Likes 10 likes
  • Comments 3 comments
  • eagle
  • nfcrfidch
  • msp430fr2633
  • nfc
  • msp430
  • trf7970a
  • capacitive touch
Related
Recommended

LockNFC - Does the PCB work?

Fred27
Fred27
28 Apr 2019
image

NFC RFID

Enter Your Electronics & Design Project for a chance to win a $100 Shopping Cart!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

So, after waiting for the PCB to arrive from Seed, it was time to populate it, run it through the toaster oven and see if I'd made any mistakes. As usual, I struggled a bit with the QFN soldering of the TRF7970A NFC transceiver. I can never seem to get these right without using solder paste, then slapping on too much solder with a soldering iron and then wicking it away. I can take a few goes, but I seem to get there in the end. The final result looks professional enough with the naked eye even if the process certainly wasn't. Give me QFP over QFN any day!image

 

You can't really test the hardware without some firmware running on the microcontroller, so I quickly adapted my test code from the development board. It wasn't too long until I had the capacitive touch button code running and working. Then I got the NFC code reading an NFC tag. I've yet to combine the two lots of code properly, other that to ensure they fit in the flash of the MSP430FR2633. The demo makes it look a lot more finished than it is. I wasn't too happy with is the sensitivity of the buttons. They seemed a bit too sensitive when I used it and would often register a double press. However, when my kids tried it had trouble detecting their little fingers. The NFC antenna certainly worked and I was pleasantly surprised for a first attempt, but I was sure it could be better. I was really pleased that the reverse mount LED diffuses nicely through the PCB. I suspect that if I have another next to it that I would get light bleed between them, but as I've only got one it works really well.
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
I don't know why I'm still surprised when a board that I've designed works, but I still am - every time.

Next post - Antenna tuning >>

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 7 years ago +2
    Hi Fred, This is awesome! It looks like a manufactured-quality product : ) The response seems quick to the tag and button-presses. Also, nice combination with the solder mask colour and the silkscreen…
  • genebren
    genebren over 7 years ago +2
    Nice job! Everything looks great and the performance seem very good. Nicely done. Gene
  • Fred27
    Fred27 over 7 years ago in reply to genebren +1
    Thanks. The antenna matching improved the NFC reader quite a bit after the video was taken. It's hard to catch the read distance on video, and even more so how accurate you need to be aligning with the…
Parents
  • shabaz
    shabaz over 7 years ago

    Hi Fred,

     

    This is awesome! It looks like a manufactured-quality product : )

    The response seems quick to the tag and button-presses. Also, nice combination with the solder mask colour and the silkscreen.. the PCB diffusion method for the LED is very cool.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 7 years ago

    Hi Fred,

     

    This is awesome! It looks like a manufactured-quality product : )

    The response seems quick to the tag and button-presses. Also, nice combination with the solder mask colour and the silkscreen.. the PCB diffusion method for the LED is very cool.