Off-the-Grid
  • Challenges & Projects
  • Project14
  • Off-the-Grid
  • More
  • Cancel
Off-the-Grid
Off-the-Grid Blog Solar Powered Tropical Beverage Cooling Mug -Blog #5 –*DRAMATIC* step fwd- building a Peltier module chill plate/fan cooled heatsink assembly.
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Off-the-Grid to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: robogary
  • Date Created: 19 Jun 2023 2:32 AM Date Created
  • Views 4762 views
  • Likes 10 likes
  • Comments 2 comments
  • Wrongco
  • robogary
  • offthegridch
  • arduino
Related
Recommended

Solar Powered Tropical Beverage Cooling Mug -Blog #5 –*DRAMATIC* step fwd- building a Peltier module chill plate/fan cooled heatsink assembly.

robogary
robogary
19 Jun 2023

The project is to build a solar powered Tropical Beverage Cooling Mug.  

image

Previous blogs:

Solar Powered Tropical Beverage Cooling Mug -Blog #4 – Learning to cool with Peltier modules

Solar Powered Tropical Beverage Cooling Mug -Blog #3 - the solar charging system

Solar Powered Tropical Beverage Cooling Mug - blog #2 - the solar panel characterization

Solar Powered Tropical Beverage Cooling Mug -Blog #1 - the concept

 

Lessons learned in Blog 4 included the Peltier module needs a heatsink and fan.

This blog #5: 

  • This blog shows how a chill plate and fan cooled heatsink assembly was built and tested for a Peltier module.
  • The fan used is a DF124020BH-A 12V .25a fan.
  • The fan is powered with 5.6V dc for this test to simulate a low battery condition.
  • Ambient temperature is a regulated 20C.
  • Peltier module resistance varies over time and temperature.

I didnt have any good heatsink paste on hand. Surfed the web for substitutes and found an interesting one, diaper rash ointment. I had a fresh tube with 40% zinc oxide, used that for heatsink paste.

Notice in the photos BOUDREAUXS BUTT PASTE ! for real, and it worked. The heatsink was salvaged from an old PC. The chill plate was a simple metal plate bent in a vice to approximately wrap a beverage container.

This test will also fair better if the cup frame is insulated.

Each test step was 30 minutes long. The peltier module was fed in 1 Volt steps, current recorded, after 30 minutes, the chill plate temperature was recorded and the heatsink hottest spot temperature recorded.

Conclusion: This design will actually work well for chilling small tropical beverages !

The lessons learned can be used to build small dehumidifiers, chillers, of compact heaters.

Likely can reduce size of heatsink and/or eliminate fan

Start time (ambient 20C)

Peltier module Volts=1V

Peltier module amps=.13A

30 minutes after start

Chill plate temp=18C

Heatsink hotspot temp=22C

30 minutes after start

Increase Peltier module Volts=2V

Peltier module amps=.73 decreasing to .33

60 minutes after start

Chill plate temp=16C

Heatsink hotspot temp=22C

60 minutes after start

Increase Peltier module Volts=3V

Peltier module amps=1.23A decreasing to 1.16A

90 minutes after start

Chill plate temp=6C

Heatsink hotspot temp=27C

90 minutes after start

Increase Peltier module Volts=4V

Peltier module amps=1.66A decreasing to 1.36A

120 minutes after start

Chill plate temp=4C

Heatsink hotspot temp=30C

120 minutes after start

Increase Peltier module Volts=4.6V

Peltier module amps=2A (MAX) decreasing to 1.95A

150 minutes after start

Chill plate temp=4C with significant chill plate condensation

Heatsink hotspot temp=35C

 

imageimage

image

significant condensation of ambient air on chill plate

image

This is the step by step photos for building the chill plate - fan cooled heatsink assembly

image

image

image

image

image

image

image

image

image

  • Sign in to reply

Top Comments

  • robogary
    robogary over 3 years ago +1
    Do you also cook with the ointment ?
  • DAB
    DAB over 3 years ago +1
    You will have to do a heat transfer measurement on the Butt Paste as opposed to standard lithium grease.
  • DAB
    DAB over 3 years ago

    You will have to do a heat transfer measurement on the Butt Paste as opposed to standard lithium grease.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • robogary
    robogary over 3 years ago

    Do you also cook with the ointment ?