Off the Shelf
  • Challenges & Projects
  • Project14
  • Off the Shelf
  • More
  • Cancel
Off the Shelf
Blog Arduino Nano as Raspberry Pi IO I2C expander PART 4 - humbling persistence, scope creep, Python Voodoo, and over the hump
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Off the Shelf to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: robogary
  • Date Created: 28 Sep 2021 1:45 AM Date Created
  • Views 1047 views
  • Likes 1 like
  • Comments 0 comments
  • offtheshelfch
Related
Recommended

Arduino Nano as Raspberry Pi IO I2C expander PART 4 - humbling persistence, scope creep, Python Voodoo, and over the hump

robogary
robogary
28 Sep 2021

The next update will be the final project completed !!

Test code of 5 bytes of data from the Arduino to the Raspberry Pi is working and being melded with functionality for meeting the final project goal + some scope creep that just fit in too well.

 

Thank you to these resources whose examples helped me the most to figure out the code:

https://oscarliang.com/raspberry-pi-arduino-connected-i2c/

https://roboticsbackend.com/raspberry-pi-master-arduino-slave-i2c-communication-with-wiringpi/

https://36projectsblog.wordpress.com/8-raspberry-pi-reading-i2c-sensors-using-python/

 

 

I still had to overcome my own stumblings - like reading the Arduino analog values over I2C, reconstructing the values to INT from bytes, then typing in an incorrect scale factor on the high byte. 

Added a feature to enable/disable the rotor main motor using the joystick push down switch. Unfortunately I forgot the switch N.O. contact was pulled down to zero rather than a pulled up to 5V.

 

This is the working Raspberry Pi Python code to read 5 bytes from the Arduino Nano.

I kept some of the code that didnt work in the python file , commented out, as a reminder of how NOT to do it.

 

The python code looks small, but it involves alot of suffering, mental anguish, and mindless determination  :-) 

 

I almost pulled out a scope to start troubleshooting the I2C data, realizing a data analyzer really is the needed tool - I'll be on watch for a Road Test opportunity for one of those  :-)

 

import smbus

import time

# for RPI version 1, use "bus = smbus.SMBus(0)"

bus = smbus.SMBus(1)

# This is the address we setup in the Arduino Program

address = 0x08

IOarray=([ 0,0,0,0,0,0])

 

 

## def writeNumber(value):

##    bus.write_byte(address, value)

    # bus.write_byte_data(address, 0, value)

##    return -1

 

 

##def readNumber():

##    number = bus.read_byte(address)

    #number = bus.read_byte_data(address, 1)

##    return number

 

 

while True:

    time.sleep(2)

    JoystickData = bus.read_i2c_block_data(0x08, 0x00, 5)

    print (" JoystickData=", JoystickData)

    LeftRightJoystick=(JoystickData[0]+(JoystickData[1]*256))

    print (" LeftRightJoystick =", LeftRightJoystick)

    FwdBackJoystick=(JoystickData[2]+(JoystickData[3]*256))

    print (" FwdBackJoystick =", FwdBackJoystick)

    EnableServos = JoystickData[4]

    print (" EnableServos =", EnableServos)

 

 

    #the array line by byte doesnt work correctly. Shown as a warning to not do it this way

    #IOarray[0] = bus.read_byte_data(address,0x00) ## this does not work right to read multiple bytes

    #IOarray[1] = bus.read_byte_data(address,0x01) ##right hi byte

    #IOarray[2] = bus.read_byte_data(address,0x02) ##back  lo byte

    #IOarray[3] = bus.read_byte_data(address,0x03) ##fwd hi byte

    #IOarray[4] = bus.read_byte_data(address,0x04) ## constant 16

    #print ("IOArray[0]=", IOarray[0])

    #print ("IOArray[1]=", IOarray[1])

    #print ("IOArray[2]=", IOarray[2])

    #print ("IOArray[3]=", IOarray[3])

    #print ("IOArray[4]=", IOarray[4])

 

Up Next - the final python code, Arduino code, schematic, and an action video  of the working project - sorry Vin Diesel was not available to operate the joystick