Op-Amp-a-Palooza
  • Challenges & Projects
  • Project14
  • Op-Amp-a-Palooza
  • More
  • Cancel
Op-Amp-a-Palooza
Blog E14 Op-amp Kit - First Power Up
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Op-Amp-a-Palooza to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: scottiebabe
  • Date Created: 23 Mar 2022 2:58 PM Date Created
  • Views 6439 views
  • Likes 13 likes
  • Comments 5 comments
  • opampsch
  • opamps
  • project14
Related
Recommended

E14 Op-amp Kit - First Power Up

scottiebabe
scottiebabe
23 Mar 2022

I am happy to report both Renesas op-amps made it safe and sound onto a breadboard. Additionally, I am even more thrilled that the 61 MHz bandwidth op-amp doesn’t breakout into oscillation when used in a breadboard.

Both op-amps I received in my op-amp-a-palooza kit are modern surface mount devices. Fortunately, I have a bag of little breakout boards on hand. So, the first step in experimenting with these op-amps was to mount them onto an SMD to DIP breakout board.

image (ISL28291 in an SOIC-8 package)

image (ISL28213 in an MSOP-8 package)

On the underside of the breakout board, I added a 10 uF 16V MLCC bypass capacitor for my best chance of success using these amplifiers on a breadboard.

image

I didn't take a photo, but I also added a 30 AWG mod wire from the capacitor to the appropriate power pin.

I then wired up the two op-amps on my breadboard as unity gain buffers. I used my MP750668 function generator as a signal source. 

 image

image

Renesas ISL28213

A nice little general purpose CMOS input op-amp with the following bannerline specifications:

image

Small signal step response of the op-amp shows minimal overshoot (good phase margin):

image

Also, the small signal step response shows good agreement with the spice model provided on Renesas’s website.

image

The large signal step response and slew rate:

image

Renesas ISL28291

Is a nice little precision, low noise, modestly fast op-amp with the following high level specifications:

image

Here is the small signal step response (not bad for a circuit on a breadboard):

image

The spice model of the ISL28291 look reasonable similar to what I measured on a breadboard, I think that is a win!

image

image

image

Summary

Both Renesas op-amps are unity-gain stable:

  • In a breadboard
  • With a 10x scope probe on the output (~20 pF)
  • With a 1x scope probe on the output (~120 pF)
  • Modest feedback resistance of 100 kOhms

The noise seen in the scope shots are the results of a rats nest of hookup wires and probes and not the op-amps themselves.

The ISL28291 is a fast op-amp, but not too fast for its own good Slight smile.

  • Sign in to reply
Parents
  • robogary
    robogary over 4 years ago

    Thanks for the photos, the surface mount breadboard adapters are handy, I hadnt seen blank ones before. That maybe something to open a new world of possibilities. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • robogary
    robogary over 4 years ago

    Thanks for the photos, the surface mount breadboard adapters are handy, I hadnt seen blank ones before. That maybe something to open a new world of possibilities.