Open Arduino
  • Challenges & Projects
  • Project14
  • Open Arduino
  • More
  • Cancel
Open Arduino
Blog Cycloboat
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Arduino to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Molham
  • Date Created: 29 May 2018 4:21 PM Date Created
  • Views 3379 views
  • Likes 9 likes
  • Comments 9 comments
  • arduino_classic
  • arduinos
  • Arduino Day
  • openarduinoch
  • project14
Related
Recommended

Cycloboat

Molham
Molham
29 May 2018

Cycloboat is a recycled boat robot that uses plastic bottles to float on water.

It can detect objects and avoid it using ultrasonic.

 

I will be posting more videos with some more description later.

 

1. Right Angle Gear Motor: voltage is 4.5-6V with a no load current of 190mA, output shaft is 9mm long and the gearbox ratio is 48:1 with a wheel speed of 140 RPM (unloaded)

2. Dual Ball Bearing Hub

3. Arduino Uno as a brain and control system of Cycloboat

4. L298N Motor Drive Controller Board Module Dual H Bridge.

5. Ultrasonic Module

6. Batteries 4 x 1.5v each total of 6v dc

7. Fan recycled from old fan

8. Sealed wood box.

9. Aluminum Pole and mounting channels hub.

10. Recycled plastic bottles X 3.

image

Figure (1): Right Angle Gear Motor

image

Figure (2): Dual Ball Bearing Hub

image

Figure (3): ARDUINO UNO MCU ATMEGA328p

image

Figure (4): L298N Motor Drive Controller Board Module Dual H Bridge.

image

Figure (5): Ultrasonic Module.

image

Figure (7): Fan recycled from old fan.

Full System

image

Code:

 

$regfile = "m328pdef.dat"
'$regfile = "m16def.dat"
$crystal = 8000000




Config Pind.2 = Output : Dc1 Alias Portd.2 : Reset Dc1
Config Pind.1 = Output : Dc2 Alias Portd.1 : Reset Dc2


Config Pind.3 = Input
Config Portd.4 = Output
Portd.3 = 0
Portd.4 = 0
Dim Distance As Word , W As Word , I As Byte


'-----------------------[LCD Configurations]




Distance = 0
Cls


Do
Pulseout Portd , 4 , 20                                     'Min. 10us pulse
'Waitms 100 'meant for testing error
Pulsein W , Pind , 3 , 1                                    'read distance
Incr I
If Err = 0 Then
W = W * 10                                                  'calcullate to
W = W / 58                                                  ' centimeters
'W = W / 6 ' milimeters
Distance = W
Gosub Move_backward : Waitms 200
Else
Distance = 0
Gosub Move_forward : Waitms 200
End If






Waitms 200
Loop
Return


'--->[Move Renbot with 4 motors forward]
Move_forward:


   Set Dc1 : Reset Dc2
   Waitms 100
Return
'-----------------------


'--->[Move Renbot with 4 motors backward ]
Move_backward:


   Reset Dc1 : Set Dc2 :
   Waitms 100
Return
'-----------------------

imageimageimageimageimage

 

First test:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • 14rhb
    14rhb over 8 years ago +2
    Hi Molham, A great idea. I was particularly taken though with those neat pre-drilled brackets, and when I searched for 'dual ball bearing hub' I found a site that makes them....they look really useful…
  • tariq.ahmad
    tariq.ahmad over 8 years ago +2
    Very cool!
  • DAB
    DAB over 8 years ago +2
    Your approach has some interesting possibilities. DAB
Parents
  • DAB
    DAB over 8 years ago

    Your approach has some interesting possibilities.

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Molham
    Molham over 8 years ago in reply to DAB

    I agree, I am going to add speed control to it and also I am testing a solar panel to be a power source since the sun here in San Diego is always shining.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Molham
    Molham over 8 years ago in reply to DAB

    I agree, I am going to add speed control to it and also I am testing a solar panel to be a power source since the sun here in San Diego is always shining.