Open Arduino
  • Challenges & Projects
  • Project14
  • Open Arduino
  • More
  • Cancel
Open Arduino
Blog Exploding Kittens Soundboard
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Arduino to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fvan
  • Date Created: 13 May 2018 12:01 PM Date Created
  • Views 5576 views
  • Likes 9 likes
  • Comments 8 comments
  • ardbeginner
  • arduino_projects
  • arduino_classic
  • openarduinoch
Related
Recommended

Exploding Kittens Soundboard

fvan
fvan
13 May 2018

Between the Pi-Top - A Raspberry Pi Laptop RoadTest and the Bluetooth Unleashed Design Challenge I had some difficulties finding time to make a proper Arduino project. On the other hand, my Hero board for the design challenge is an Arduino compatible board with Bluetooth capabilities, so that must count for something ? image

 

Here's a very simple project I made a while back, using the Bare Conductive Touch Board Bare Conductive Touch Board: an Exploding Kittens Soundboard. Don't worry, I didn't really make any kittens explode ... Exploding Kittens is a card game I play frequently, which I find to be a lot of fun.

 

There's no coding involved in this particular project, as the default sketch on the TouchBoard takes care of all the needed functionality.

 

Build

 

I started off by picking en element from the game and reproducing it physically. The obvious choice, is one of the kittens on an explosion card.

image

 

Based on the card, I drew the kitten on a piece of wood and cut it out using the jigsaw. After a bit of sanding, I applied grey paint to the front and when dry, applied the details using black. Taking into consideration the fact that I’m not a woodworker and that I suck at drawing, the result is not that bad!

image

 

To have the kitten be able to stand up straight, I added a hinge and a small piece of wood.

image

 

Electronics

 

The electronics are simple. The Touch Board (originally launched via Kickstarter) is an Arduino compatible board, offering capacitive touch sensing and mp3 play out, making it perfect for this project. Using conductive paint, four pads were created, each capable of triggering a different sound effect. The board supports up to twelve touch points, should you want or need even more sound effects.  Copper tape connects the pads to the Touch Board. No programming required, as explained earlier!

image

 

Even through the wood (18mm), hovering your hand in front of the pad, triggers the sensor and plays the sound effect.

 

The Touch Board is powered using a LiPo battery, which can be charged via the board when connected via USB. There is also a handy on/off switch available onboard.

image

 

Finally, the speaker I used is a rechargeable, powered speaker connected to the Touch Board using the stereo jack. Alternatively, a small speaker and amplifier breakout board could be used.

 

Video

 

Here's a video showing the build process of the project, followed by a demo:

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

This little kitten has been making playing sessions more interactive since image

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 8 years ago +3
    I played this card game with one of the grandkids. Very Strange. Your build was great and I enjoyed watching the construction. John
  • fmilburn
    fmilburn over 8 years ago +3
    Brought a smile ... I may have to try something like this.
  • tariq.ahmad
    tariq.ahmad over 8 years ago +3
    Thanks fvan ! When you're as young as Project14 you want everyone that helped you get this far at your birthday and your project made an awesome an entrance!
Parents
  • mcb1
    mcb1 over 8 years ago

    Very good.

    I'm amazed at how fast the whole process was ... I guess it was sped up, or you've resolved that time contineum thing.

     

    Surprising how far the sensor will pick up the change in capacitance.

     

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mcb1
    mcb1 over 8 years ago

    Very good.

    I'm amazed at how fast the whole process was ... I guess it was sped up, or you've resolved that time contineum thing.

     

    Surprising how far the sensor will pick up the change in capacitance.

     

    Mark