• Products and Partners
    Products and Partners
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
Portable Electronics Kit
  • Challenges & Projects
  • Project14
  • Portable Electronics Kit
  • More
  • Cancel
Portable Electronics Kit
Blog Babbages Baggage
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Portable Electronics Kit to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Workshopshed
  • Date Created: 10 Feb 2018 9:37 PM Date Created
  • Views 3882 views
  • Likes 20 likes
  • Comments 13 comments
  • portableekitch
Related
Recommended

Babbages Baggage

Workshopshed
Workshopshed
10 Feb 2018

When I saw the brief for this month the first thing I thought of was "The Luggage".

The Luggage is a fictional object that appears in several of the Discworld novels by Terry Pratchett. It is a large chest made of Sapient Pearwood (a magical, intelligent plant which is nearly extinct, impervious to magic, and only grows in a few places outside the Agatean Empire, generally on sites of very old magic, such as Indian burial grounds and ancient monolithic sites). It can produce hundreds of little legs protruding from its underside and can move very fast if the need arises. It has been described as "half suitcase, half homicidal maniac" (Sourcery paperback p22).image

"Babbages baggage" is my interpretation of this, perhaps Rincewind travelled through a magic portal to England on one of his adventures and taught Babbage how to make his own version of the chest.

 

For the project I first looked at a range of walking robots. There are loads of these and many you can 3D print yourself. These required a lot of servos but they typically have about 6 legs and that did not seem enough for me.

 

Then I spotted some giant centipede toys with loads of legs and a remote control. I took a look at the pictures and concluded that it had lots of potential so I ordered one. In parallel to this I got thinking about the chest. I had seen some small "treasure chests" at a recent Pirate Themed party and wonder if I could get hold of one of those. After a lot of searching I eventually found one on my doorstep in the local corner shop.

 

When the centipede arrived I did a quick test and was very happy.  When I started taking it apart I was even happier as it was a complete dream to hack. The centipede was screwed together and came apart really easily. The chest was just the right size for the legs. As suspected the mechanics were all hidden in the head. Two tiny motors with right angled gearboxes drove two wheels, there were LEDs to indicate that it was turned on (bonus). And to my surprise it actually came with the ability to steer and the centipede could be controlled although I kept crashing it into the chairs.

imageimage

The control circuit consists of a Lipo battery, there's no sign of a charger here but there is a "special" cable that connects to USB so perhaps there's a small charger in that. The switch simply connects the + of the battery to either the control circuit or to the charging socket. There's an IR photo transistor on the top of the board and an 8 pin chip on the bottom. That chip seems to drive a couple of transistors which I'm guessing are connected to the motors. There does not seem to be any markings on the chip other than the silk screen.

imageimage

I collected together the parts and made some suitable holes in the chest for the LED eyes, power connector, on-off switch and motor wiring. The electronics were nicely housed in the lid of the chest and I used sugru to hold everything in place. A couple of brackets and a meccano wheel were added to the bottom along with the motor and some legs. There's still plenty of space left in the chest to store a range of electronic components such as variable dibbler, high voltage angua or a nanny ogg.

 

image

Here's the resulting "Babbages Baggage"

image

Demo

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • Workshopshed
    Workshopshed over 8 years ago in reply to genebren +6
    The cat is the only other member of the family that's seen it. I feared that if the others saw it before it was disassembled they might insist that it was kept.
  • genebren
    genebren over 8 years ago +5
    Andy, What a fun little project. But I wonder, isn't the cat a like upset that you hacked his toy to pieces? I look for to the video of your test drive. Keep having fun, it keeps you young! Gene
  • mcb1
    mcb1 over 8 years ago +4
    Nice. Not sure it's a Portable Electronics Kit but is certainly very novel. My cats aren't interested in wheeled vehicles or things that move along the floor, but bring out the micro drone and they're…
Parents
  • mcb1
    mcb1 over 8 years ago

    Nice.

    Not sure it's a Portable Electronics Kit but is certainly very novel.

     

    My cats aren't interested in wheeled vehicles or things that move along the floor, but bring out the micro drone and they're sitting there waiting to swat it. The blade noise doesn't phase them one bit.

     

    Be interesting to see the video.

     

    Mark

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 8 years ago in reply to mcb1

    I seem to recall reading that a cats vision system responds more to side-to-side movement and not too close. May be why they respond to the drone more ?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 8 years ago in reply to beacon_dave

    According to this video, cats are far-sighted so best to keep the toy >10" away from the cat and to move the toy away from the cat

    https://www.youtube.com/watch?v=BY3SLVNBkeo

    ...and let the cat catch/kill the toy. (Not sure that this is such a good idea for the micro drone approach however !)

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 8 years ago in reply to beacon_dave

    Somewhere I read/heard that cats that are good hunters don't react to the images on the Tv as they don't see the picture.

    Not sure if it's true or not, but we have two that hear the noise but can't match it to the image.

     

    Mark

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 8 years ago in reply to mcb1

    I've heard that with dogs. It may be the low refresh rate of the TV image. Some animals apparently still see flicker until 70-100Hz.

     

    Because of this heightened sensitivity to flicker, a television program, in which the screen is updated 60 times/s and appears as a fluidly moving story line to most humans, may appear to rapidly flicker to dogs.

    http://redwood.berkeley.edu/bruno/animal-eyes/dog-vision-miller-murphy.pdf

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 8 years ago in reply to mcb1

    >..cats that are good hunters don't react to ... Tv

     

    My cats are terrible hunters, and they watch tv... the theory holds image

     

    They're pretty good at catching flies though...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • ntewinkel
    ntewinkel over 8 years ago in reply to mcb1

    >..cats that are good hunters don't react to ... Tv

     

    My cats are terrible hunters, and they watch tv... the theory holds image

     

    They're pretty good at catching flies though...