Programmable Logic
  • Challenges & Projects
  • Project14
  • Programmable Logic
  • More
  • Cancel
Programmable Logic
Blog MKR VIDOR 4000 Simple DVM
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Programmable Logic to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: rsc
  • Date Created: 16 Jul 2019 7:13 PM Date Created
  • Views 1141 views
  • Likes 5 likes
  • Comments 0 comments
  • programmablelogicch
  • mkr_vidor
Related
Recommended

MKR VIDOR 4000 Simple DVM

rsc
rsc
16 Jul 2019

Here's a simple DVM made from an Arduino VIDOR 4000.

A potentiometer is placed in between VCC and GND with the wiper connected to analog input A3.

The value of the analog input is read and then shown through the HDMI to a monitor screen.

The arduino example code for showing the Arduino logo was modified for this project.

Here is the code listing:

//MKR VIDOR 4000 Simple DVM
//R. Scott Coppersmith
//Last Edit 16July2019


#include "VidorGraphics.h"
#include "Vidor_GFX.h"


Vidor_GFX  vdgfx;
int analogPin = A3; // potentiometer wiper (middle terminal) connected to analog pin 3
                    // outside leads to ground and +5V
int val = 0;  // variable to store the value read
void setup() {
  // Initialize the FPGA
  if (!FPGA.begin()) {
    Serial.println("Initialization failed!");
    while (1) {}
  }


  delay(4000);
  // Fill the screen with a white background
  vdgfx.fillRect(0,0,640,480,vdgfx.White());


}


void loop()
{
  
  while (1) {
    delay(200);
    val = analogRead(analogPin);  // read the input pin
    vdgfx.fillRect(50,50,250,180,vdgfx.Yellow());
    vdgfx.text.setCursor(50,150);
    vdgfx.text.setAlpha(255);
    vdgfx.text.setSize(4);
    vdgfx.text.setColor(vdgfx.Blue());
    vdgfx.println(val);
  }
}

 

 

Video of operation:

https://www.element14.com/community/videos/29879

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

To convert counts (14-1023) to voltage (0.0 vdc to 3.3 vdc) change val from int to double and add this line of code after reading the analog input:

 

val = (val-14)*3.3/(1023-14); //convert to voltage 0-3.3vdc