Remote Monitoring & Control
  • Challenges & Projects
  • Project14
  • Remote Monitoring & Control
  • More
  • Cancel
Remote Monitoring & Control
Blog Smarthab: Remote Sensing and Control .iv  Software Design
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Remote Monitoring & Control to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 4 Jul 2019 3:40 PM Date Created
  • Views 1605 views
  • Likes 2 likes
  • Comments 1 comment
  • smarthab
  • remotemonitoringcontrolch
  • dht22
  • msp432 boostxl-k350qvg-s1 kentec_qvga_display
  • kentec_display
  • msp432
  • iot
  • smart thermostat
  • diy software
  • c progrmming
Related
Recommended

Smarthab: Remote Sensing and Control .iv  Software Design

phoenixcomm
phoenixcomm
4 Jul 2019

Ok, I have settled on the MSP-432 with the Kentec display. Out of the box the feature set is quite impressive:

  • 48MHz 32-bit ARM Cortex M4F with Floating Point Unit and DSP acceleration
  • Power consumption: 95uA/MHz active, and 850nA RTC standby operation
  • Analog: 24Ch 14-bit differential 1MSPS SAR ADC, Two Comparators
  • Digital: Advanced Encryption Standard (AES256) Accelerator, CRC, DMA, HW MPY32
  • Memory: 256KB Flash, 64KB RAM
  • Timers: 4x16-bit, and 2x32-bit
  • Communication: Up to 4 I2C, 8 SPI, 4 UART

What else do you need for less than 20 bucks? The price point is lower than an Arduino Mega!

So here is what I need for I/O:image

  • UART 1: Communications to the room controller.
  • UART 2: Communications to DHT22
  • I2C: Display
  • A few digital pins for the touch screen.

Now this is written in ANSI-C. So you should use the TI CSS (eclipse), and TI has a huge library of graphics primitives, and I/O library. I don't know is Sketch (Arduino like IDE) supports this board.

Most of the communications is between the DHT22 and the display, with commands like turn on the fans to the room controller. During various times a user will adjust the temperature or the humidity so this must come first, or as the highest priority for an interrupt.

There is also commands going to the thermostat from the room controller. For instance every minute the clock is updated by the room controller, from the network clock.

 

 

 

part iii

imageimage

 

part v

  • Sign in to reply
  • DAB
    DAB over 7 years ago

    I am curious about what type of additional applications you intend to run that would require the horsepower of the 432.

    If all you intend is UI and display I would say the 430 would be adequate, but it would limit you to any application needing more calculation or data driven responses.

     

    DAB