Products
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
RF Radio Frequency
  • Challenges & Projects
  • Project14
  • RF Radio Frequency
  • More
  • Cancel
RF Radio Frequency
Forum How to compute the required length and turns for a air cored antenna
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RF Radio Frequency to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Answers 2 answers
  • Subscribers 17 subscribers
  • Views 4181 views
  • Users 0 members are here
  • antenna design
  • radio receiver
Related

How to compute the required length and turns for a air cored antenna

obones
obones over 5 years ago

Hello,

 

While experimenting with various designs for the 433MHz antenna to be used with my RFM69 receiver, I stumbled across step by step instructions created by Ben Schueler in 2013 and republished a large number of times since then, such as here: https://arduinodiy.wordpress.com/2015/07/25/coil-loaded-433-mhz-antenna/

 

It works quite well for my application, but now I would like to dabble into the 868MHz range and I was wondering how I can calculate the appropriate dimensions/number of turns to replicate the above design, but tuned for 868MHz reception.

 

Would you have the link to a reference document so that I can compute it myself? Or should I just go ahead and divide every value by two as 868 is roughly 433 multiplied by two?

 

Thanks for any pointers.

  • Sign in to reply
  • Cancel

Top Replies

  • kmikemoo
    kmikemoo over 5 years ago +3 suggested
    obones Oh! Antenna building! I'm interested. First things first, shabaz is super smart and really knows his stuff, so I'd encourage listening to his advice. As a hobby antenna builder... yes, you can try…
  • shabaz
    shabaz over 5 years ago in reply to obones +2 verified
    Hi Olivier, I don't think there is a formula (or at least, not some single universal formula where you can plug in your desired frequency) for such an antenna. There are sets of formulas for the simple…
  • shabaz
    shabaz over 5 years ago +1 suggested
    Hi Olivier, You can just try a length of wire, roughly half, and snip bits off to experiment. It won't be able to be an optimum value, because each antenna has an impedance. The antenna that you're replacing…
Parents
  • shabaz
    0 shabaz over 5 years ago

    Hi Olivier,

     

    You can just try a length of wire, roughly half, and snip bits off to experiment.

    It won't be able to be an optimum value, because each antenna has an impedance. The antenna that you're replacing has an impedance, and the circuit board will have components on it to match the antenna. If you swap out with a different type of antenna then it is now unmatched to the board. Performing the matching requires a VNA and swapping out the matching components on the board with ones determined by using the VNA.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • obones
    0 obones over 5 years ago in reply to shabaz

    Hello,

    Thanks, but I already know the value for the basic "whip" 1/4 length monopole antenna.
    What I'm looking for here is a way to reproduce the design mentioned above which has a coil at is base, made from turns of the wire, which basically creates an inductor.
    Using the following website, I can estimate the inductor value: https://m0ukd.com/calculators/air-cored-inductor-calculator/

     

    But I could not find a way to compute the two lengths of straight wire.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 5 years ago in reply to obones

    Hi Olivier,

     

    I don't think there is a formula (or at least, not some single universal formula where you can plug in your desired frequency) for such an antenna. There are sets of formulas for the simple antennas (e.g. monopole, dipole, helix) and that's it. Anything else, and you're likely to either need to simulate, or try it out, or both.

    The link you have specified is not an antenna calculator, it's just an inductor calculator. By the way, the formula is not exact with real life, although it's close, and in practice you'll have to try it, and tweak it. You can't get away from experimentation at such frequency ranges.

     

    Also, as mentioned, if your board is not designed for that antenna, then there is the matching problem to solve too.

    For just a hobby antenna for an off-the-shelf low-cost module, I'm not sure it's worth all that effort/cost.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 5 years ago in reply to obones

    Hi Olivier,

     

    I don't think there is a formula (or at least, not some single universal formula where you can plug in your desired frequency) for such an antenna. There are sets of formulas for the simple antennas (e.g. monopole, dipole, helix) and that's it. Anything else, and you're likely to either need to simulate, or try it out, or both.

    The link you have specified is not an antenna calculator, it's just an inductor calculator. By the way, the formula is not exact with real life, although it's close, and in practice you'll have to try it, and tweak it. You can't get away from experimentation at such frequency ranges.

     

    Also, as mentioned, if your board is not designed for that antenna, then there is the matching problem to solve too.

    For just a hobby antenna for an off-the-shelf low-cost module, I'm not sure it's worth all that effort/cost.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • obones
    0 obones over 5 years ago in reply to shabaz

    Thanks for your answer, yes you are right that for a hobby project, it's not worth the effort and investment into a VNA. But I find it a bit sad that "trial and error" is the only viable option for hobbyist.