RFID or NFC
  • Challenges & Projects
  • Project14
  • RFID or NFC
  • More
  • Cancel
RFID or NFC
Project14: RFID or NFC Competition NFC powered high voltage generator / NFC field detector with neon lamp
  • Blog
  • Forum
  • Documents
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RFID or NFC to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: JWx
  • Date Created: 15 Dec 2022 3:07 PM Date Created
  • Views 48673 views
  • Likes 10 likes
  • Comments 2 comments
  • rfidornfcch
Related
Recommended

NFC powered high voltage generator / NFC field detector with neon lamp

JWx
JWx
15 Dec 2022

Ever wondered how much power can you get from NFC reader? It seems - a lot!

For me, first indication of this fact was this Discovery series kit form ST:

image

As can be seen, reader is powering tag circuit containing MCU, LCD display and some sensors, generating about 3.3V.

Second indication was some draft version of ISO-10373-6 (Identification cards - Test methods - Part 6: Proximity Cards), where test case for checking reader field strength was circuit of full-wave Schottky rectifier connected to the antenna, which was supposed to generate about 3V on 1.8kOhm resistor  - nice!

So - lets build something!

First test - antenna (about 8 turns of 0.3mm wire put inside plastic milk bottle cap - about 36mm diameter, ~4uH) - on photo below generating over 7V open-circuit through voltage doubling RF peak voltage probe:

image

Then some experiments using breadboard - not very repeatable because of capacitance coupling between contacts - to the level that about 1mA could be drawn when RF is connected not directly, but to the contact one row separated from the rest of circuit:

image

At this stage I was able to get several tens of volts open-circuit - so can we light a neon lamp?

Then first proper version was created (using RF modification of Dickson charge pump circuit):

image

This one was generating about 100V open-circuit - reverse voltage limit of 1N4148 diodes (previous pspice simulation hinted that better performance can be obtained from generic 1N4148 diodes than dedicated Schottky RF components - probably because of difference in  their forward impedance) but still too low to reliably light a neon bulb (retrofitted from screwdriver type mains detector rated for 125V+ voltage - 230V+ types have neon lamps with higher startup voltage which limits sensitivity).

So - we need another multiplication stage. After brief experimenting with "ultrafast" high voltage rectifiers - still too slow it seems, third stage was build using 500V capacitors and series connected 1n4148 pairs:

image

This one is generating about 170V open-circuit and works like this:
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
And here is schematics:

image

Assuming that input power is low, there is no overvoltage protection nor neon lamp current limiter - can be added as needed...

Final observation is that we cannot tune generic detector for given resonance frequency (which would result in increased sensitivity), because this frequency varies - some readers work at 13.56MHz (eg. NFC reader in authors's mobile phone), but for example ST reader from discovery kit seems to work at about 2MHz, so circuit tuned to 13.56MHz (using 27pF capacitor connected in parallel with antenna), which nicely detects signal from mobile phone is not working with this reader. Detection can be obtained by removing fine-tuning capacitor (as seen on schematics above).

  • Sign in to reply
  • JWx
    JWx over 3 years ago in reply to dougw

    It seems that second stage is indeed limited to around 100V - so third stage uses series connected diode pairs (didn't have switching diodes rated > 100V and high voltage/high speed rectifier diodes didn't work - probably they are still too slow [especially considering the fact that some tested readers seem to work on different frequencies than usual 13.56MHz - detector tuned for resonance at 13MHz is not detecting them, and removing tuning capacitor improves detection], so I decided to increase reverse voltage by connecting more diodes)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 3 years ago

    Usually 1n4148 diodes are rated around 100V but it looks like they are hanging in there.