RFID or NFC
  • Challenges & Projects
  • Project14
  • RFID or NFC
  • More
  • Cancel
RFID or NFC
Project14: RFID or NFC Competition PiBook Tracker : Blog #02-- Hardware setup and initial PN7120 driver testing
  • Blog
  • Forum
  • Documents
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RFID or NFC to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: flyingbean
  • Date Created: 22 Nov 2022 3:34 AM Date Created
  • Views 7489 views
  • Likes 7 likes
  • Comments 0 comments
  • rfidornfcch
  • nfc
Related
Recommended

PiBook Tracker : Blog #02-- Hardware setup and initial PN7120 driver testing

flyingbean
flyingbean
22 Nov 2022

 I am going to demonstrate how to use PN7120/ with NTAG215 in this blog.

I ordered NTAG215 chips from eBay and received them this week. It is time to set up the hardware on my bench now. I followed the instructions (Ref[4])from NXP community to setup the platform PN7210 controller on a Raspberry Pi 3B as below:

image

Step #01: Setup Rasbian and I2C port on Raspberry Pi 3B. If you are very familiar with Rasbian, please skip this step

a. Visiting Rasberry Pi OS website: https://www.raspberrypi.com/software/

Download Raspberry Pi Imager for Windows 10: I downloaded imager_1.7.3.exe.

After I installed imager_1.7.3.exe, I selected Raspberry Pi OS(32-bit) and SDHC card to generate a Rasbian SD card.

image

It takes about 5 minutes to create a Rasbian SD card.

b. Install Rasbian from the SD card

Run “sudo raspi-config” and select “3 Interface Options” as below:

image

The snapshot telling me that my Raspberry Pi hardware version is Raspberry Pi 3 Model B Plus Rev1.3.

Then select “I5 I2C …”

image

Select “Yes” from this pop-up menu to confirm that I2C interface on Raspberry Pi is populated.

image

After selecting I2C interface, use right arrow to select <Finish> button. Finally reboot Raspberry Pi.

Verify I2C interface from Raspbian OS with the command

$ ls /dev/*i2c*

Step #02: Running out-of-box PN7120 applications

a. Install tools for PN7210 driver on Raspberry Pi

$ sudo apt-get install autoconf automake libtool git

image

b. Clone NXP PN7120 from NXP Github

$ git clone https://github.com/NXPNFCLinux/linux_libnfc-nci.git

image

c. Configure the library

$ cd linux_libnfc-nci

$ ./bootstrap

$ ./configure –enable-alt

image

d. Build and install the library

Execute the commands (take up to 5 minutes to build libraries)

$ make

$ sudo make install

$ export LD_LIBRARY_PATH=/usr/local/lib

image

Step #03: Testing eBay NTAG215 chips

Run demo application in poll mode executing the command:

$ nfcDemoApp poll

 imageimage

 

It looks the PN7120 controller working as expected on Raspberry Pi platform now. My next step is to use Python to call NXP PN7210 driver which will pave the path for building  PiBook Tracker software frame work.

Appendix #01:  NTAG215 NFC PVB Coins Chip from eBay:

 image

Ref[1]: https://www.nxp.com/products/rfid-nfc/nfc-hf/nfc-readers/nfc-controller-with-integrated-firmware-and-nci-interface-for-home-appliances:PN7120

Ref[2]: https://www.nxp.com/products/rfid-nfc/nfc-hf/ntag-for-tags-labels/ntag-213-215-216-nfc-forum-type-2-tag-compliant-ic-with-144-504-888-bytes-user-memory:NTAG213_215_216

Ref[3]: https://www.nxp.com/design/training/nfc-use-cases:TIP-NFC-USE-CASES

Ref[4]: https://community.nxp.com/t5/NXP-Designs-Knowledge-Base/Easy-set-up-of-NFC-on-Raspberry-Pi/ta-p/1099034