Robots with Wheels
  • Challenges & Projects
  • Project14
  • Robots with Wheels
  • More
  • Cancel
Robots with Wheels
Blog RoboBobLet #2 : The Basic Chassis
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robots with Wheels to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dubbie
  • Date Created: 29 Mar 2018 3:57 PM Date Created
  • Views 1898 views
  • Likes 9 likes
  • Comments 4 comments
  • roboboblet
  • robotwheelsch
Related
Recommended

RoboBobLet #2 : The Basic Chassis

dubbie
dubbie
29 Mar 2018
image

Robots with Wheels

Enter Your Electronics & Design Project for Your Chance to Win a $100 Shopping Cart!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

I decided to use a fairly common chassis from feetechrc (www.feetechrc.com) FT-MC-003 available from several distributors as it provides the four continuous rotation servo motors as well as the wheels and rubber types, plus the chassis which all fit together nicely, albeit a bit fiddly. The photograph should show the chassis with the Arduino Nano mounted onto a piece of strip board to allow connectors to be used instead of soldering the motors. I used a Nano as it is low cost and has everything needed (at the moment anyway). Power is provided by the 4 x AA battery pack which also has an ON/OFF switch. I am only using the motors in full speed mode(forwards and backwards) at the moment. It takes a bit of fiddling around to get all the motors moving in the correct directions as none of the datasheets seem to show which direction the motors rotate for different pulse widths.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The YouTube video at https://www.youtube.com/watch?v=N_mAkRxrT_k&feature=youtu.be  shows the chassis just moving forwards and backwards for 1 second periods. When the chassis changes from backwards to forwards it rears up due to the momentum and the centre of gravity being nearer the back due to the battery pack position. It might be necessary to change the battery pack position if this becomes a problem. At the moment any problems will be overcome via software. There is some problem as can be seen in the YouTube video that after a few cycles it suddenly stops and then restarts. This isn't programmed so I think that this is a power dip caused by motor in-rush currents when changing direction that is resetting the Nano. I hope to fix this in the software otherwise a separate power pack for the Nano might be needed. At the end of the YouTube you can see the advantage of four wheel drive as the chassis climbs over my obstacle strewn desk without any problems.

 

Next a Bluetooth link will be used to provide manual control of the chassis hopefully via a smart phone.image

  • Sign in to reply

Top Comments

  • genebren
    genebren over 8 years ago +2
    Great update on your robot project. That robot really wanted to rearrange your workbench a bit. Keep up the great work! Gene
  • three-phase
    three-phase over 8 years ago +1
    Cool little robot, look forward to the updates on the control. Kind regards
  • mcb1
    mcb1 over 8 years ago +1
    Nice start. It appears that you're feeding the battery pack straight to the 5v input on the Nano?? I'm also thinking that you have a 5v Nano rather than the 3v3 versions. AA batteries are usually 1.5v…
Parents
  • genebren
    genebren over 8 years ago

    Great update on your robot project.  That robot really wanted to rearrange your workbench a bit.  Keep up the great work!

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • genebren
    genebren over 8 years ago

    Great update on your robot project.  That robot really wanted to rearrange your workbench a bit.  Keep up the great work!

    Gene