Can I use both secondary windings to power separate loads?
I have a need for two 4.5VAC power supplies.
I have a transformer that is 9VAC with a center tap. I would like to connect one load to one 4.5VAC O/P and the other load to the other 4.5VAC. I'm assuming I can do this, provided I don't exceed the max current rating. It has been a long time since I have dabbled this low in analogue. I was looking for some reassurance or refresher.