• Products and Partners
    Products and Partners
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
Solar Power Devices
  • Challenges & Projects
  • Project14
  • Solar Power Devices
  • More
  • Cancel
Solar Power Devices
Blog Solar System Description
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Solar Power Devices to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ralphjy
  • Date Created: 2 Aug 2018 6:01 AM Date Created
  • Views 1756 views
  • Likes 7 likes
  • Comments 4 comments
  • solar panel
  • solarpwrdevicesch
  • solar inverter
Related
Recommended

Solar System Description

ralphjy
ralphjy
2 Aug 2018
image

Solar Power Devices

Enter Your Electronics & Design Project for Your Chance to Win a Grand Prize for the most inspiring project or a $100 Shopping Cart!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

I thought that as I contemplate my project design that I'd use this blog post to provide a brief description of my solar PV system that I will be monitoring.

 

System Tradeoffs

As I mentioned in the earlier post, I wanted a system that generates 5 MWHrs per year at the lowest possible cost.  I was willing to sacrifice some performance and features but not quality and reliability.  I had some physical constraints that I had to accommodate - the usable roof area, the roof pitch, roof orientation, and possible shadowing.  My house unfortunately was not designed with any consideration for solar.  I have a kind of chopped up rooftop (multiple planes) that's common in my neighborhood.  I have usable surfaces that face directly south and west.   My roof pitch is 40 degrees, so for Oregon it's probably best to have a south facing installation.  I had space for 18 panels (nominally 3'x5') in a somewhat convoluted configuration to accommodate the roof geometry, a skylight, and vent pipes.

 

List of tradeoffs

1)  Module type - I chose to use an older generation module in order get lower pricing.  I am using American made Solar World Protect Mono Black 285W panels.  This monocrystalline panel has an efficiency of 17% and has a 30 year linear performance guarantee (maintains 86% of output capacity).  I could have used newer 300W+ panels which have higher energy densities and higher efficiency at a higher cost.  A solar survey indicated that I would need 16 panels to meet my energy requirement using only south facing panels..

2)  Inverter type - I chose to use a string inverter rather than more efficient micro inverters, again for cost reasons.  Using micro inverters requires that you have an inverter per panel.  This gains a lot of efficiency because you have power point tracking per panel and panels are essentially independent so you are more resistant to performance degradation due to shadowing or defective panels.  Another difference with micro inverters is that you have AC power distribution rather than DC from the panel.  I am using an SMA Sunny Boy 4000TL-US inverter.  This is a 4200W grid-tie transformerless string inverter.  It can accommodate 4 panel strings but only has 2 independent MPP (Maximum Power Point) trackers.

3)  Connectivity - The inverter model that I selected included a optional Webconnect module, but it was only available in wired Ethernet although newer models are available with WiFi capability.

4)  Orientation - Because I had 2 MPP trackers available I could have configured a west facing and a south facing string to try to optimize the array performance during seasonal variations.  Since the design simulation indicated that I would have some annualized power margin with only a south facing array, I decided to do that to ease the installation effort and cost.

 

image

 

Final Configuration

As the picture above shows, I installed 18 south facing panels configured in 2 strings of 9 panels each.  That gives me a spec capacity of 5130 W (this is under "optimum" conditions: 1000 W/m^2, 25C).  We used a 4200 W inverter because in reality that power level is only exceeded for short periods of time and the inverter just "clips" during those intervals.  Each string with modules at MPP is around 279V @ 9.2A.

 

I used my Tello drone to take the picture.

  • Sign in to reply

Top Comments

  • DAB
    DAB over 8 years ago +1
    It will be interesting to see what you really achieve with your installation. DAB
  • gio60
    gio60 over 8 years ago +1
    Congratulations, very interesting ! Can you give us an idea about costs ?
  • ralphjy
    ralphjy over 8 years ago in reply to gio60 +1
    Solar system costs are highly variable depending on the constraints. so it's probably best to make trade-offs for a given installation. That being said, the average cost of a solar system in Oregon is…
Parents
  • gio60
    gio60 over 8 years ago

    Congratulations, very interesting ! Can you give us an idea about costs ?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • gio60
    gio60 over 8 years ago

    Congratulations, very interesting ! Can you give us an idea about costs ?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • ralphjy
    ralphjy over 8 years ago in reply to gio60

    Solar system costs are highly variable depending on the constraints. so it's probably best to make trade-offs for a given installation.  That being said, the average cost of a solar system in Oregon is currently about $3.40/watt for a 5kW system like mine (before applying incentives).  I have a reasonable pitch on my roof (~40 degrees), so my installation cost was higher than the cost of the solar equipment.  Based on the trade-offs that I made, the cost of my solar equipment (panels, inverter, racking, web connect) was a little over $1/watt.  After solar incentives (rebates, tax credits), my installed cost was under $3k.