• Products and Partners
    Products and Partners
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
Solar Powered Yard Gadget
  • Challenges & Projects
  • Project14
  • Solar Powered Yard Gadget
  • More
  • Cancel
Solar Powered Yard Gadget
Blog Upcycled Wireless Sensor Accent Light, Part 2
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Solar Powered Yard Gadget to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: pettitda
  • Date Created: 24 Sep 2017 12:36 AM Date Created
  • Views 1035 views
  • Likes 4 likes
  • Comments 1 comment
  • solaryardgadgetch
Related
Recommended

Upcycled Wireless Sensor Accent Light, Part 2

pettitda
pettitda
24 Sep 2017

Testing the solar panel

 

The next step in my project was to test the solar panel to see exactly how much power I could get out of it.  To do this, I set up a variable resistor load on the output of the solar panel.  Additionally, I used a small resistor in series with the load to measure the current being supplied by the panel.  Here's a quick schematic of the setup:

 

image

And here's a picture of the circuit (without the meters):

 

image

 

I took this setup outside and measured it under a couple of conditions, cloudy day and sunny day.  I used Fluke Series 85V DMMs for the voltage measurements.  The one across the 10 ohm current sense resistor is set to mV range to record the voltage across the resistor.  The meter across the 100K potentiometer is set to measure in Volts.  Here's a graph of the recorded data for these conditions:

 

image

 

image

 

So, it looks like I can get about 7mW out of this panel on a cloudy day and about 55mW out of it on a sunny day.  To maximize the power from the solar cell, it looks like I need to keep the load voltage in the 1.7V range.  However, it looks like anything in the range of 1 to 2 Volts would be reasonable.

 

Next, I will determine how to use this solar panel to charge a supercap so that I can store that energy for reporting the sensor readings on a regular basis.  Stay tuned...

  • Sign in to reply

Top Comments

  • DAB
    DAB over 9 years ago +3
    Nice post. One of the things I always wanted to know about solar cells was just how effective are they when charging batteries or supercaps. I know about the Maximum Power Point and all of the fancy graphs…
Parents
  • DAB
    DAB over 9 years ago

    Nice post.

     

    One of the things I always wanted to know about solar cells was just how effective are they when charging batteries or supercaps.

     

    I know about the Maximum Power Point and all of the fancy graphs, but what I really would like to know is just how efficient are they when charging batteries?

     

    Just because you can pull 48mW of power out of a cell does not mean you can put 48mW into a battery.

     

    Could be a fun exercise to run.  As David Jones recently showed in one of his videos, there is a big difference between Power output and Energy output.

     

    DAB

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 9 years ago

    Nice post.

     

    One of the things I always wanted to know about solar cells was just how effective are they when charging batteries or supercaps.

     

    I know about the Maximum Power Point and all of the fancy graphs, but what I really would like to know is just how efficient are they when charging batteries?

     

    Just because you can pull 48mW of power out of a cell does not mean you can put 48mW into a battery.

     

    Could be a fun exercise to run.  As David Jones recently showed in one of his videos, there is a big difference between Power output and Energy output.

     

    DAB

    • Cancel
    • Vote Up +3 Vote Down