Sub -1 GHz Band
  • Challenges & Projects
  • Project14
  • Sub -1 GHz Band
  • More
  • Cancel
Sub -1 GHz Band
Blog Project14 | Sub-1GHz Band Challenge - Radio_On
  • Blog
  • Forum
  • Documents
  • Files
  • Leaderboard
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sub -1 GHz Band to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: rsc
  • Date Created: 22 Sep 2023 3:03 PM Date Created
  • Views 3137 views
  • Likes 10 likes
  • Comments 5 comments
  • STM32WL55
  • NUCLEO-WL55JC1
  • Sub-1 GHz Band
  • NUCLEO-WL55JC2
  • amateur radio
Related
Recommended

Project14 | Sub-1GHz Band Challenge - Radio_On

rsc
rsc
22 Sep 2023

My plan is to develop a Ham Radio Fox like this one by @kmikemoo using the Nucleo-STM32WL55 board.  My first blog was the unboxing and running of the demo software for the Nucleo-STM32WL55JC1. 

 Project14 | Sub-1GHz Band Challenge - Unboxing and running demo programs 

My first issue was that the JC1 option is RF optimized for 865MHz ~ 928MHz and I needed the JC2 version optimized for

433MHz to 510MHz, so I ordered two JC2 version boards.

 The Frugal Fox 

After finding only the blinky and Lorawan project code for mbed Studio, I switched over to STM32CubeIDE and found the STM32CubeWL set of examples to play with.

https://www.st.com/en/development-tools/stm32cubeide.html

image

https://github.com/STMicroelectronics/STM32CubeWL/tree/main/Projects/B-WL5M-SUBG1/Examples/BSP/BSP_Example/Src

After some get acquainted time with the new programming software, I managed to import and compile the examples for the Nucleo board in the STM32CubeIDE workspace.

 The example I started with is called SubGHz_Phy_Per and is used to determine Packet Error Rates (PER) between two radios.

There are some configuration changes to make to the code for the RX board and the TX board software. 

In subghz_phy_app.c the variable to determine the RX board from the TX board is:

#define TEST_MODE RADIO_TX (or RADIO_RX)

image

In the file subghz_phy_app.h the variable RF_FREQUENCY I set for 433.000 MHz for use in the 70cm ham radio band.

image

I flashed both the RX and TX boards and tested the configuration along with a spectrum analyzer and handheld ham transceiver set to 433.000.

image

image

The UART connections let me verify that the radios were transmitting and receiving packets correctly. 

image

The following videos show the RF transmitted pulse on the spectrum analyzer at 433.000 MHz and the blue LED on the TX board is in sync with the red LED on the RX board.
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
The ham radio received a short blip when the VFO is set to AM mode on 433 MHz.  The example software is selectable between LoRa and FSK modes, however, I need to transmit something that the FOX-Hunters can "hear" based on AFSK or "Audio-Frequency-Shift-Keying"  So net next task is to format some FSK data that can be heard on the air.

Stay tuned to this channel.....

Scott

  • Sign in to reply
  • DAB
    DAB over 3 years ago

    Nice update.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kmikemoo
    kmikemoo over 3 years ago

    rsc  Like javagoza , I'm looking forward to what you figure out.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • javagoza
    javagoza over 3 years ago in reply to scottiebabe

    Looking forward to getting there to undo several points and see what happens to the Verint system.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to javagoza

    You're about to crossover into the 6-figure points category congrats! Tada

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • javagoza
    javagoza over 3 years ago

    Wow, it looks like you're going to have a lot of fun with your project too. Luck! Eager to see the progress and learn more.