Test Instrumentation
  • Challenges & Projects
  • Project14
  • Test Instrumentation
  • More
  • Cancel
Test Instrumentation
Blog Automated Cable Test System .. part 4
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test Instrumentation to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 5 Nov 2018 5:36 AM Date Created
  • Views 2268 views
  • Likes 3 likes
  • Comments 0 comments
  • software development
  • vme
  • hardware plan
  • vmicvme-7648
  • cable tester
  • diy electronics
  • diytestinstruch
  • diy test equipment
Related
Recommended

Automated Cable Test System .. part 4

phoenixcomm
phoenixcomm
5 Nov 2018

Ok, so the work continues on three fronts.

  • BBC microbit no guts no glory. Underpowered, Lack of any real I/O, Banana Plugs that don't fit into the holes - Almost Trash.
  • Arduino, found the code, for a self-contained cable tester, but has no flying probe and no easy configuration changes.
  • VME possibility of a finished client.
    • Trying to decide to run Intel or Sun Sparc.
    • Found a Zycom DID 6U board with 64 bits of random  Digital I/O, Rotec gmbh seems like they just want to ignore me. Maybe I' ll go away.
    • have a Disk drive solved with some choices.
      • PMC Module (on Intel CPU) for IDE
      • SCSI-2 controler.
  • Host software. with nice GUI.

Results so far.

  • For the BBC micro bit, I have two (2) 16-bit I2c expanders.
  • For the Arduino between native I/O and the two (2) 16-bit I2c expanders I can do two (2) DB-25 Connectors, plus a dedicated flying probe.
  • For the VME System, I have the following working components.
    • Intel:
      • CPU, P3: VMICVME-7648 (VME-64) with 32bit 128Mb Compact Flash, 512Mb PC-133 Dram, 2x 100Mb Ethernet, 2x USB, VGA, PS2 Mouse/Keyboard Port.  Has room for a PMC module. I did not fully test this with video and keyboard (next step)
      • PMC IDE Module: RAMIXPMC235 with IDE connector in the front panel.
    • Sparc:
      • Force Sparc: CPU-1E/16
      • Force Sparc: CPU-2CE, 40Mhz, KBD, Mouse, (2) serial, (2) S-bus ports, SCSI-2, Network Interface. (needs repair: Front panel missing, Reset and Abort switches will have to be replaced as well as a new micro-D Network Interface.
    • Common Boards:
      • Zycom DIO: XVME-240, 64 bits random I/O + 8 interrupt lines + 8 flag lines
      • Rotec gmbh: DIG32-IS & DIG32-OK I have four (4) each of these cards they seem to be in working order but without any documents to guide me, I will be a long-term solution. As I will have 2x 4 x 32 = 256 pins of I/O (will require bus probes) image

For the time being it looks like I will go with the P3 CPU as it is not a big hill to climb.

 

Back to the Monthly Index