Test Instrumentation
  • Challenges & Projects
  • Project14
  • Test Instrumentation
  • More
  • Cancel
Test Instrumentation
Blog Automated Cable Test System .. part 7
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test Instrumentation to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 18 Dec 2018 2:47 AM Date Created
  • Views 1818 views
  • Likes 6 likes
  • Comments 0 comments
  • software design
  • automated
  • vme
  • cable tester
  • diy electronics
Related
Recommended

Automated Cable Test System .. part 7

phoenixcomm
phoenixcomm
18 Dec 2018
image

Test Instrumentation

Enter Your Electronics & Design Project for a chance to win a Grand Prize for Originality, a Tool Set, and a $100 Shopping Cart!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

The CPU specs are:
  • PentiumRegistered III FC-PGA/PGA2 socket processor-based single board computer (SBC) with 133 MHz system bus
  • 1.26 GHz Pentium III processor with 256 Kbyte advanced  transfer cache or 933 MHz Pentium III processor
  • 512 Mbyte PC-133 SDRAM using a single SODIMM
  • Internal AGP SVGA controller with 4 Mbyte display cache 133 MHz system bus via IntelRegistered 815E chipset
  • Dual Ethernet controllers supporting 10BaseT and 100BaseTX interfaces
  • Onboard Ultra DMA/100 hard drive and floppy drive controllers (uses VMEbus P2 for connection to IDE/floppy)
  • Two high performance 16550-compatible serial ports
  • PS/2-style keyboard and mouse ports on the front panel
  • Real-time clock and miniature speaker included
  • Dual front panel universal serial bus (USB) connections
  • Two 16-bit and two 32-bit programmable timers
  • PMC expansion site (IEEE-P1386 common mezzanine card
  • VME64 modes supported:

This is just a quick update for ACTS. I have had some help today to move some of the heavy stuff around for me. I have a torn rotator in my left shoulder, so picking up more than a pound or two kills me. The SBC module is a VMIC VMIVME-7648 P3 and it is up and running in its new home my large VME rack. So this card has 640k+128K = 192k of real memory but it will take 512k + 256 Cache SRAM. So I know the CPU is working and it runs preboot diagnostics fine, as you can see below. And it cries when it can't find the OS!

Now that I can talk to the SBC is to get an IDE HDA on it and load an OS. There are some Linux distros that will work with these small resources.

imageimage
imageimage