• Products and Partners
    Products and Partners
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
The World in Motion
  • Challenges & Projects
  • Project14
  • The World in Motion
  • More
  • Cancel
The World in Motion
Blog Pulse Width Modulation a Speed Equalizer(4): Theory at the bench
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join The World in Motion to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: colporteur
  • Date Created: 30 Jul 2022 9:12 PM Date Created
  • Views 2264 views
  • Likes 8 likes
  • Comments 6 comments
  • motor projects
  • worldinmotionch
  • pwm
Related
Recommended

Pulse Width Modulation a Speed Equalizer(4): Theory at the bench

colporteur
colporteur
30 Jul 2022

The third blog installment for this challenge presented the theory for pulse width modulation. The post talked about the concept of duty cycle and provided static waveform drawings to reinforce the concept. This post further enforces the PWM theory by providing a bench demonstration of the operation using some basic Arduino code and an oscilloscope.

The L298N driver library for the Arduino supports a method of setting the speed of a motor.
The speed range is from 0 to 255.

  // Change speed
  motor.setSpeed(45);

Three different speed values were tested 45, 127 & 254. An oscilloscope sample was taken at each value.

The oscilloscope was attached to the Arduino output that produces the PWM signal to the L298N module.

As the value in the code changed so did the width of the pulse change as seen on the oscilloscope. As the value in the code changed so did the duty cycle of the waveform change. As the value in the code changed so does the motor speed change.

{gallery}Oscilloscope PWM Outputs

image

setSpeed(45): 17% duty cycle

image

setSpeed(127): 49% duty cycle

image

setSpeed(254): 99% duty cycle

 

The value of 45 in the code was the first entry that resulted in any movement for the motor. The value of 127 is half of the maximum value of 255. The value of 254 is the maximum that could be set and the oscilloscope still displays the waveform. This testing was done with a 12VDC motor. The code value to establish the required train speed will need to be determined on the track.

Well, that completes the bench work. I'm reasonably confident I have everything that I need to now start testing with a locomotive.

  • Sign in to reply
  • shabaz
    shabaz over 4 years ago

    Hi Sean,

    Maybe it's unnecessary, although a future luxury add-on could be an encoder, and then the speed can be controlled down to (say) very slow settings, with no motor stalls. I don't know if that's needed or not, or even if such a thing is possible to retrofit to train motors. fmilburn has some Arduino code for it here in case it gives ideas: /products/arduino/b/blog/posts/simple-arduino-dc-motor-control-with-encoder-part-1

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<