• Products and Partners
    Products and Partners
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
The World in Motion
  • Challenges & Projects
  • Project14
  • The World in Motion
  • More
  • Cancel
The World in Motion
Blog Pulse Width Modulation a Speed Equalizer(5): The plan didn't survive first contact.
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join The World in Motion to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: colporteur
  • Date Created: 31 Jul 2022 9:55 PM Date Created
  • Views 2867 views
  • Likes 6 likes
  • Comments 10 comments
  • motor projects
  • worldinmotionch
  • pwm
Related
Recommended

Pulse Width Modulation a Speed Equalizer(5): The plan didn't survive first contact.

colporteur
colporteur
31 Jul 2022

I did the first field tests with a HO scale locomotive today with limited success. The locomotive speed was controllable by using PWM but the whine from the motor is not acceptable for operational use.

In 1871 Prussian Field Marshal Helmuth von Moltke the Elder wrote an essay about military strategy. The following is an English translation, "No plan of operations extends with any certainty beyond the first encounter with the main enemy forces. Only the layman believes that in the course of a campaign he sees the consistent implementation of an original thought that has been considered in advance in every detail and retained to the end."

It appears I am the layman in Moltke's quote. The motor used for bench testing was not a locomotive motor but rather a 12VDC surplus motor. It did produce a whine during testing but only at a lower speed. I never gave it much thought. The locomotive motor when powered from PWM whines at all speeds. In addition, the maximum speed is slower with PWM than with the train power supply. Looking online, there are some examples of PWM producing a whine when used to power a motor. 

My first thought was the PWM frequency. Could a higher PWM frequency eliminate the whine?

The default PWM frequency for pin 3 ( pin used for PWM) is 490 Hz. Pin 4 has a default frequency of 980Hz. Using the PWM signal from pin 4 eliminated the whine with a loss of speed control. Using a speed code value of 127 the locomotive didn't move. At a value of 128, the locomotive moved at maximum speed. On the lower PWM frequency, (I can't recall the speed values) there was a greater range of control. I could get a slow speed as well as a top speed but with the whine.

This first contact's poor success has given me cause to make some changes. For any further bench testing, I will be using a locomotive motor and not my bench surplus motor. Initial google search suggests PWM frequency changes from defaults are possible but don't appear to support a frequency between 490Hz and 980Hz. I have yet to garner an understanding of why using the 980Hz frequency results in a loss of speed control.

I thought my plan was sound but it appears to need some tuning. Maybe a different motor driver module is required? Would a filter cap on the module output help? I'm not sure at the moment. I'm open to suggestions as I bandage my wounds and prepare for another attempt.

  • Sign in to reply

Top Comments

  • robogary
    robogary over 4 years ago +1
    Industrial AC & DC motor drives have a similar issue. I can also hear the whine of an electric vehicle H bridge. Those controls have features to change the switching frequency to adjust audible noise,…
  • colporteur
    colporteur over 4 years ago +1
    Error on my part. The website that reference pin 4 as 980Hz is wrong! Looking at the spec sheet pin 4 doesn't support PWM it is pin 5 that is PWM at 980Hz. Something I will need to investigate.
Parents
  • robogary
    robogary over 4 years ago

    Industrial AC & DC motor drives have a similar issue. I can also hear the whine of an electric vehicle H bridge. Those controls have features to change the switching frequency to adjust audible noise, and also putting a slight ramp on the H bridge switch when it fires to get rid of that nasty switch on step.AC output filters also help with that issue.There are also possibilities to hit some electrical resonance frequency of the switching and inductance/capacitance. A couple ideas:   1) A Raspberry Pi Pico has more flexibility for setting PWM frequency, some projects are a good fit to leverage that flexibility.. 2) I will "cheat" sometimes by doing a digitalWrite = true or false with the timing of a duty cycle desired rather than implementing PWM. It does a good job of wasting compute power but it can be used to experiment and study behaviors..  3) You could try adding a clamp on ferrite core to the H bridge + output lead https://en.wikipedia.org/wiki/Ferrite_core and an RC filter on the output to smooth out the current zipping thru the motor. If you have a spare transformer laying around, run the DC output thru one of the low impedance windings in series just to see if adding inductance helps the problem. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • robogary
    robogary over 4 years ago

    Industrial AC & DC motor drives have a similar issue. I can also hear the whine of an electric vehicle H bridge. Those controls have features to change the switching frequency to adjust audible noise, and also putting a slight ramp on the H bridge switch when it fires to get rid of that nasty switch on step.AC output filters also help with that issue.There are also possibilities to hit some electrical resonance frequency of the switching and inductance/capacitance. A couple ideas:   1) A Raspberry Pi Pico has more flexibility for setting PWM frequency, some projects are a good fit to leverage that flexibility.. 2) I will "cheat" sometimes by doing a digitalWrite = true or false with the timing of a duty cycle desired rather than implementing PWM. It does a good job of wasting compute power but it can be used to experiment and study behaviors..  3) You could try adding a clamp on ferrite core to the H bridge + output lead https://en.wikipedia.org/wiki/Ferrite_core and an RC filter on the output to smooth out the current zipping thru the motor. If you have a spare transformer laying around, run the DC output thru one of the low impedance windings in series just to see if adding inductance helps the problem. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • colporteur
    colporteur over 4 years ago in reply to robogary

    Much appreciate you sharing your insight. I worked with guys that did only motors. There experience was extremely valuable when it came to troubleshooting. My electronics were general. A little bit of everything.

    My test today generated a number of questions that didn't come up on testing from a bench breadboard. This is good. I rather discover them now than after it is installed.

    I just discovered not all locomotive engines are the same. The bench locomotive I am using now as a replacement for the surplus motor doesn't whine.

    I also discovered a pin error in the documentation I used on the internet. CRAP!

    Examining the train power supply it has a switch labeled pulse. It is typically off. I asked the guys if the switch would be for locomotives that support PWM. They looked at me and said, "what is PWM?" I may need to scope the supply output to answer my question.

    I'm investigating if it is train motor-related or something else. Lots of variables:(

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • colporteur
    colporteur over 4 years ago in reply to robogary

    A novice question robo. Is there an ideal PWM frequency for a motor? I'm curious if the 490 vs 980 Hz will make a difference. Once I got the pin assignment correct yes 980Hz does work to control the motor speed.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • robogary
    robogary over 4 years ago in reply to colporteur

    That is a PH.D. question about ideal PWM freq. There are so many kinds and sizes of permanent magnet DC hobby motors, it also depends how they are used. You also have some unique variables, one is called a track. The track is a variable inductor from the point of coupling until it hits the motor. You may be dealing with some voltage drop too from the wheels /pickupsand track connections.  Dirty spots may bite you too.  You could also watch the track volts with a digital voltmeter to look for something fishy and a second DVM watching the load current.   ( for example today I was testing stepper motors for the Twist Design Challenge, one was acting weird. The scope traces looked really weird too. Finally figured out one step coil was open circuit.) 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • colporteur
    colporteur over 4 years ago in reply to robogary

    Way above my formal education! I thought maybe there was a rule of thumb. I did scope the PCM pins of the Nano and determine what frequency is used by default. That led me to knowledge that fills some gaps in servo motor operation. I can take that memory post-it note down, now that I have the answer.

    As I expected, a response from a model railroader confirms whine in motors occurs but it is usually with older motors. He referred to three pole motor verse four and five poles. The railroad has a collection of motors. I'm going to do some comparisons to see what I can discover.

    I will try the alternate PWM frequency tomorrow at the site on the motor that whines. I'm curious if the whine differs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • robogary
    robogary over 4 years ago in reply to colporteur

    I wonder if the track platform acts like a piano soundboard   :-)