The World in Motion
  • Challenges & Projects
  • Project14
  • The World in Motion
  • More
  • Cancel
The World in Motion
Blog Remote Monitoring and controlling motor using open source IoT platform
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join The World in Motion to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: balajivan1995
  • Date Created: 22 Sep 2022 4:00 PM Date Created
  • Views 2681 views
  • Likes 6 likes
  • Comments 2 comments
  • motor projects
  • worldinmotionch
  • motors
Related
Recommended

Remote Monitoring and controlling motor using open source IoT platform

balajivan1995
balajivan1995
22 Sep 2022
Remote Monitoring and controlling motor using open source IoT platform

Summary

As a part of my predictive maintenance exercises, I have started using motor usage to collect data and to perform anomaly detection. As a first step, I have decided to release a simple version of data generator using motor. Motor will be controlled by ESP32 MCU, which will receive commands from Thingsboard server. The forward/backward/resting position along with speed set will be recorded and saved in postgresDB. The code and dashboard template are available in GitHub repository. I am really excited to present my current project as an entry for world in motion contest. Hope you all will like it.

Hardware requirement

  • L293D motor driver
  • DC gear motor
  • ESP32 (I have used ESP wroom32)
  • Jumper cables
  • breadboard

Software requirement

  • Arduino IDE
  • Thingsboard server (self-hosted or use trial version        

Connection

               ESP32    L293D    MOTOR

               18            IN1                       

               19            IN2                       

               4              ENA        ENA

                               OUT1     M+

                               OUT2     M-

Creating a device in Thingsboard

  • Log into your thingsboard account. On left side, you’ll “Devices” option. Select that option.
  • Click the “+” on right side to create a new device. Give it a name and select “Credentials”.
  • Enter a non-easily recognisable password and make sure to note it down somewhere safe. Once done, click “add”.

Creating a dashboard

  • On left side, select “Dashboards”. Import the json file available in GitHub repository.
  • Once imported make sure to replace the device ID with the one you have created by editing the widgets.

Programming the ESP32 MCU

  • Install the ESP32 package for Arduino.
  • Install ThingsBoard & arduinojson library through library manager.
  • Open the file provided in the GitHub repo.
  • Replace the SSID, password, server IP and device credentials in config.h to match yours.
  • Select the board according to your MCU and upload the code

Video Demonstration

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Data generation

  • On the dashboard you’ll greeted with multiple widgets. Use the knob widget to set the speed. Backward/Forward/halt are self-explanatory. The charts will show the state diagram of motor at a time and the chart below will show you the speed set at that time.
  • Control the motor using the widgets, the data will be automatically stored into postgresdb available by default in thingsboard server.

To be implemented

  • Attach vibration sensor to pick up vibration caused by motor - especially whenever the state changes.
  • The alarm widget is a placeholder for now. Severity of alarm will be calculated; alerts will be generated. Email will be sent to user when motor speed exceeds threshold.
  •  Perform analytics on the sensor data

Notes

  • This blog is meant to be a basic intro to a multi part series. Currently the data is generated by manually pressing the widgets. In subsequent blogs, motor will be attached with a load and will be automated to move forward/backward.
  • Few more parameters need to be incorporated to provide reliable analytics.

                             

PS: If you guys know a way to measure DC motor speed using microcontroller (With and without load), please let me know.

Will meet you guys on next blog without updated version! Toodles!!

  • Sign in to reply
  • balajivan1995
    balajivan1995 over 4 years ago in reply to robogary

    Can I use the one in mouse?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • robogary
    robogary over 4 years ago

    One way to measure speed is with a slotted wheel on the motor shaft, an LED to shine thru it, and a light detector to see the light.. Here is just one example to get you started. https://bc-robotics.com/product-category/robotics/wheel-encoders/