The World in Motion
  • Challenges & Projects
  • Project14
  • The World in Motion
  • More
  • Cancel
The World in Motion
Blog Wheels of Illusion - A hypnotic nomad robot
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join The World in Motion to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: robogary
  • Date Created: 20 Sep 2022 9:24 PM Date Created
  • Views 13893 views
  • Likes 13 likes
  • Comments 4 comments
  • worldinmotionch
  • raspberry pi pico
Related
Recommended

Wheels of Illusion - A hypnotic nomad robot

robogary
robogary
20 Sep 2022

And now for something completely different for the World in Motion Challenge 

The video, glamour photos, schematic, and code are humbly submitted for your entertainment.

This Raspberry Pi Pico robot is built with subtle and not so subtle optical effects. 

  • The rear wheels spin opposite the direction of travel.
  • The tires have hubcaps with the "Twilight Zone Spiral of Madness" to make them appear off center.
  • The spiral on the right hand side will make you really dizzy if you stare at it for long and then look away. 
  • The black & white wheel (Benham's Disc) on the back will show colors when it rotates at the proper speed, which fixed in the code, found by experiments using a power supply.
  • A rotating warning beacon spins and lights when the robot is moving forward. 

For motional content, the Wheels of Illusion has qty 4 servos and 4 DC motors controlled  by a Raspberry Pi Pico. 

The control is by bumper switches on the front, and a ping sensor on the rear.

All my gear motors on hand have different gear ratios and each optical pattern were effective at different speeds. Each motor was run with a power supply to find their best sweet spot rpm and running volts. The value was noted, and set into the PWM duty, tweaked a bit while running on battery.

Python makes the PWM really easy. 

The video:  https://youtu.be/unmvSvUllOM 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

image

image

image

I'd ordered some clamp TBs 1-2834015-3 to try.

Wire-To-Board Terminal Block, Screwless, 2.54 mm, 3 Positions, 26 AWG, 20 AWG, Clamp

https://www.newark.com/te-connectivity/1-2834015-3/tb-wire-to-board-3pos-26-20awg/dp/30AC2754

as shown in this photo of the motor driver assembly. I only have used the screw type in the past.

Those clamp connectors are fabulous on the homebrew level shifter board (far right).

I'm mixed on using them on the FET driver card, I had to plan daisy chains since they only fit one wire. 

image

image

image

# If the LHS side whisker bumps an object, Wheels Of Illusion backs up and makes a righthand turn to avoid it.
# The time Wheels Of Illusion backs up is random, from 1.5 seconds to 4 seconds,.
# It will stop backing up if an object is detected 7 inches from the rear
# HC-SR04 ping sensor in the rear of Wheels Of Illusion.
# If the RHS whisker encounters an object, the behavior is the same except Wheels Of Illusion turns left after backing up.
# The beacon turns off when backing up

from machine import Pin, PWM
# Pin uses the GPIO value , not the actual pin number 
import utime
import random

LHSWhisker= Pin(14, machine.Pin.IN,machine.Pin.PULL_DOWN)#GPIO14 physical pin 19
RHSWhisker= Pin(13, machine.Pin.IN,machine.Pin.PULL_DOWN)#GPIO13 physical pin 17

LHSWhiskerLED= Pin(12, machine.Pin.OUT)#GPIO12 physical pin 16
RHSWhiskerLED= Pin(11, machine.Pin.OUT)#GPIO11 physical pin 15
AliveLED = Pin(25,machine.Pin.OUT)


LHSservo = PWM(Pin(16))#GPIO16 physical pin 21
RHSservo = PWM(Pin(17))#GPIO17 physical pin 22
# 50 Hz is 20 msec period
LHSservo.freq(50)
RHSservo.freq(50) 
# 100% duty of PWM is 65200 counts
# 2 ms of 20 ms is 10% for full spd FWD
# ( 1.5 ms / 20 ms ) * 65200 = 4875 for servo zerospeed
# 1 ms of 20 ms is full spd rev , .05* 65200 
zerospd = 4875
LHS_FullSpd = 3250 # LHS side servo is mounted opposite so gets a reversed reference 
RHS_FullSpd = 6500
LHS_TopSpdRev = 6500
RHS_TopSpdRev = 3250
AliveLED.value(1)

PingTrigger=Pin(9,Pin.OUT)#GPIO9 physical pin 12
PingEcho=Pin(8,Pin.IN)#GPIO18 physical pin 11

Beacon = Pin(18, machine.Pin.OUT)#GPIO18 physical pin 24
#ColorSpinner = Pin(19, machine.Pin.OUT)#GPIO19 physical pin 25
#LHS_Spinner = Pin(20, machine.Pin.OUT)#GPIO20 physical pin 26
#RHS_Spinner = Pin(21, machine.Pin.OUT)#GPIO21 physical pin 27

ColorSpinner = PWM(Pin(19))#GPIO19 #GPIO19 physical pin 25
LHS_Spinner = PWM(Pin(20))#GPIO20 physical pin 26
RHS_Spinner = PWM(Pin(21))#GPIO21 physical pin 27
ColorSpinner.freq(100)
LHS_Spinner.freq(100)
RHS_Spinner.freq(100)
ColorSpinner.duty_u16(7000)
LHS_Spinner.duty_u16(2500)
RHS_Spinner.duty_u16(65000)

def Ping():
    echotries=0
    PingTrigger.low()
    utime.sleep_us(2)  # note sleep_us is for microsecs
    PingTrigger.high()
    utime.sleep_us(10)
    PingTrigger.low()
    while ((PingEcho.value() == 0) and (echotries<30)):
        EchoStartTime = utime.ticks_us()
        echotries=echotries+1
         # This check bails out of the loop on a problem with a long echo  or failed echo, I havent been able to prove its needed.
         
    while PingEcho.value()==1:
        EchoHeard = utime.ticks_us()
    PingDeltaTime=EchoHeard-EchoStartTime
    PingDistance_cm =(PingDeltaTime*.0343)/2  # sound is 343.2 m/s .0343 cm/usec
    PingDistance_in=(PingDistance_cm)/2.54
    #print ("Measured distance is ",PingDistance_cm, "cm"  )
    print ("Measured distance is ",PingDistance_in, "inches"  )
    #print ("Echotries =", echotries)
    return PingDistance_in

def backup():
    LHSservo.duty_u16(LHS_TopSpdRev)  #top speed rev on LHS
    RHSservo.duty_u16(RHS_TopSpdRev) # top spd rev on RHS
    Beacon.value(0)
 ###################### MAIN LOOP ################################ 

while True:  #this is start of the main loop routine
    AliveLED.toggle()
     # if no action on the whiakers go straight
    LHSservo.duty_u16(LHS_FullSpd)  #top speed forward on LHS
    RHSservo.duty_u16(RHS_FullSpd) # top spd fwd on RHS
                            # zerospeed = 4875
    Beacon.value(1)
    # if no action on the whiskers go straight, clear LEDs
    
    if ((LHSWhisker.value() ==0) & (RHSWhisker.value() ==0)):
        LHSWhiskerLED.value(0)
        RHSWhiskerLED.value(0)
      
      
      ################ LHS whisker routine, backup and turn right   
          
    if LHSWhisker.value() ==1: #gotta latch this operation
        LHSWhiskerLED.value(1)
        count=1
        while True:  # using break to exit the loop
            backup()
            #Ping()
            PingDistance=Ping()
            utime.sleep(.2)
            count=count+1
            backuptime=random.randint(7,14)  # backuptime is comprised as the number of 200msec cycles before breaking out of the backup loop
            #print ("backuptime = ",backuptime)
            print ("count = ",count)
            print ("backuptime = ",backuptime)
            #print ("LoopCycles= ",Loopcycles)
            if (PingDistance<6):
                break        
            if (count>backuptime):
                break
           # print ("ping distance = ",PingDistance)
            
    # back up tthen right turn
        RHturntime=random.uniform(.5,3)
        LHSservo.duty_u16(LHS_FullSpd)  #top speed forward on LHS
        RHSservo.duty_u16(zerospd) # zerospeed on RHS
        utime.sleep(RHturntime)
        
        #on exit of LHS Whisker routine, go staright again
    LHSservo.duty_u16(LHS_FullSpd)  #top speed forward on LHS
    RHSservo.duty_u16(RHS_FullSpd) # top spd fwd on RHS
        
        ## start RHS side whisker behavior definition 
        
    if RHSWhisker.value() ==0:
        RHSWhiskerLED.value(0)
        
    if RHSWhisker.value() ==1:
        RHSWhiskerLED.value(1)
        count=1
        while True:  # using break to exit the loop
            backup()
            #Ping()
            PingDistance=Ping()
            utime.sleep(.2)
            count=count+1
            backuptime=random.randint(7,14)  # backuptime is comprised as the number of 200msec cycles before breaking out of the backup loop
            #print ("backuptime = ",backuptime)
            print ("RHScount = ",count)
            print ("RHSbackuptime = ",backuptime)
            if (PingDistance<6):
                break        
            if (count>backuptime):
                break
           # print ("ping distance = ",PingDistance)
        
    # turn left
        LHturntime=random.uniform(.5,3)
        
        LHSservo.duty_u16(zerospd)  # zerospeed on LHS
        RHSservo.duty_u16(RHS_FullSpd) # top spd fwd on RHS
        utime.sleep(LHturntime)
      
        LHSservo.duty_u16(LHS_FullSpd)  #top speed forward on LHS
        RHSservo.duty_u16(RHS_FullSpd) # top spd fwd on RHS
    

  • Sign in to reply
Parents
  • kmikemoo
    kmikemoo over 4 years ago

    robogary   How wonderfully fun!  The hypnotic wheels are good, but the face is the best!!  ThumbsupLaughing

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • robogary
    robogary over 4 years ago in reply to kmikemoo

    Thank you. The face was a very last second inspiration. I get a chance to share this robot with 20 student homeschool class, hoping the face grabs them. I'm just starting to try using Pico with a VL53L5CX-SATEL with the goal to have the ToF sensor on top of this robot for some crude steering using hand gestures. I'd also like to eventually replace the ping module and bumper switches with this ToF sensor.  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • robogary
    robogary over 4 years ago in reply to kmikemoo

    Thank you. The face was a very last second inspiration. I get a chance to share this robot with 20 student homeschool class, hoping the face grabs them. I'm just starting to try using Pico with a VL53L5CX-SATEL with the goal to have the ToF sensor on top of this robot for some crude steering using hand gestures. I'd also like to eventually replace the ping module and bumper switches with this ToF sensor.