Vision Thing
  • Challenges & Projects
  • Project14
  • Vision Thing
  • More
  • Cancel
Vision Thing
Blog Vision Thing: Smarthab Facial Recognition .iii RANT
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Vision Thing to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 27 Oct 2019 8:40 AM Date Created
  • Views 1337 views
  • Likes 7 likes
  • Comments 2 comments
  • visionthingch
  • vision thing
  • beaglebone-ai
  • hdmi-dvi adapter problems
  • rant
  • hdmi problems
Related
Recommended

Vision Thing: Smarthab Facial Recognition .iii RANT

phoenixcomm
phoenixcomm
27 Oct 2019

This project for me has been an adventure into blind alleys and wrong turns. First I did not get my BBAI on time it arrived late as it was sent to my old address. Then we had issues of not booting as I thought it was plugged into a USB 3 connector on the back of my computer (a power brick solved this issue). Then the lowly fan would not run, I took a 5vdc 500ma wall wart down to 1.5v. (almost looks like a dead short, the reason the voltage was so low was that current was so high. remember E=ixr which meas they act as inverses. )  image So I plugged the fan into my Harrison Power Supply took it to 5volts and no joy, so what the hell, I turned up the juice to about 10vdc and the fan took off. Hey, now it even works with that 500ma wall wart. image  One trip to Fry's for an HDMI/DVI  then adapter,  then back today for the micro-HDMI to HDMI cable as they did not have the adapter and the HDMI to DVI adapter. Oh, let's not forget the nonsense with mounting the dam fan with 3mm  screws.image I struck out at the Home Depot and Lowes, and I finally found them at ACE Hardware! (I will have to go back for longer screws so I can raise the fan off the heat sink which will decrease the back pressure on the fan, and it will flow better.image

Good News Now: I got the board working to my tablet via WiFi. Its shell is almost unusable, so I decided to run it free-standing with a monitor and keyboard, then I can change the board's IP-address to sit on my network.  So tonight a 3 AM I hooked up a Viewsonic monitor via the cable and adapter. But alas the monitor was bust. Luckily I had a second monitor there as well I changed the cables and the monitor light up and said no input on VGA and when into power-saving mode. Luckily  I have HDMI to VGA cable here so that is my stunt, to put a VGA cable back on the monitor (I just took the dam thing off). The rigging will be as follows VGA cable between the Monitor and the HDMI adapter, and then the HMDM to micro HDMI to the board.

Hopefully in the morning after I get up and change the cables around again, I will have a eureka moment. LOL image

 

UPDATE: Clem thinks there is a problem with the HDMI driver on the board, as it does not want to work with a DVI adapter.image Well, that did not go well as I ended up with two male HDMI connectors and that did not work. image So I hauled the board and power supplies into the bedroom where the only HDMI monitor lives. I plugged it in and now I'm looking at a desktop! Next comes the keyboard & mouse. At this time I will be able to change the board's IP-address, so it will sit on my 192.168.1.1 network at 192.168.1.100 put an ethernet cable to my switch. Next, I can start a shell from this desktop at 192.168.1.23 and then start X with the address of .1.23 and if the gods are smiling I should have a desktop open locally.  After I do this I will update this page again.

  • Sign in to reply

Top Comments

  • mudz
    mudz over 7 years ago +1
    It seems you had quite a fun there, till now. This is so much to learn about BB-AI, it's a good thing you made a blog regarding one can say >> " problems you might stuck with BB-AI " & how to resolve it…
  • phoenixcomm
    phoenixcomm over 7 years ago in reply to mudz

    mudz Thank you so much, I have to look at this with a grain of salt.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mudz
    mudz over 7 years ago

    image It seems you had quite a fun there, till now. image

    This is so much to learn about BB-AI, it's a good thing you made a blog regarding one can say >> " problems you might stuck with BB-AI" & how to resolve it. Absolutely helpful to others.

    I've seen, you've a humorous way to describe things, Loved it. keep it updating, I'm following it. image

    -mudz