Vision Thing
  • Challenges & Projects
  • Project14
  • Vision Thing
  • More
  • Cancel
Vision Thing
Forum Not enough disk space for apt upgrade on Beaglebone AI
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Vision Thing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 17 replies
  • Answers 5 answers
  • Subscribers 11 subscribers
  • Views 8599 views
  • Users 0 members are here
Related

Not enough disk space for apt upgrade on Beaglebone AI

weiwei2
weiwei2 over 7 years ago

I face a not enough space left on device after attempting to do sudo apt upgrade on the device.

the same scenario happen if i try to update the cloud9 by pulling by following example in https://beagleboard.org/upgrade 

i also try to follow https://www.hackster.io/175809/tidl-on-beaglebone-ai-1ee263  but all of these will fail at the same 'not enough space scenario'

 

originally i thought the 8GB sd card i use is really insufficient then i change to a much bigger one and realize problem persists....then it must be something wrong

below is my sudo apt update and the subsequent sudo apt upgrade procedure

 

 

debian@beaglebone:/var/lib/cloud9$ sudo apt update

[sudo] password for debian:

Ign:1 http://deb.debian.org/debian stretch InRelease

Get:2 http://deb.debian.org/debian stretch-updates InRelease [91.0 kB]

Get:3 http://repos.rcn-ee.com/debian stretch InRelease [3,064 B]                                  

Get:4 http://deb.debian.org/debian-security stretch/updates InRelease [94.3 kB]      

Get:5 http://deb.debian.org/debian stretch Release [118 kB]   

Get:6 http://deb.debian.org/debian stretch Release.gpg [2,365 B]

Get:7 http://deb.debian.org/debian stretch-updates/main armhf Packages [27.3 kB]

Get:8 http://repos.rcn-ee.com/debian stretch/main armhf Packages [1,066 kB]

Get:9 http://deb.debian.org/debian-security stretch/updates/main armhf Packages [484 kB]

Get:10 http://deb.debian.org/debian-security stretch/updates/contrib armhf Packages [1,764 B]

Get:11 http://deb.debian.org/debian-security stretch/updates/non-free armhf Packages [1,272 B]                    

Get:12 http://deb.debian.org/debian stretch/main armhf Packages [6,915 kB]                                              

Get:13 http://deb.debian.org/debian stretch/contrib armhf Packages [42.1 kB]

Get:14 http://deb.debian.org/debian stretch/non-free armhf Packages [59.7 kB]

Fetched 8,906 kB in 17s (511 kB/s)                                                                                                                                                       

Reading package lists... Done

Building dependency tree      

Reading state information... Done

56 packages can be upgraded. Run 'apt list --upgradable' to see them.

debian@beaglebone:/var/lib/cloud9$ sudo apt upgrade

Reading package lists... Done

Building dependency tree      

Reading state information... Done

Calculating upgrade... Done

The following packages have been kept back:

  chromium

The following packages will be upgraded:

  base-files bb-cape-overlays bonescript e2fslibs e2fsprogs gpiod libcomerr2 libcpupower1 libcups2 libexpat1 libexpat1-dev libgd3 libglib2.0-0 libgpiod2 libicu57 libiio-utils libiio0

  libldap-2.4-2 libldap-common libmariadbclient18 libnghttp2-14 libnginx-mod-http-auth-pam libnginx-mod-http-dav-ext libnginx-mod-http-echo libnginx-mod-http-geoip

  libnginx-mod-http-image-filter libnginx-mod-http-subs-filter libnginx-mod-http-upstream-fair libnginx-mod-http-xslt-filter libnginx-mod-mail libnginx-mod-stream libpam-systemd libpq5

  libss2 libssl1.0.2 libssl1.1 libsystemd0 libudev-dev libudev1 libxslt1.1 linux-cpupower linux-libc-dev nginx nginx-common nginx-full openssh-client openssh-server openssh-sftp-server

  openssl systemd systemd-sysv tzdata udev unzip usbutils

55 upgraded, 0 newly installed, 0 to remove and 1 not upgraded.

Need to get 32.0 MB of archives.

After this operation, 194 kB of additional disk space will be used.

E: You don't have enough free space in /var/cache/apt/archives/.

 

subsequently i do a fdisk -l for my very huge sd card after reading about https://www.linuxquestions.org/questions/debian-26/no-space-left-on-device-880308/  but unsure if i can follow it

here's my fdisk output

 

debian@beaglebone:/var/lib/cloud9$ sudo fdisk -l

Disk /dev/mmcblk0: 119.3 GiB, 128043712512 bytes, 250085376 sectors

Units: sectors of 1 * 512 = 512 bytes

Sector size (logical/physical): 512 bytes / 512 bytes

I/O size (minimum/optimal): 512 bytes / 512 bytes

Disklabel type: dos

Disk identifier: 0xf7146e7c

 

Device         Boot Start     End Sectors  Size Id Type

/dev/mmcblk0p1 *     8192 7372799 7364608  3.5G 83 Linux

 

Disk /dev/mmcblk1: 14.6 GiB, 15678308352 bytes, 30621696 sectors

Units: sectors of 1 * 512 = 512 bytes

Sector size (logical/physical): 512 bytes / 512 bytes

I/O size (minimum/optimal): 512 bytes / 512 bytes

Disklabel type: dos

Disk identifier: 0x209da4b7

 

Device         Boot Start      End  Sectors  Size Id Type

/dev/mmcblk1p1 *     8192 30621695 30613504 14.6G 83 Linux

 

Disk /dev/mmcblk1boot1: 4 MiB, 4194304 bytes, 8192 sectors

Units: sectors of 1 * 512 = 512 bytes

Sector size (logical/physical): 512 bytes / 512 bytes

I/O size (minimum/optimal): 512 bytes / 512 bytes

 

Disk /dev/mmcblk1boot0: 4 MiB, 4194304 bytes, 8192 sectors

Units: sectors of 1 * 512 = 512 bytes

Sector size (logical/physical): 512 bytes / 512 bytes

I/O size (minimum/optimal): 512 bytes / 512 bytes

debian@beaglebone:/var/lib/cloud9$

  • Sign in to reply
  • Cancel

Top Replies

  • mp2100
    mp2100 over 7 years ago in reply to weiwei2 +3 verified
    Wei, you had an 8 GB card, but the downloaded image is a 4 GB image. You found the manual instructions to expand the image to fill up your 8 GB card. On that page https://elinux.org/Beagleboard:Expanding_File_System_Partition_On_A_microSD…
  • weiwei2
    weiwei2 over 7 years ago +2 suggested
    i have found this page https://elinux.org/Beagleboard:Expanding_File_System_Partition_On_A_microSD and follow it. originally, my SD is /dev/mmcblk0p1 8192 7372799 7364608 3.5G 83 Linux after the successful…
  • clem57
    clem57 over 7 years ago +1
    Background: I read somewhere that the BB and probably the BB-AI creates a temporary space in RAM. If this contains your cache ( I bet it does ), that is the problem. To solve this, add a hard/soft link…
Parents
  • clem57
    0 clem57 over 7 years ago

    Background: I read somewhere that the BB and probably the BB-AI creates a temporary space in RAM. If this contains your cache (I bet it does), that is the problem. To solve this, add a hard/soft link to the SDcard  space instead of RAM.

     

    Check what partition contains /var/cache/apt/archives/

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 7 years ago in reply to clem57

    Filesystem Size Use Mounted On

    /dev/sda1 327m 86% /

    tmpfs 976M 0% /lib/init/rw

    udev 10M 2% /dev

    tmpfs 976M 0% /dev/shm

    /dev/sda9 289G 1% /HOME

    /dev/sda8 1.9g 1% /tmp

    /dev/sda5 20g 21% /usr

    /dev/sda6 12g 16% /var

     

    The above has tmpfs at almost 1G and 0%

    but sda1 is 327m and 86% full!!!image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 7 years ago in reply to clem57

    Filesystem Size Use Mounted On

    /dev/sda1 327m 86% /

    tmpfs 976M 0% /lib/init/rw

    udev 10M 2% /dev

    tmpfs 976M 0% /dev/shm

    /dev/sda9 289G 1% /HOME

    /dev/sda8 1.9g 1% /tmp

    /dev/sda5 20g 21% /usr

    /dev/sda6 12g 16% /var

     

    The above has tmpfs at almost 1G and 0%

    but sda1 is 327m and 86% full!!!image