Project14
  • Challenges & Projects
  • More
Project14
Documents Project14 | You Decide the Next Monthly Project Competition!
  • News
  • Member Updates
  • Competitions
  • Forum
  • Documents
  • Theme Suggestions
  • Polls
  • Members
  • More
  • Cancel
  • New
Join Project14 to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 10 May 2017 8:26 PM Date Created
  • Last Updated Last Updated: 23 Sep 2024 3:52 PM
  • Views 61690 views
  • Likes 20 likes
  • Comments 338 comments
Related
Recommended

Project14 | You Decide the Next Monthly Project Competition!

In the Forums or as an Idea:  Send Your Suggestions for Future Themes and vote on them!

 Forum  / Theme Suggestions  

 

How are Themes selected?

 Project14 | Quick Update on Upcoming Competitions + What Would You Like To See Happen In Project14?  

 

  • led display
  • communication_protocol
  • music tech
  • home automation
  • decide the next monthly project competition!
  • monthly_project
  • project14 featured
  • arduino home automation
  • analog devices
  • analog & digital wireless communication
  • project14
  • test & measurement
  • arduino communication
  • analog on pi
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • dougw
    dougw over 9 years ago +24
    I guess the suggestion box moved here so I will reiterate one idea I mentioned earlier and add one: - a classroom demonstration of some physics phenomenon ( jc2048 had some good ideas ) - a solar powered…
  • jack.chaney56
    jack.chaney56 over 9 years ago +11
    Keeping with July and (northern hemisphere) Summer time, I like Douglas' ideas. Demonstration of physical phenomenon for classroom is a great avenue, I was thinking lots of solar stuff. Charging systems…
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to Workshopshed +11
    I will ad also a time machine. Sound good ? Enrico
Parents
  • jack.chaney56
    jack.chaney56 over 9 years ago

    Thank you for your feedback image

     

    DAB is spot on! I started off in real time systems (what it was called before embedded) working on brake dynomometer control, then got into writing video games for Atari and Commodore. From my time writing games, I discovered nothing exercises the capabilities of a computer as much as a game, and nothing requires more general knowledge of a system's operation that writing games. To this day, whether I am writing code for a controller, a diagnostic monitor, a simulator, what I see is a video game. The difference is just the consequence when something goes wrong.

     

    balearicdynamics hit on my thinking for what to use for platforms. There are several platforms out there, depending on the application Raspberry Pi, Arduino, and Beagle are a few more. The projects that are available for these platforms focus on the how. I think where I am aiming with this is working on the why question. Why should I use one platform over another? Why do I need a database? Why did I want to solve this? image

     

    Jack

    I have started a discussion at If I Had a Hammer covering the same topic.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to jack.chaney56

    Jack, IMHO the question of Why is strictly depending on the project. Here in most of the cases the approach is: I have this platform and want to do this. I try to give suggestions as I can but I am aware that a better approach is just I want to reach this goal, what platform should I use? Better Better image

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jack.chaney56
    jack.chaney56 over 9 years ago in reply to balearicdynamics

    The "whys" of an investigation can be endless. The weighing of cost and benefit sometimes seems to have no solution. The other factors for determining why is dealing with opinion over fact and what sometimes rise to the level of religious wars.  Used to be fights over Intel v AMD, or worse x86 v 68000. Zealots were everywhere.

     

    As you point out, often the platform is "the one that is available" which is why, when I write code, I always try to maintain platform independence whenever possible.

     

    A couple of wise thoughts I have picked up:

    1. Arguing with an engineer is like wrestling with a pig in the mud. You both get covered from head to toe, and the pig loves it.
    2. If there is a room full of N engineers you will always get at least N+1 "best" solutions
    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jack.chaney56
    jack.chaney56 over 9 years ago in reply to balearicdynamics

    The "whys" of an investigation can be endless. The weighing of cost and benefit sometimes seems to have no solution. The other factors for determining why is dealing with opinion over fact and what sometimes rise to the level of religious wars.  Used to be fights over Intel v AMD, or worse x86 v 68000. Zealots were everywhere.

     

    As you point out, often the platform is "the one that is available" which is why, when I write code, I always try to maintain platform independence whenever possible.

     

    A couple of wise thoughts I have picked up:

    1. Arguing with an engineer is like wrestling with a pig in the mud. You both get covered from head to toe, and the pig loves it.
    2. If there is a room full of N engineers you will always get at least N+1 "best" solutions