Project14
  • Challenges & Projects
  • More
Project14
Documents Project14 | You Decide the Next Monthly Project Competition!
  • News
  • Member Updates
  • Competitions
  • Forum
  • Documents
  • Theme Suggestions
  • Polls
  • Members
  • More
  • Cancel
  • New
Join Project14 to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 10 May 2017 8:26 PM Date Created
  • Last Updated Last Updated: 23 Sep 2024 3:52 PM
  • Views 61726 views
  • Likes 20 likes
  • Comments 338 comments
Related
Recommended

Project14 | You Decide the Next Monthly Project Competition!

In the Forums or as an Idea:  Send Your Suggestions for Future Themes and vote on them!

 Forum  / Theme Suggestions  

 

How are Themes selected?

 Project14 | Quick Update on Upcoming Competitions + What Would You Like To See Happen In Project14?  

 

  • led display
  • communication_protocol
  • music tech
  • home automation
  • decide the next monthly project competition!
  • monthly_project
  • project14 featured
  • arduino home automation
  • analog devices
  • analog & digital wireless communication
  • project14
  • test & measurement
  • arduino communication
  • analog on pi
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • dougw
    dougw over 9 years ago +24
    I guess the suggestion box moved here so I will reiterate one idea I mentioned earlier and add one: - a classroom demonstration of some physics phenomenon ( jc2048 had some good ideas ) - a solar powered…
  • jack.chaney56
    jack.chaney56 over 9 years ago +11
    Keeping with July and (northern hemisphere) Summer time, I like Douglas' ideas. Demonstration of physical phenomenon for classroom is a great avenue, I was thinking lots of solar stuff. Charging systems…
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to Workshopshed +11
    I will ad also a time machine. Sound good ? Enrico
  • ninjatrent
    ninjatrent over 9 years ago in reply to fvan

    Really great suggestion of repairing electronics. There needs to be more awareness of recycling and proper disposal of electronics. Not for monetary gain but to reduce humanity's impact on the environment. Repairing an electronic device rather than discarding it is a very green idea.

     

    It would be interesting to mod a guitar hero into an electric guitar with speaker. There was a guitar hero for Xbox 360, PS2, PS3, and other gaming consoles. It would be cheap to purchase one of the older versions for hacking. The buttons could trigger midi tones as a musical instrument or play directly from a small speaker and amp inside the guitar. There is a company by the name of " Gakken " that manufactures a Mini Electric Guitar Kit. It would be awesome to put it in a Guitar Hero. Any of the Rock Band stuff would be cool to hack.

     

    I am currently working on replacing a faulty power switch on my  second Coca Cola mini vending machine. I had to return the first one back to manufacturer for same reason so there is likely some issue in the design or faulty power switch. Now I have lost the receipt for this one so it is on workbench in my shop.

     

    When electronics fail or become obsolete, I do not throw them away. If the device cannot be repaired then it will be broken down for recycling. I have saved many components from trash pile. Electronics are expensive. Switches, buttons, PIR sensors, LEDs, and other parts can be recovered from broken, used, and obsolete devices.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ipv1
    ipv1 over 9 years ago

    I think we could do something to help the disabled. People with disability could benefit from this competition to get a wearable or portable assistant. There a numerous examples out there like the ultrasonic walking cane for the blind or sound to visual indicators for the hearing impaired. I already have a wireless visual alert system at my house for my mother. It lights up when someone knocks at the door or rings the bell.

    My mom is not deaf or anything but rather has the habit of keeping the tele at full blast in her room. image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fvan
    fvan over 9 years ago

    Here's a theme suggestion: (simple) electronic repairs

     

    Repair a device that is malfunctioning instead of throwing it away or buying a replacement. Could be as simple as repairing a faulty switch, and could help people realise repairs don't need to be that complicated and get insights in some troubleshooting techniques!

     

    For example:

     

    We have a guitar for the XBox, but one of the buttons would only allow movement up instead of up and down. I opened up the guitar, measured and found that a reed switch is used for each position, and that one of them was constantly "ON", even in idle position, due to the magnet and switch being too close to each other.
    I gently bent the legs of the reed switch a bit further away, et voila, there was enough distance to be in "OFF" position in idle, and "ON" when pushed.

     

     

    image

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ninjatrent
    ninjatrent over 9 years ago in reply to jack.chaney56

    Great idea for a project. Here are a few images of the predicted path

    imageimageimage

    These and other images are available at the following links. There are also very detailed high resolution maps and other resources available for download from https://www.nasa.gov/  .

    Some of the images are over 20 MB.

      

          https://eclipse2017.nasa.gov/eclipse-maps

        

         https://eclipse.gsfc.nasa.gov/SEgoogle/SEgoogle2001/SE2017Aug21Tgoogle.html

     

         https://eclipse.gsfc.nasa.gov/SEpubs/RP1178.html

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jack.chaney56
    jack.chaney56 over 9 years ago

    Just been reading through all the ideas, and thought of one to combine some of the ideas I like. Might need some remote help though.  I hear the eclipse is going to be over Oregon, so that would probably be the place to set up. Then set up an RPi with infrared camera and a tracking stand (can be controlled by the Pi as well) and make a time lapse video of the eclipse.  Not sure of what the record rate should be.

     

    Jack

     

    ...wish my brain would slow down a bit sometimes, so my typing can catch up. Time lapse idea got me thinking about special effects and the great stop action sequence in The Matrix, when Neo does the leap, and using a bunch of cameras with some splicing, panned the room while the scene remained motionless. $10 pi zero and $30 for the camera module, times however many frames to shoot, makes the venture much more affordable.

     

    Jack

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jomoenginer
    jomoenginer over 9 years ago in reply to dougw

    How about a solar powered Yard/Beach Gnome or object that comes to life after dark? Perhaps follows the Moon if visible. Heck, it could even double as a Watch Gnome if accessorized with a camera. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to dougw

    Yep! I was serious, should think to something nice...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 9 years ago in reply to balearicdynamics

    A beach makes a great yard. Can't complain too much about no yard if you have a beach nearby..image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to dougw

    I have no yard at all image Should think to something on the beach

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 9 years ago in reply to tariq.ahmad

    It isn't a strong feeling but the yard project might be better in summer months ....

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>