Project14
  • Challenges & Projects
  • More
Project14
Documents Project14 | You Decide the Next Monthly Project Competition!
  • News
  • Member Updates
  • Competitions
  • Forum
  • Documents
  • Theme Suggestions
  • Polls
  • Members
  • More
  • Cancel
  • New
Join Project14 to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 10 May 2017 8:26 PM Date Created
  • Last Updated Last Updated: 23 Sep 2024 3:52 PM
  • Views 61725 views
  • Likes 20 likes
  • Comments 338 comments
Related
Recommended

Project14 | You Decide the Next Monthly Project Competition!

In the Forums or as an Idea:  Send Your Suggestions for Future Themes and vote on them!

 Forum  / Theme Suggestions  

 

How are Themes selected?

 Project14 | Quick Update on Upcoming Competitions + What Would You Like To See Happen In Project14?  

 

  • led display
  • communication_protocol
  • music tech
  • home automation
  • decide the next monthly project competition!
  • monthly_project
  • project14 featured
  • arduino home automation
  • analog devices
  • analog & digital wireless communication
  • project14
  • test & measurement
  • arduino communication
  • analog on pi
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • dougw
    dougw over 9 years ago +24
    I guess the suggestion box moved here so I will reiterate one idea I mentioned earlier and add one: - a classroom demonstration of some physics phenomenon ( jc2048 had some good ideas ) - a solar powered…
  • jack.chaney56
    jack.chaney56 over 9 years ago +11
    Keeping with July and (northern hemisphere) Summer time, I like Douglas' ideas. Demonstration of physical phenomenon for classroom is a great avenue, I was thinking lots of solar stuff. Charging systems…
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to Workshopshed +11
    I will ad also a time machine. Sound good ? Enrico
  • jomoenginer
    jomoenginer over 9 years ago in reply to ninjatrent

    Oh, I loved this game.  I think I still have one somewhere.  I know I certainly have a Vintage Pulsonic Baseball Game as well as a Coleco Amaze-A-Tron.  I always wanted to reproduce the Amaze-A-Tron and doing so with an FPGA would be very interesting.

     

    Even a homage to Ralph H. Baer would be interesting. Baer, who is argued to be the father of video games, created The Magnavox Odyssey, Simon, and a Table Tennis idea which led to Bushnell creating Pong for Atari.  Perhaps something like "Baer Month", or just Retro Game Month.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ninjatrent
    ninjatrent over 9 years ago in reply to RParkerE

    Your idea has reminded me of the LED and LCD handheld games of the 80's.

    image

    An e-Ink / ePaper display or 16-bit OLED display would be interesting.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • RParkerE
    RParkerE over 9 years ago

    I'd be interested in seeing a project which is a game. You could make something similar to the Ben Heck logic game using an FPGA, a chess board where you can play against an AI who actually moves the pieces on the board, program your own video game and make controls using an accelerometer or other motion based control rather than an actual controller. Below are some images that could accompany this idea.

     

    Image result for diy hardware games

     

    Image result for diy hardware games

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 9 years ago in reply to ninjatrent

    Just about to add a I2S Amp to a Pi Zero too

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jack.chaney56
    jack.chaney56 over 9 years ago

    I'd like to see something music based as well. Perhaps a MIDI sequencer, that takes and ABC file as input. Many churches out there with nice organs but can't afford an organist salary, or need a fill in over summer vacation.

     

    Jack

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ninjatrent
    ninjatrent over 9 years ago in reply to dougw

    Thank you for the suggestion. I just found an I2S 3W Class D Amplifier Breakout at Adafruit that will work. It has a built in DAC and will fit in the tin with a small speaker.  https://learn.adafruit.com/adafruit-max98357-i2s-class-d-mono-amp/overview

    There is another method of getting audio from the GPIO. https://learn.adafruit.com/adding-basic-audio-ouput-to-raspberry-pi-zero

    I might try the I2S Class D amp and a small speaker. If I do make a second version I might also use a small NTSC/PAL TFT Display wired to the video pins on the Pi Zero instead of the Adafruit PiTFT I used before. Thank you again for the suggestion. The Class D Amp, I2S DAC, and small speaker would be a great solution.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 9 years ago in reply to ninjatrent

    I've seen mini USB speakers that would fit in a (second) Altoids tin.

    Or I have purchased replacement cell phone speakers which are much smaller - two could be run from one of those class D amps that is less than a square inch and 3.4 mm high.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ninjatrent
    ninjatrent over 9 years ago in reply to ninjatrent

    It would be interesting to see if someone else could make a better version of a RetroPie gaming console in an Altoids tin. While the Adafruit display fit inside of the Altoids tin, the buttons that are located under the display are not necessary. One limitation of my original design was that the audio was provided by a USB speaker. It was my intention to put a small speaker inside the Altoids tin but I ran into some issues with creating an audio output for the speaker.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to ninjatrent

    I did a mini version of your project - single pixel (light sensor) instead of a camera:

     

    Measure Eclipse 2015 with a Hercules LaunchPad

    image

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ninjatrent
    ninjatrent over 9 years ago

    The Tin Man Heart is one of my photos. image I put a Raspbery Pi Zero and Adafruit PiTFT 320x240 2.2" TFT Display HAT in an Altoids tin.

     

    image

    image

    image

     

    Here is another one that I made with a different cable config.

     

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>