Project14
  • Challenges & Projects
  • More
Project14
Polls Project14 | Poll to Decide the June '19 Competition!
  • News
  • Member Updates
  • Competitions
  • Forum
  • Documents
  • Theme Suggestions
  • Polls
  • Members
  • More
  • Cancel
  • New
Join Project14 to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 12 Apr 2019 6:40 PM Date Created
  • Last Updated Last Updated: 11 Oct 2021 2:58 PM
  • Views 1638 views
  • Likes 0 likes
  • Comments 6 comments
Related
Recommended

Project14 | Poll to Decide the June '19 Competition!

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • dougw
    dougw over 7 years ago +3
    Here is another idea for a future poll: an electronic toy - in case it hasn't cropped up before. Toys may seem a little too juvenile for this forum, but toy design can be very sophisticated and it is definitely…
  • Workshopshed
    Workshopshed over 7 years ago in reply to beacon_dave +3
    Dave, I did look at this with this a few years back. The "Massively Distributed Rube Goldberg Machine". My idea was to have an MQTT protocol to pass the message on to the next stage. I wondered if something…
  • beacon_dave
    beacon_dave over 7 years ago in reply to dougw +2
    Sounds a great idea with plenty of avenues to choose from - executive toy, puzzle toy, educational toy, cuddly toy... Another twist might be some form of collaborative challenge similar to the Rube Goldberg…
Parents
  • dougw
    dougw over 7 years ago

    Here is another idea for a future poll: an electronic toy - in case it hasn't cropped up before.

    Toys may seem a little too juvenile for this forum, but toy design can be very sophisticated and it is definitely big business.

    Games and toys often drive the electronics industry to develop new technology.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 7 years ago in reply to dougw

    Sounds a great idea with plenty of avenues to choose from - executive toy, puzzle toy, educational toy, cuddly toy...

     

    Another twist might be some form of collaborative challenge similar to the Rube Goldberg Machine where there is a standard input/output interface requirement which allows the output of one member's machine to be able to connect to the input of another member's machine. RGMs have been suggested before but without the collaboration element. This could be an on-going theme, perhaps even using the monthly theme as a basis for each new module. The interface could perhaps be a 3D printed component to help ensure a degree of compatibility.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • beacon_dave
    beacon_dave over 7 years ago in reply to dougw

    Sounds a great idea with plenty of avenues to choose from - executive toy, puzzle toy, educational toy, cuddly toy...

     

    Another twist might be some form of collaborative challenge similar to the Rube Goldberg Machine where there is a standard input/output interface requirement which allows the output of one member's machine to be able to connect to the input of another member's machine. RGMs have been suggested before but without the collaboration element. This could be an on-going theme, perhaps even using the monthly theme as a basis for each new module. The interface could perhaps be a 3D printed component to help ensure a degree of compatibility.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Fred27
    Fred27 over 7 years ago in reply to beacon_dave

    I like that idea. Would we all post them off to E14 HQ to physically connect them together (nice but not very practical) or were you thinking of a virtual connection so that as one device finishes it triggers another one on the other side of the planet?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 7 years ago in reply to Fred27

    It could take a number of forms and is of course open for discussion.

     

    Initially I was thinking of Doug's electronic toy idea and how it would be good if one could somehow make a collective Rube Goldberg Machine out of it. For this to work E14 would need to host a standard interface spec, and ideally designs submitted would be sufficiently documented in order to be reproducible by others joining in. That way people could build the modules they like and connect them together in the order they like similar to the collaborative RGM events.

     

    Another idea as you suggest was along the lines of submitting the finished modules to the E14 HQ for use at maker type shows etc. Virtual connections had also crossed my mind taking RGM into the IoT world.

     

    As far as I am aware, the RGM contests currently rely on mechanical coupling via the ball bearings, but here at E14 we perhaps could also have an electronic element to it in that each interface has an electronic bus which passes from module to module. If the module is purely mechanical, then this might just be a pass through connection, whereas other modules may use it for a synchronisation clock or perhaps modify the data being sent in some way.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 7 years ago in reply to beacon_dave

    Dave, I did look at this with this a few years back. The "Massively Distributed Rube Goldberg Machine".

     

    My idea was to have an MQTT protocol to pass the message on to the next stage. I wondered if something like google hangouts could be automated using an API to switch the video feeds.

     

    https://github.com/Workshopshed/mdrgm

     

    Machine

     

    Unfortunately I never had the time to flesh the idea out.

    • Cancel
    • Vote Up +3 Vote Down