Products
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
Wearable Tech
  • Challenges & Projects
  • Project14
  • Wearable Tech
  • More
  • Cancel
Wearable Tech
Blog Helping Alzeihmer Patients with tech!
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wearable Tech to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: vimarsh_
  • Date Created: 14 Jan 2019 6:04 PM Date Created
  • Views 1650 views
  • Likes 11 likes
  • Comments 3 comments
  • pocketbeaglebone
  • maxim_rt
  • project14
  • pocketbeagle
  • wearabletechch
Related
Recommended

Helping Alzeihmer Patients with tech!

vimarsh_
vimarsh_
14 Jan 2019
image

Wearable Tech

Enter Your Electronics & Design Project for a chance to win a $100 Shopping Cart!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

Note: The project is not fully completed and ready... Updates will be shared as it is complete.

 

Many Alzheimer patients suffer sudden shaking movements with increased heart rate. This may lead to heart stroke and further damage to the patient.
To solve this problem I wanted to make a device that can detect the instant little vibrating motions and the heart rate of a person. And for the instant processing, I needed a fast MCU that can also connect to a smartphone via Bluetooth.

 

Parts:

For detecting vibrations I planned to use ADXL345 accelerometer as it operates on i2c and I had one. But I had sent problems in taking reading to my MCU i.e., Pocket Beagle. Also, it was slow so detecting small vibrations was difficult. So I decided to use ADXL335 an analogue accelerometer which was easy to use.

For the heart rate sensor, I used MAX30100.

And the MCU was Pocket Beagle -  An RPi zero W alternative by BeagleBone. It has a faster processor more RAM and more features but lacks WiFi and Bluetooth. Above all that RPi community is far better than beagle bone. The documentation available for RPi and the OEM support is also better. Even though there were these problems I wanted to try Pocket beagle (due to all of its hype) .

 

Working:

This concept works in a simple way. When there are shaky movements detected by the accelerometer, then it starts taking a reading and compares them to the given set of data. If the amplitude is too high then, it may be the normal movement of the person. But if there are very small jerky movements then it will detect them and measure the heart rate of the person, that data will conclude about the condition of the person. If it not good then there will be an alarm sent on the smartphone which will ring loudly and may also call Emergency services. This can prevent any heart injury or more brain damage.

 

Methodology:

I started it off by downloading the image from beagle bone website and then inserting the flashed sd card into Pocket Beagle. The first thing after the getting started was that I opened node red my favourite GUI editor. It was nothing special and also had some functionalities compromised. The best part was the cloud9 IDE. I could program in ay language I want to achieve the same result. And due to this advantage, I could try out (never tried) languages like Ruby and JS to do embedded programming.

The transfer to the smartphone I used a simple Bluetooth module - HC05

 

After having the concept, I ordered the parts i.e., ADXL335 and MAX30100 on eBay. and sadly, they have not arrived till date. Hence, the project is not complete. But the software is ready to go.

But here is a short video on the concept of how the project will work... It is quite explanatory.

 

                                                           Video about the concept of its working: 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The code will be kept here once it is completely ready: https://github.com/vimarsh244/Helping-Alzeihmer-Patients

 

The project is not complete presently, but it surely will be later. Stay Tuned for that.

  • Sign in to reply

Top Comments

  • DAB
    DAB over 7 years ago +2
    Nice post. Since my heart attack I have become more interested in wearable medical devices. DAB
  • toolkitman
    toolkitman over 6 years ago in reply to DAB +2
    I can give my little help by adding this homepage Federazione Alzheimer Italia - iPhone - Android - Alzheimer App It's an app for iphone and Andorid who helps reminds Alzehimer people tasks. Not my invention…
  • mayermakes
    mayermakes over 7 years ago +1
    interesting project! Keep us up to date with your project!
Parents
  • mayermakes
    mayermakes over 7 years ago

    interesting project! Keep us up to date with your project!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mayermakes
    mayermakes over 7 years ago

    interesting project! Keep us up to date with your project!