Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog And The Lamp Begins To Look Brighter
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
  • Author Author: RParkerE
  • Date Created: 29 Apr 2015 1:06 AM Date Created
  • Views 1086 views
  • Likes 3 likes
  • Comments 4 comments
  • mini_automator
  • enchanted-objects-design-challenge
  • enchanted-objects
Related
Recommended

And The Lamp Begins To Look Brighter

RParkerE
RParkerE
29 Apr 2015

I just received an dimmable LED (LOHAS 20W LED Chip). I plan on running a few test programs, starting with the ones that Infineon provide, while I wait for my recessed can whip extension to arrive and I will start prototyping the lamp.

 

Here is a picture of the beauty:

image

 

I have also been messing around with TinkerCAD to build a case for the Arduino Yún and Infineon RGB Shield, which is also how I will attempt to prototype multiple lampstands. I would also like to thank all who helped me on my last post!

 

image

image

  • Sign in to reply

Top Comments

  • RParkerE
    RParkerE over 11 years ago in reply to Workshopshed +1
    This housing is for the Yún with the RGB Shield already attached, so I doubt you would be able to be able to see the LEDs on the Yún anyway. The LEDs from the RGB Shield will extend outward from the shield…
  • Workshopshed
    Workshopshed over 11 years ago in reply to RParkerE +1
    If you are using the opkg package manager to install any new packages onto the Yun, I strongly advise expanding the O/S onto an SDCard before you start installing those.
  • Workshopshed
    Workshopshed over 11 years ago in reply to RParkerE

    If you are using the opkg package manager to install any new packages onto the Yun, I strongly advise expanding the O/S onto an SDCard before you start installing those.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • RParkerE
    RParkerE over 11 years ago in reply to Workshopshed

    This housing is for the Yún with the RGB Shield already attached, so I doubt you would be able to be able to see the LEDs on the Yún anyway. The LEDs from the RGB Shield will extend outward from the shield and will be attached to a lamp. But thank you for reminding me about the SD Card, as of now I have not been using one, so I completely overlooked that fact.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • saum
    saum over 11 years ago

    Waiting for the results you get. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 11 years ago

    Don't forget that the SD Card sticks out, also perhaps a window so you can see the LEDs?