Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog MagicHat - 10 - Blood pressure measurement
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
  • Author Author: amgalbu
  • Date Created: 29 Apr 2015 1:35 PM Date Created
  • Views 1229 views
  • Likes 4 likes
  • Comments 5 comments
  • enchanted_objects
  • earth_beat
  • magic_doctor_hat
  • arduino
  • blood_pressure
Related
Recommended

MagicHat - 10 - Blood pressure measurement

amgalbu
amgalbu
29 Apr 2015

In this post I will talk about the blood pressure measurement subsystem

The main components of this subsystem are

  1. the heart beat detector
  2. a continuous rotation servo
  3. a force sensor resistor

 

The idea behind this experimental blood pressure measurement is to replace the arm cuff that is inflated by an air compressor with an elastic rubber pulled by a servo motor. When the rubber exercise a force that is exactly equal to the pressure of the blood, the blood stops flowing through the finger. At that moment, I can read the force the finger is squeezed y means of the FSR. Force can then be converted to a pressure value by applying a simple linear conversion

The following flowchart gives an overview of the whole process

 

                                                            image

In order to make test easier, I built a frame where all the components will be placed

 

image

Note the plastic strip that will pull the elastic rubber back when the pressure measurement process has finished

Then I put the Force Sensor Resistor in place

 

image

 

On top of FSR, I placed the heart beat sensor. I enclosed the sensor in foam to protect the FSR (and the patient finger as well..). Then, I placed the elastic rubber

 

image

Then I added a microswitch to detect when the finger is in place. Since Atmel 32U4 is not that monster, this makes me save a lot of computational power when there is nothing to measure...

 

image

 

Finally, the servo that pulls the elastic rubber has been added

image

 

The implementation, is easy because I just need to put some software pieces together. I already implemented the heart beat detection algorithm and the FSR reading procedures. Moving the servo is very easy thanks to the servo library included in the Arduino IDE.

I will probably need some experiments to determine the PWM that allows the best trade-off between measurement speed and accuracy.

Also, some measurements on different subjects and a reference instrument (a blood monitor system you can buy in any pharmacy) will be reuqired to determine the force-to-pressure conversion law

After that, I hope I will finally able to measure my blood pressure...

  • Sign in to reply

Top Comments

  • tomaja
    tomaja over 11 years ago +1
    This is a very interesting idea! I would love to see a video once it's complete.
  • amgalbu
    amgalbu over 11 years ago in reply to tomaja +1
    Thanks Dragan!
  • amgalbu
    amgalbu over 11 years ago in reply to Workshopshed +1
    Hi Andy Clark you are right: typically you get a sistolic and diastolic pressure, My target is to measure both, but I would be very happy just to succeed in measuring reliably the sistolic one! cheers
  • xever
    xever over 11 years ago

    Very nice!  Looking forward to your results and its accuracy.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • amgalbu
    amgalbu over 11 years ago in reply to Workshopshed

    Hi Andy Clark

    you are right: typically you get a sistolic and diastolic pressure, My target is to measure both, but I would be very happy just to succeed in measuring reliably the sistolic one!

     

    cheers

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • amgalbu
    amgalbu over 11 years ago in reply to tomaja

    Thanks Dragan!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 11 years ago

    If I remember correctly blood pressure is measured both on the stopping and starting of a pulse so you slowly unwind and check for the pulse restarting. You get two measurements. Also you might want to have a max setting so you don't want to crush the finger.

     

    Understanding Blood Pressure Readings

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • tomaja
    tomaja over 11 years ago

    This is a very interesting idea! I would love to see a video once it's complete.