MusicTech
  • Challenges & Projects
  • Design Challenges
  • MusicTech
  • More
  • Cancel
MusicTech
Blog PlectralEFFECTS - Final Notes and Demonstration
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 10 Apr 2016 5:57 PM Date Created
  • Views 917 views
  • Likes 2 likes
  • Comments 1 comment
  • plectraleffects
  • musictech
Related
Recommended

PlectralEFFECTS - Final Notes and Demonstration

e14 Contributor
e14 Contributor
10 Apr 2016

PlectralEFFECTS - Final Notes

 

 

I have had a busy couple of weeks, and unfortunately the project has been on hold.  I have been busy with getting our family home ready to go on the market.

 

I did however complete the implementation of continuous controllers, and obtained my main goal of the project to control the effect / envelopes from the plectrum.   Please see the following video for the demonstration purpose :

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

The main challenge for me in implementation of the enveloped effects was gaining an understanding of MIDI Clock.  The effect mode is varied between two states, depending on which side of the plectrum is used.  Effects are tempo synced to the DAW and are in time with beats.  MIDI Clock generates a byte 0xF8 at exactly 24 pulses per quarter note.  The envelope effects are sinusoidal calculated at 1/24th of a 1/2 wave, or 0.130899 radians to keep in time with the MIDI Clock.

 

 

 

The code is attached below, and I hope that is of some use. I will continue on with the project and see if there is more I can implement with it, but right now I am happy to play with it.

 

 

I would have liked to have seen what I could do with the BeagleBone Black.  Unfortunately, the main components including the BBB of the challenger kit never arrived.

 

 

 

Arduino Code :

 

// Include the Bounce2 library found here :
// https://github.com/thomasfredericks/Bounce2
#include <Bounce2.h>

#define BUTTON_PIN_1 0
#define BUTTON_PIN_2 1


#define LED_PIN  13
#define LED_PIN2 10
#define LED_PIN3 9

// Instantiate a Bounce object
Bounce debouncer1 = Bounce(); 
Bounce debouncer2 = Bounce(); 

// Current clock
byte midiClock;

// Current effect mode
byte effectMode;

float rads;


void noteOn(byte channel, byte pitch, byte velocity) {
  MIDIEvent noteOn = {0x09, 0x90 | channel, pitch, velocity};
  MIDIUSB.write(noteOn);
}

void noteOff(byte channel, byte pitch, byte velocity) {
  MIDIEvent noteOff = {0x08, 0x80 | channel, pitch, velocity};
  MIDIUSB.write(noteOff);
}


void controlChange(byte channel, byte control, byte value) {
  MIDIEvent event = {0x0B, 0xB0 | channel, control, value};
  MIDIUSB.write(event);
}

bool value1state=false;
bool value2state=false;

void loop() {
  debouncer1.update();
  debouncer2.update();

  int value1 = debouncer1.read();
  int value2 = debouncer2.read();

  // Turn on the LED if either button is pressed :
  if ( value1 == LOW ) {
    digitalWrite(LED_PIN, HIGH );
    if (!value1state)
    {
    effectMode=1;
    rads=0;
    value1state=true;
    }
  } 
  else {
    digitalWrite(LED_PIN, LOW );
    if (value1state)
    {
    value1state=false;
    }
  }

 if (  value2 == LOW ) {
    digitalWrite(LED_PIN, HIGH );
    if (!value2state)
    {
     effectMode=2;
     rads=0.13089969*6; // phase offset
     value2state=true;
    }
  } 
  else {
    digitalWrite(LED_PIN, LOW );
    if (value2state)
    {    
     value2state=false;
    }
  }


 while(MIDIUSB.available() > 0) {  
      MIDIEvent e;
      e = MIDIUSB.read();

      if (e.m1 == 0xFA) {
        midiClock = 0;
        rads = 0.0;
      }

      if (e.m1 == 0xFC) {
        midiClock = 0;
        rads = 0.0;
      }

      if (e.m1 == 0xF8) {
      
      if (midiClock == 0) 
       {
        digitalWrite(LED_PIN, HIGH );
       }

       midiClock++;
       if (midiClock >= 24) midiClock = 0;

       if (effectMode == 1)
        rads = rads + (0.13089969*4);
       else
        rads = rads + (0.13089969);

       
       if (rads >= PI*2) rads = 0;   
     
       controlChange(0, 74,  round((sin(rads)*63)+64));       
       MIDIUSB.flush();
      }
     }

   digitalWrite(LED_PIN, LOW );



}

void setup() {
  // Setup the first button with an internal pull-up :
  pinMode(BUTTON_PIN_1,INPUT_PULLUP);
  debouncer1.attach(BUTTON_PIN_1);
  debouncer1.interval(5); // interval in ms
  
   // Setup the second button with an internal pull-up :
  pinMode(BUTTON_PIN_2,INPUT_PULLUP);
  debouncer2.attach(BUTTON_PIN_2);
  debouncer2.interval(5); // interval in ms


  //Setup the LEDs :
  pinMode(LED_PIN,OUTPUT);
  pinMode(LED_PIN2,OUTPUT);
  pinMode(LED_PIN3,OUTPUT);
}

  • Sign in to reply
  • DAB
    DAB over 10 years ago

    It looks like you are making good progress.

     

    It is clear that you have a host of new techniques to play with to make music.

     

    Nice job,

     

    DAB