Sustain The World - Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Sustain The World - Design Challenge
  • More
  • Cancel
Sustain The World - Design Challenge
Blog Sustain The World - Smart Portable Freezer #2 The Cooling Peltier
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
  • Author Author: fyaocn
  • Date Created: 26 Aug 2020 2:43 AM Date Created
  • Views 1095 views
  • Likes 4 likes
  • Comments 1 comment
Related
Recommended

Sustain The World - Smart Portable Freezer #2 The Cooling Peltier

fyaocn
fyaocn
26 Aug 2020

      • 1. The Cooling Peltier
      • 2. Thermal Energy Harvesting
      • 3. How to use

1. The Cooling Peltier

Here is the picture , with nameplate rating 12V

image

The principle is simple, as the following picture shows, I have just fetch the pic from other web directly, so, just for reference. It would be better I draw by hand and use my version.

image

image

The Cooling  Peltier can be heating pad if change side but it is fragile and easy to be damaged when overheating. It is covered with ceramic, so, install carefully, it can be broken by pressure from screws.

 

2. Thermal Energy Harvesting

It can be stacked for other purpose, harnest power from temperature. Set the range of 200mV, connect the red-black wire directly, the reading is 0.00mV in room temperature.

image

Then, put one bottle of boiling water on top of the pad, the reading is -53.7mV. In fact, the maximum rating is 0.7V and several mA. Enough to drive some electronics. Some one uses them in arrays to get high power output.

image

It can be some fun to played with. But not now for me. I have issues with login and delay in the project.

This type of  cooling pad used to be expensive and not worth a try. But it is much cheaper now. Many small fridge are designed with it, cheap but I can guarantee their performance. Anyone can afford one on top of workbench for handy fresh beer.

 

3. How to use

All I need is on relay and one 12V DC power to drive. It shall be fixed on aluminum cooling fins.

My project is just make the freezer smarter, with Infineon product line.

image

 

Previous Blog,

Sustain The World - Smart Portable Freezer #1 The IDEA

  • Sign in to reply

Top Comments

  • rati89
    rati89 over 6 years ago +1
    Nice Idea! I used peltieres once and needed 3.3V. It took me in the end over 4 peltiers with a high temperatur difference/temp gradient to achieve it. But in the end, it was quite hard to get a constant…
  • rati89
    rati89 over 6 years ago

    Nice Idea! I used peltieres once and needed 3.3V. It took me in the end over 4 peltiers with a high temperatur difference/temp gradient to achieve it.

    But in the end, it was quite hard to get a constant voltage of at least 3V..