Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Blog Automated Green  Blog:25.1 - Growing: Transplanting Seedlings
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
  • Author Author: m.ratcliffe
  • Date Created: 28 Nov 2015 3:54 PM Date Created
  • Views 1622 views
  • Likes 1 like
  • Comments 2 comments
  • adapted_greenhouse
  • vertical_farming
Related
Recommended

Automated Green  Blog:25.1 - Growing: Transplanting Seedlings

m.ratcliffe
m.ratcliffe
28 Nov 2015

So the seedlings have grown to a stage that they are ready for transplanting from the propagator to the aquaponics, hydroponics and soil systems.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Germinated/planted :      20/10/2015

Transplanted:                 24/11/2015

 

 

They have grown slow [very slow], this is an expected problem in England during November where the light intensity has dropped considerably. But as it is a comparison experiment we should still be able to gather some useful data.

 

Results from propagator experiment, If you recall we used two types of rock wool cubes. One set had been pre soaked in PH and EC solutions the other just the Ec and PH was left at its original value. The video shows the results, very little visual difference between the two, similar growths similar colours and similar root structures.

 

Keep an eye on the main page for future updates:

  • Sign in to reply
  • m.ratcliffe
    m.ratcliffe over 10 years ago in reply to DAB

    Thanks DAB, Ive done this comparison in the past and they grow better without the pots. The water flow is only around 1l/min to 2l/min so only a thin layer on the bottom of the tube, celery and other tall plants are much easier to place in the NFT than the lettuce but after a while you get the hang of it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 10 years ago

    It will be interesting to see how well the plants grow after being plunked down into the solution.

     

    I suspect that as long as your fluid flow is low volume that they should stay in place and grow well.

     

    DAB