Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Blog Automated Green House Blog:9.1 - Updated uptime counter
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
  • Author Author: m.ratcliffe
  • Date Created: 12 Sep 2015 4:37 PM Date Created
  • Views 1102 views
  • Likes 1 like
  • Comments 2 comments
  • adapted_greenhouse
  • arduino
Related
Recommended

Automated Green House Blog:9.1 - Updated uptime counter

m.ratcliffe
m.ratcliffe
12 Sep 2015

This doesnt really deserve to be a blog, So it is 9.1 and a supplement to blog 9:

Automated Green House Blog:9 -  Some Generic Arduino Tricks - SRam - UpTime

 

Here is an updated uptime counter that makes life a little simpler

Header 1

/* This Script is the bare bones needed to Keep a Uptime counter that will survive the 50 day timer rollover

This will not give a uptime of great accuracy over long periods, but it will let you see if your arduino has reset

if you want better accuracy, pull the Unix time from the IOT, External RTC or GPS module

Also Reconnecting the serial com's will reset the arduino. So this is mainly useful for a LCD screen

 

 

Michael Ratcliffe  Mike@MichaelRatcliffe.com

   

    This program is free software: you can redistribute it and/or modify

    it under the terms of the GNU General Public License as published by

    the Free Software Foundation, either version 3 of the License, or

    (at your option) any later version.

 

 

    This program is distributed in the hope that it will be useful,

    but WITHOUT ANY WARRANTY; without even the implied warranty of

    MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the

    GNU General Public License for more details.

 

 

    You should have received a copy of the GNU General Public License

    along with this program.  If not, see <http://www.gnu.org/licenses/>.

 

 

   

*/

 

 

//************************** Just Some basic Definitions used for the Up Time LOgger ************//

long Day=0;

int Hour =0;

int Minute=0;

int Second=0;

int HighMillis=0;

int Rollover=0;

 

 

 

 

//************** Setup routine - Runs once at power up **************************//

void setup(){

Serial.begin(9600); // starting Serial Com's

 

};

 

 

//****** Main Loop - Put your Code Here ********************//

void loop(){

 

uptime(); //Runs the uptime script located below the main loop and reenters the main loop

print_Uptime();

delay(500);

};

 

 

 

 

 

 

//************************ Uptime Code - Makes a count of the total up time since last start ****************//

 

 

void uptime(){

//** Making Note of an expected rollover *****//  

if(millis()>=3000000000){

HighMillis=1;

 

 

}

//** Making note of actual rollover **//

if(millis()<=100000&&HighMillis==1){

Rollover++;

HighMillis=0;

}

 

 

long secsUp = millis()/1000;

 

 

Second = secsUp%60;

 

 

Minute = (secsUp/60)%60;

 

 

Hour = (secsUp/(60*60))%24;

 

 

Day = (Rollover*50)+(secsUp/(60*60*24));  //First portion takes care of a rollover [around 50 days]

                      

};

 

 

//******************* Prints the uptime to serial window **********************//

void print_Uptime(){

 

  Serial.print(F("Uptime: ")); // The "F" Portion saves your SRam Space

  Serial.print(Day);

  Serial.print(F("  Days  "));

  Serial.print(Hour);

  Serial.print(F("  Hours  "));

  Serial.print(Minute);

  Serial.print(F("  Minutes  "));

  Serial.print(Second);

  Serial.println(F("  Seconds"));

};

  • Sign in to reply
  • m.ratcliffe
    m.ratcliffe over 11 years ago in reply to DAB

    You are correct Dab, It is recommend to use time pulled from a RTC, GPS or internet for any critical projects.


    In the main system I am pulling the time via an ethernet shield and shooting a warning email saying the system has reset in the setup() loop. I included this for anyone needing a estimate of uptime with no extra hardware handy but a need to know if a system has recently reset [ie the water meter total volume measurements in another blog].

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 11 years ago

    Looks like a good start.

     

    Have you considered using a RTC chip so that you can off load the timing and just read updates?

     

    DAB