Learning Center
  • Learn
  • More
Learning Center
Blog One of the Best CPU ever made: MC680xx
  • Blog
  • Documents
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Learning Center to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 17 Dec 2023 7:38 PM Date Created
  • Views 3694 views
  • Likes 8 likes
  • Comments 9 comments
  • intel pentium
  • 68000 vs pentium
  • motorola mc68000
  • motorola mc68k
Related
Recommended

One of the Best CPU ever made: MC680xx

phoenixcomm
phoenixcomm
17 Dec 2023

imageIn the late 70's Motorolla, stunned the world with a new CPU family. It was the MK68k family first it was 32-bits internally,  Launched first was the MC68008 which only had an 8-bit external I/O bus. Following the MC68010 was released.  Followed by the MC68012 which included support for virtual memory. Next came the 2nd Generation CPUs MC68020 and MC6830. The MC68040 is a  3rd Generation CPU that was heavily pipelined! Then the 4th Generation emerged the MC68060 which was a supper scaller. 

The processor family was well thought out, from the beginning the MC6000 family had an integer math processor built on the die, but no floating point processors but later the family got two floating point processors MC68881 and later, the MC68882.

The MC68000 family was so successful, in fact, there were multiple computer systems built around the family, Radio Shack TRS-80 Model 16  (Feb 82),  Sun Microsystems Sun-2 (1983),  Apple Mac (1984),  TRS-80 Model 16, and others. 

image image image

The architecture of the MC8000 family was CISC or a Complex Instruction Set Computer, but there were additions. Like in any operation, you can do pre or post-operations like in one clock cycle C, Java, Python, and others. Below is a table that shows the difference between both processors Intel and Motorola.  Now being a C programmer this is neat.  Sorry I can't show the assembler for this, but I worked out to 5 instructions (Intel) vs 1 instruction (MC69000). What does this mean to software performance? Well, how about a for(int a; a <10; a++) with a counter or any other counter for that matter? 

Fins: This processor is in a lot of stuff, and was the favorite of embedded stuff, until recent times. 

INTEL  MOTOROLA

B = TempB - 1
C= TempC - 1
tempA = B + C
A = A + 1

+A = B- + C-
  • Sign in to reply
Parents
  • DAB
    DAB over 2 years ago

    I agree, the design of the chip was very cool at the time.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 2 years ago in reply to DAB

    It is still a great CPU I have a VME system that runs my cable tester, It has crappy I/O so I front ent it currently with an Android, but I think I will use a PC and a webpage for my interface that way I can use QT! ~~ Cris H. 

    Oh, BTW my next blog will be Sun Microsystems Sparc and Ultra-Sparc.  Which blows up intel!! 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 2 years ago in reply to phoenixcomm

    The "Age of Workstations" really pushed the boundaries forwards. Unfortunately, as soon as they ported their software to run on PC's, Their (better but expensive) hardware lost its viability.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 2 years ago in reply to dougw

     dougw Yes, but no!  The PC (Windows) could not load or, the amount of processes running concurrently as well as the Sparc!  It was like 3 to one. The demise was in fact, the rapid increases in the speed of the CPU and Memory. And there were other things remember the y2k bugs yes bugs, one was for leap year and the other was for leap day in February. Sun had fixed both bugs by standardizing on a longer clock register by using  64  bits. vs 32 bits of a Windows system. 

    See our press release of June 10, 1999. ~~ Cris H. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • phoenixcomm
    phoenixcomm over 2 years ago in reply to dougw

     dougw Yes, but no!  The PC (Windows) could not load or, the amount of processes running concurrently as well as the Sparc!  It was like 3 to one. The demise was in fact, the rapid increases in the speed of the CPU and Memory. And there were other things remember the y2k bugs yes bugs, one was for leap year and the other was for leap day in February. Sun had fixed both bugs by standardizing on a longer clock register by using  64  bits. vs 32 bits of a Windows system. 

    See our press release of June 10, 1999. ~~ Cris H.