Learning Center
  • Learn
  • More
Learning Center
Blog One of the Best CPU ever made: The CELL processor.
  • Blog
  • Documents
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Learning Center to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 25 Dec 2023 8:45 PM Date Created
  • Views 4301 views
  • Likes 7 likes
  • Comments 5 comments
  • STI alliance
  • AIM alliance
  • 790040-LF
  • Mercury Computer Systems
  • playstation 3
  • powerpc
  • IBM CELL processor
  • linux
Related
Recommended

One of the Best CPU ever made: The CELL processor.

phoenixcomm
phoenixcomm
25 Dec 2023

image This processor was an overlooked beast.  At its heart was a 64-bit image core was developed by Apple, IBM, and Motorola became known as the AIM alliance [Wiki], with Enhanced RISC,  with dual-issue in-order two-way simultaneous-multithreaded CPU core with a 23-stage pipeline acting as the controller for the eight SPEs, which handle most of the computational workload It was developed by Sony, Toshiba, and IBM, an alliance known as "STI" [Wiki]. In 2006 Sony released its image 3, with imagea 2.8 GHz board that will deliver about 180 GFlops, while Clearspeed rates its CSX600 processor-based board at about 50 GFlops.

image image

 Mercury has built a CAB, CELL Accelerator Board, on a PCI Express ATX form factor. Another example is  Clearspeed's PCI-X accelerator board. Mercury says that its Cell systems will deliver about 15-30 times the floating point performance and in some scientific applications may be up to 100 times faster. Since floating point performance playsa critical role in flight simulation programming where you must continually do things like 3-D transforms, and other floating-point processes, the CELL fits in very nicely. In fact, DARPA got into the act with their Off-Road challenge! there was a winning team "Axion Racing" who used several PS3s and Yellow Dog Linux in an autonomous off-road vehicle. 

The biggest problem that the CELL was up against was itself, as it was a pain in the you-know-what-to program. The PS3 lived for one year and then died. ~~ RIP

  • Sign in to reply

Top Comments

  • maxpowerr
    maxpowerr over 2 years ago +1
    Interesting information. I just don’t understand why the PS3 died a year later.
Parents
  • maxpowerr
    maxpowerr over 2 years ago

    Interesting information. I just don’t understand why the PS3 died a year later.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to maxpowerr

    I specifically purchased a PS3 just to try the processor, but around that time Sony killed support for Linux for it : ( They deliberately removed advertised functionality in a firmware update that couldn't be undone.

    The cooling wasn't that great, and some of the earlier ones overheated (I got my reflow oven from someone who made a bit of a living for several years by repairing PS3s in it!). I was glad to be rid of the PS3 to be honest! It was a super-interesting chip at the time though.

    I don't recall the PS3 only being around for a year though. I thought it was much longer (i.e. it was a success for Sony I thought - I know nothing about Playstations though).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 2 years ago in reply to shabaz

     shabaz Nope some distros support the CELL CPU and the ps3. ~~Cris

    there are two problems first you have to "jail-break" the system, and btw you still can't get into the GPT! Maybe but then you need a new ROM/EPROM, etc. 

    next, find a tutorial on YouTube for installing the distro.  It really is underwhelming when all is said and done. But I never wanted to load the whole OS I need something small and stripped down to do my 3d math transforms for the simulator,  Apparently, the  8 cells are very good at this kind of stuff. So I am thinking of more as a coprocessor. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • phoenixcomm
    phoenixcomm over 2 years ago in reply to shabaz

     shabaz Nope some distros support the CELL CPU and the ps3. ~~Cris

    there are two problems first you have to "jail-break" the system, and btw you still can't get into the GPT! Maybe but then you need a new ROM/EPROM, etc. 

    next, find a tutorial on YouTube for installing the distro.  It really is underwhelming when all is said and done. But I never wanted to load the whole OS I need something small and stripped down to do my 3d math transforms for the simulator,  Apparently, the  8 cells are very good at this kind of stuff. So I am thinking of more as a coprocessor.