Essentials
  • Learn
  • Learning Center
  • Essentials
  • More
  • Cancel
Essentials
Forum Ohms law
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Essentials to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 27 replies
  • Subscribers 1042 subscribers
  • Views 7795 views
  • Users 0 members are here
  • ohms law
Related

Ohms law

salesm21
salesm21 over 8 years ago

To anyone who can help,

I have been recently wondering about something rather simple. Why is it in ohms law does R=V/I & I=V/R? This means that voltage is proportional to both resistance and current? I know the more voltage you have the more energy is given to each coloumb of charge but why is it that when 1 volt of energy is in 1 C of charge is there 1 ohm?

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 8 years ago +8
    Hi Mitchell, Let's imagine that we have a perfect source of 10 volts with no internal resistance. What ohms law does is give us a formula for calculating the current in a circuit if we know the resistance…
  • jw0752
    jw0752 over 8 years ago in reply to gdstew +8
    Hi Gary, While I tend to agree with you, if one really has a scientific thought process we have to leave open the possibilities. The scientific community went 200 years believing that they had things all…
  • mcb1
    mcb1 over 8 years ago in reply to michaelkellett +8
    michaelkellett I'm with you. I've managed all these years without worrying about the unseen things causing it to happen. Quite frankly I don't really care which way they actually move, as long as something…
Parents
  • DAB
    DAB over 8 years ago

    Hi Mitchell,

     

    You need to understand the issues involved.

    Charge flow occurs when you establish a potential (EMF measured as voltage) through a conductor.

    Every conductor has some level of resistance due to impurities in the material.

    As the charge flows through the conductor, the mass/energy is passed from atom to atom.  The conductor atoms are arranged in a crystal structure and can easily pass each photon from atom to atom.  When the photons reach an atom of different type (impurity), that atom may emit a photon of a different type (usually IR), which reduces the amount of charge through the conductor.  That is why wires get warm when you pass a lot of current through them.  Their residual resistance caused by the impurities causes some of the current to be released as IR photons.

     

    In a superconductor, the atoms are all at their minimum energy state, which allows them to pass the photons between atom without emitting any IR photons, but the impure atoms will release photons of higher frequencies.  So there is still some loss, but in general, even the impure atoms will mostly pass the charge with less loss.

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 8 years ago in reply to DAB

    Not photons, electrons. And while impurities do cause resistance I'm fairly certain that electrons bouncing off the atoms of the conductor,

    and imparting energy on those atoms in the form of heat is the main source of resistance in "pure" conductors.

     

    P.S. It was Ben Franklin that first postulated that electric current was the flow of "particles" in conductors. It was over a hundred

    years later that the electron was finally discovered as that particle in experiments with early cathode ray tubes.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 8 years ago in reply to gdstew

    Hi Gary,

     

     

    No, I really meant photons.  I have done extensive research into subatomic physics over the last nine years and I have found that there is NO experimental evidence to support the idea that electrons are either a part of atoms or flow between atoms in electronic devices.

     

    The mathematical proofs we present in my book "Reverse Engineering The Universe" show that the atom is more likely to have a shell of captured photons instead of the accepted orbiting electrons.  The photon model shows that you get a better understanding of how mass/charge flows between atoms to support all of the macro-level attributes associated with electron flow.

     

    My photon flow model works very well to explain how and why V = I*R works at all levels from sub-atomic to Universe level events.

     

    I know this idea runs contrary to everything everyone has been told or taught, but so far my models do a much better job of explaining actual electronic measurements at the atom and subatomic level.

     

    DAB

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 8 years ago in reply to DAB

    Based on the overall success of modern electronics from over a hundred years of research by some of the greatest minds in science

    and engineering I'll stick with everybody else is right and you are wrong. Thanks anyway.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 8 years ago in reply to gdstew

    Hi Gary,

     

    While I tend to agree with you, if one really has a scientific thought process we have to leave open the possibilities. The scientific community went 200 years believing that they had things all figured out until Einstein showed them that at high speeds and high gravities the universe is not quite as simple as Newton portrayed it. I have looked briefly at DAB  's theories and I even bought his first book. If there is merit to his new ideas, at least, at the level that I do physics it is not worth changing from my familiar view. I believe that he might have better luck explaining things if the terminology did not overlap so much between his theory and the standard model. In the end I have chosen to stay with the standard theory of physics and not try to make the transition to something new. However, at this point, I would hesitate to tell DAB that he was wrong. We have even seen instances where two seemingly competing theories turned out to simply be the same but viewed from different mathematical perspectives. The test will be when DAB can propose an experiment whose result is correctly predicted by his approach and isn't correctly predicted by the current approach. I will keep my mind open but in the meantime, for me, electricity will remain the drifting of electrons through a conductor.

     

    John

    • Cancel
    • Vote Up +8 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 8 years ago in reply to gdstew

    That is fine.

     

    I am challenging everything everyone thinks they know about subatomic physics.

     

    I fully understand that nearly everyone will reject my ideas and findings.

     

    That said, the math proofs and data analysis of my theory versus conventional thought has clearly shown that I just might be right.

     

    My wife added a warning to the book for all students to not read the book until they are out of school and ready for independent thought.

     

    All I ask is for everyone to have an open mind and ask themselves honestly, just how well do you really understand what goes on when charge flows.  So far, I find many people really just accept the conventions, even when they defy logical conclusions.

     

    Case in point, Werner Heisenberg claimed that you cannot measure the positon of an electron around an atom because you cannot know its position at the time of measurement.

     

    Yet, if you take his data, he confirms the location of small mass/charge objects at roughly 10-34 meters, which is approximately the size of captured photons in my model.

     

    My model also validated he measurements by Niels Bohr when he found that all atoms appeared to have a diameter of about .5 * 10-10 meters, which is exactly where we found the balance point of the photon shell around the atomic nucleus for all atoms.

     

    So my work continues, but stacked up against accepted theory, I am beating the pants off all of the basic atomic assumptions.

     

    I use element14 as a sounding board to see if I can entice knowledgeable people to interact with.

     

    DAB

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 8 years ago in reply to jw0752

    Hi John,

     

    In my latest update, I do propose a simple experiment to demonstrate my point.

     

    Take a glass tube with two electrodes on each end and fill the tube with only Hydrogen gas.

     

    Then apply voltage across the tube.

     

    What you will find is a stream of photons moving between the two electrodes. If you measure the current at each end of the tube, you will find a loss of charge running through the tube as the photons are emitted.

     

    If you use the electron model, then you should see each Hydrogen atom dissociate as an electron is ripped from its orbit, leaving a pile of protons at the bottom of the tube and little or no Hydrogen gas remaining inside the tube after a short period of operation.

     

    So how sure can you be that electrons are flowing instead of photons?

     

     

    A spectrometer shows a very wide range of photons being released between the two electrodes and a simple pressure check will show that no Hydrogen gas was lost during operation.

     

    Since photons are released every time you draw an electrical arc, why is photon flow such a difficult idea?

     

    Has anyone actually seen an electron flow through a wire?

     

    Just saying.

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • DAB
    DAB over 8 years ago in reply to jw0752

    Hi John,

     

    In my latest update, I do propose a simple experiment to demonstrate my point.

     

    Take a glass tube with two electrodes on each end and fill the tube with only Hydrogen gas.

     

    Then apply voltage across the tube.

     

    What you will find is a stream of photons moving between the two electrodes. If you measure the current at each end of the tube, you will find a loss of charge running through the tube as the photons are emitted.

     

    If you use the electron model, then you should see each Hydrogen atom dissociate as an electron is ripped from its orbit, leaving a pile of protons at the bottom of the tube and little or no Hydrogen gas remaining inside the tube after a short period of operation.

     

    So how sure can you be that electrons are flowing instead of photons?

     

     

    A spectrometer shows a very wide range of photons being released between the two electrodes and a simple pressure check will show that no Hydrogen gas was lost during operation.

     

    Since photons are released every time you draw an electrical arc, why is photon flow such a difficult idea?

     

    Has anyone actually seen an electron flow through a wire?

     

    Just saying.

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • jw0752
    jw0752 over 8 years ago in reply to DAB

    Hi DAB,

     

    When the difference in potential is put across your tube of hydrogen,  electrons are accelerated  and their increased velocities are the means by which energy is transferred to the hydrogen atoms. When there is electron - electron interaction energy is transferred to orbital electrons. These orbital electrons then emit a photon as they jump back to a lower energy level in the atom. There are cases where an electron is removed but it is quickly replaced with another and again photons of specific energies are released as it falls back into lower energy states.

     

    I do not understand why you say that I will find a stream of photons moving between the potential difference. Photons would be undetectable and they have no reason to move as they are not affected by an electric field. I might see a source of photons between the two potential terminals but these are successfully explained by the interaction of electrons with orbital electrons and their subsequent returning to lower energy levels.

     

    There is no need for the atoms to disassociate. Electrons are being supplied and recovered by the potential difference and the net ionization of the hydrogen gas will likely remain fairly stable. I am not sure what the characteristics are of the protons in your physics but from the standard theory they are positively charged which would cause them to repel one another. They would not accumulate at the bottom of the tube. Gasses that have a lot of ions are called a plasma and exist at very high temperatures such as your arc, in areas where the particle density is too low for easy recombination like the upper atmosphere or in places like the Sun's atmosphere where there is heat and low density. Even in plasma there is likely a net neutrality of charge.

     

    Using an ideal gas model you may be able to calculate the amount of hydrogen in the tube by measuring temperature and pressure. I would not expect this to change under the standard model up until the point where temperature became great enough for the gas to transition to a plasma. Frankly I do not know if the ideal gas law applies to plasma.

     

    If photons were affected by an electric field as you seem to indicate I should be able to place an electric field between my eyes and a light source and modulate the flow of the photons. This would produce a distortion that is not observed in experiments.

     

    Your ideas are interesting and always spark a discussion. Nothing that I do or experiment with has any need to have a precise theory at the molecular level. I like

    michaelkellett 's previous post as it accurately reflects how I feel. In the mean time when I feel like trying to imagine the atomic world I am comfortable with the standard theory even though I suspect that future revelations will tweak it towards more perfection without the radical change that you propose.

     

    John

    • Cancel
    • Vote Up +5 Vote Down