Essentials
  • Learn
  • Learning Center
  • Essentials
  • More
  • Cancel
Essentials
Forum Advice needed! Need to re-wire an air pump with special features...
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Essentials to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 1039 subscribers
  • Views 2259 views
  • Users 0 members are here
Related

Advice needed! Need to re-wire an air pump with special features...

ellbobeee
ellbobeee over 8 years ago

Hi there,

 

I have a technical 'problem' which a Farnell employee thought might be worth posing to the community on here.

 

I am an artist and I am looking to make a 'breathing' sculpture.

 

I have started by buying a battery operated air pump (designed for mattresses etc.) which has a power supply input bit so that the batteries (7.5V DC 300mA) can be re-charged when the pump is not in use.

 

What I had hoped to be able to do was re-wire the pump to include a) a dial which allows me to lessen the speed of the fan (or can this be done by using lower voltage batteries?) and b) to solder in a sort of intermittent timer so that the fan comes on and off every 5 seconds or so, giving the impression of breathing.

 

If anyone can help with this I would be very grateful! I don't have much of a budget... :-)

  • Sign in to reply
  • Cancel
Parents
  • krappleby
    krappleby over 8 years ago

    I would opt to use an arduino, to control everything,

    using some relatively simple programming you can control the fan on time off time, speed plus other options, i believe you would have a lot more control over it also.

    You would need to add a relay or transistor to turn the unit on and off, as the arduino cannot handle that sort of power, but you could with a power regulator reduce that 7.5v down to run the arduino

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • krappleby
    krappleby over 8 years ago

    I would opt to use an arduino, to control everything,

    using some relatively simple programming you can control the fan on time off time, speed plus other options, i believe you would have a lot more control over it also.

    You would need to add a relay or transistor to turn the unit on and off, as the arduino cannot handle that sort of power, but you could with a power regulator reduce that 7.5v down to run the arduino