Essentials
  • Learn
  • Learning Center
  • Essentials
  • More
  • Cancel
Essentials
Documents Tools & Test Equipment: Optical Spectrometers
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Essentials to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: pchan
  • Date Created: 21 Aug 2021 1:42 AM Date Created
  • Last Updated Last Updated: 3 Sep 2024 1:20 PM
  • Views 7358 views
  • Likes 16 likes
  • Comments 31 comments
Related
Recommended

Tools & Test Equipment: Optical Spectrometers

Electromagnetic (EM) radiation consists of a broad spectrum of different wavelengths of light, both visible and invisible to the human eye. This spectrum can be analyzed using optical spectroscopy. An optical spectrometer breaks up light into a higher number of bands, and these spectral components of light can be used to analyze the characteristics of a wide range of materials. Spectrometers are key test instruments in multiple fields, from industrial to scientific research. They play crucial roles in several applications, including Process Control and Monitoring, Environmental Quality Analysis, Medical Diagnostics, Quality Control, Chemical Analysis, and Material and Polymer Analysis. In this learning module, we discuss different kinds of spectrometers, the basic concepts underlying the operation of an optical spectrometer, and various use cases.

2. Objectives

Upon completion of this module, you will be able to:

image Explain the different types of spectrometers

image Understand the basic concepts and workings of an optical spectrometer

image Discuss Broadcom’s Q-series (Qwave, Qmini, Qneo) spectrometers

image Discuss applications using spectrometers

3.Scope

Back to Top

A spectrometer is an instrument that measures the variance of physical characteristics over a provided spectrum range. For example, a mass spectrometer measures the mass-to-charge ratio spectrum, and an NMR spectrometer measures the contrast of nuclear resonant frequencies.

One common application for spectrometers is analyzing food and agricultural samples. Near-infrared (NIR) spectrometers use light at NIR wavelengths to penetrate food samples, allowing the analysis of the composition inside the sample without causing any damage.

Different types of spectrometers are available, with common ones being optical spectrometers, nuclear magnetic resonance (NMR) spectrometers, and mass spectrometers. Optical spectrometers measure the characteristics of light and materials identified through variation in light intensity absorption and emission, along with wavelength. NMR spectrometers observe and evaluate the interplay of nuclei spins of a sample placed in a strong, sustained magnetic field. Mass spectrometers measure the mass-to-charge ratio of one or more molecules present in a sample and identify its composition of elements. Mass spectrometers have an ionization source that produces ions from the sample chemical substance under analysis, after which molecular weight can be determined using electric and magnetic fields.

The scope of this learning module is limited to optical spectrometers, the different types, their working principles, and Broadcom Q-series spectrometers, including Qwave, Qmini, and Qneo, along with their use case applications.

4. Basic Concepts

Back to Top

An optical spectrometer measures a sample's intensity of absorption, scattering, reflection, or emission of radiation in the spectrum's ultraviolet, infrared, or visible region (as illustrated in Figure 1). Materials in the sample can be recognized with changes in the absorption and emission of the light intensity at different wavelengths. All optical spectrometers share a common aspect: a wavelength selection mechanism.

Click below to enlarge image:

image

Figure 1: Electromagnetic Spectrum

Figure 2A illustrates the technological process of the optical spectrometer. Light enters through a narrow entrance slit. The slit size limits the amount of light to be measured and influences the spectrometer's optical resolution; a smaller slit size equals better resolution. The beam starts to spread, or becomes divergent, after it proceeds through the slit. A first mirror is used to collimate the beam, or to make the beam’s rays parallel. The collimated rays are then directed towards a grating, which separates the light into different wavelengths.

image

Figure 2A: The inside / technology of the optical spectrometer.

image
image

Figure 2B & C: Spectrometer measurement set up

A diffraction grating separates different wavelengths of light by reflecting them at different angles. The light reflected off the diffraction grating becomes divergent once again, and must be collimated, again using a collimating mirror. The collimated rays are then directed towards a detector, which measures the intensity of light for each of the wavelengths. The resulting data can be uploaded to a computer for further analysis. Contemporary spectrometer systems interact with computers via USB, Ethernet, or RS-232. Technological advances have enabled newer systems to transfer data wirelessly, via Bluetooth and Wi-Fi.

- 4.1 Optical Spectrometer Types

Wavelength

image Ultraviolet (UV) Spectrometers

A UV spectrometer measures light absorption spanning the electromagnetic spectrum's ultraviolet range (between 180-400 nm) to determine the composition of the sample. The molecules in the sample absorb the energy from the UV light, exciting their electrons. The level of excitement is proportional to the wavelengths that each type of molecule can absorb, and these levels are used to determine the types of molecules present in the sample. A standard UV Spectrometer typically uses a deuterium arc, tungsten halogen, or xenon arc lamp as a light source. The detector can be a PMT, CCD, photodiode, or photodiode array. UV spectroscopy is employed by analytical chemists for quantitative diagnosis of different analytes, like transition metal ions, biological macromolecules, and highly conjugated organic compounds.

image Visible (VIS) Spectrometers

A VIS spectrometer works in a similar fashion as a UV spectrometer; however, light in the electromagnetic spectrum's visible region (380-750 nm) is used instead. VIS and UV spectrometers share common applications and, by extension, industries as well. Many spectrometers are UV-VIS spectrometers, which cover both spectrums.

image Near Infrared and Infrared (NIR & IR) Spectrometers

Near infrared and infrared spectrometers use infrared (750 nm to 1 mm) radiation to induce vibrations in the molecules of a sample. Because different molecules absorb specific frequencies that are characteristic of their structure, measuring the absorption of the sample for a range of wavelengths can successfully identify its chemical composition. NIR & IR spectrometers are used in various applications such as protein characterization, nanoscale semiconductor analysis, space exploration, and compound identification.

Light Interaction

Spectrometers work on different principles, taking advantage of the behavior of light in order to make their measurements. These are some examples of how spectrometers function.

image Absorption Spectrometers

Absorption spectrometers measure the radiation absorption of a given sample. In any sample, the absorption intensity changes with the frequency of the light, and this variation is used to generate an absorption spectrum. The absorption spectrum is effective at determining the concentration of compounds present within a sample. Absorption spectrometers are found in remote sensing, atomic and molecular physics, and astronomy. The UV, VIS, and NIR spectrometers previously discussed have been described as absorption spectrometers.

image Reflectance Spectrometers

image

Figure 3: The operating principle of reflectance spectrometers

Reflectance spectrometers measure the quantity of scattered or reflected light from a sample. Figure 3 illustrates the scattering of light reflected from or passing through a sample after it has arrived from the light source. A detector, usually a CCD or photodiode, measures the light reflected throughout the spectrum, enabling a reflectance versus wavelength plot to be generated. Reflectance spectrometers are widely used in the medical industry to offer information related to tissue concentration. They are also used in environmental science and geology.

image Transmittance Spectrometers

image

Figure 4: The operating principles of transmittance spectrometers

Transmittance spectrometers measure the amount of light that a sample lets flow through it unaffected. Figure 4 illustrates the typical setup of a transmittance spectrometer. The wavelengths where the sample absorbs the least will have the highest amount of transmission, and vice versa. Transmittance spectrometers are frequently used in pharmaceutical analysis.

image Scattering Spectrometers

Scattering spectrometers measure the amount of light that is scattered when it passes through a sample. While most light continues on its original path when passing through a material, some photons change course. This is caused by the light’s energy exciting the vibrational modes of the molecules in the material, and scattering it at a diminished energy level. This is known as Raman Scattering or the Raman Effect. The vibrational change in the sample can be analyzed to determine properties like chemical composition, crystallinity, and molecular interactions. Scattering Spectrometers are commonly used in the chemical and pharmaceutical industries, where they help with tasks such as identifying molecules, investigating chemical bonding, and discovering counterfeit drugs inside packages.

image Raman Spectrometers

Raman spectrometers take advantage of the way light interacts with the chemical bonds in a sample. A Raman spectrometer uses a filter designed to remove light scattered by other methods (such as Rayleigh scattering) in order to limit the measurements to Raman scattered light. The filtered light is then used to generate the Raman spectrum of the sample. The light source in Raman spectrometers is a continuous-wave laser. Raman spectrometers analyze the material and produce data related to chemical structure, impurity, contamination, phase and polymorphism, and intrinsic stress/strain.

- 4.2 Broadcom’s Optical Spectrometer Range

Broadcom’s range of compact modular spectrometer devices include the Qwave, Qmini, and Qneo series for UV–VIS–NIR measurements ranging from 190 nm to 1700 nm. Based on the Czerny-Turner configuration, these spectrometers lack moving parts, which avoids optical misalignment and ensures reliable and stable long-term performance. All devices have good thermal stability and are factory-calibrated. Broadcom spectrometers are used in applications such as process control and monitoring, biomedical applications, chemical research, environmental analysis, medical and pharma applications, forensic analysis, and more.

image Qwave Series: this series is fitted with a high-resolution 3648-pixel linear CCD detector featuring optimal resolution down to 0.2 nm, a focal length of 75 mm, a high dynamic range of up to 1500:1, and spectral coverage ranging from 220 to 1030 nm covered by three wavelengths configurations. The Qwave series can cope with most setups, while maintaining a relatively small size of 89.5 × 68 × 19.5 mm. This series is intended for more critical spectral analysis, where the high resolution and throughput of the spectrometer are required. AFBR-S20W2VI is a good example from this series.

image Qmini Series:  The Qmini Series covers a wide spectral range, starting at 220 nm up to 1100 nm. Its compact size (64 x 42 × 14.5 mm) allows it to be easily integrated into space-constrained applications, making it an appropriate solution for mobile analysis. Onboard processing capabilities save the processing cycles of the host controller, making it possible to use them in IoT setups or similar MCU or MPU-driven applications. Despite their size, these spectrometers deliver a variety of functionalities and connectivity options common to all Q-series spectrometers. AFBR-S20M2VI and AFBR-S20M2WU are some examples from the Qmini series.

image Qneo Series: The Qneo series is a pocket-sized NIR spectrometer designed for sensitive measurements between 950 and 1700 nm. The compact form factor of 60 x 40 x 19 mm provides versatility in integrating the spectral sensor in a process analyzing system (PAT) or handheld device for point-of-care diagnostics (POC). The thermal stability of the electro-optical system is important to spectrometer performance over the full temperature range -15°C to +55°C (5°F to 131°F). This series features a spectral resolution of 8 nm [FWHM], integrated electronics with full system calibration, and serial interfaces (USB, SPI, and UART). In addition, they are equipped with an uncooled 256-pixel InGaAs array in an ultra-compact design. AFBR-S20N1N256 is an example of this series.

- 4.3 Application Software

All Q-series spectrometers can be used with Broadcom’s complimentary Waves Spectrometer software, which simplifies data acquisition and spectra evaluation. This software features:

image Capture and display series of spectra

image Automatic exposure control with dark spectrum interpolation

image Ability to import and export ASCII based files

image Comprehensive tools for displaying and analyzing spectra

image Strip charts for comparing characteristic values between multiple spectra, including peak follower in real-time

image Transmission, absorption, and reflection measurements

The Waves Software is a useful tool for evaluation. For OEM integration, a software development kit (SDK) with several device commands is online to start the implementation.

image

Figure 6: Waves Main Interface Window

5. Analysis

Back to Top

Optical spectrometers are used for material analysis in a wide variety of fields in engineering and science. We will now analyze some specific optical spectrometer use case applications.

Spectral Analysis of Water with the Qmini UV Spectrometer

Dissolved nitrate in water is difficult to detect without testing, as it is odorless, tasteless, and colorless. Nitrate-nitrogen contaminated drinking water causes harm when the nitrate changes into nitrite within the digestive system. Nitrite causes the iron component of the RBC hemoglobin to oxidize, forming methemoglobin. The latter cannot carry oxygen like hemoglobin and creates a condition termed methemoglobinemia (aka "blue baby syndrome"), where oxygen absence in the individual body cells causes the skin and veins to appear blue. A lab water test for nitrate is essential for families with infants, nursing mothers, pregnant women, or the elderly.

Ultraviolet-visible (UV-Vis) spectroscopy can effectively detect contaminant quality and quantity in an aqueous environment. The Qmini UV (AFBR-S20M2UV) and Qmini WIDE UV (AFBR-S20M2WU) spectrometers can be a good fit for online detection of nitrite and nitrate content in waste and freshwater. They can also effectively measure turbidity within the VIS range. The lower UV range (< 200 nm) absorbance spectroscopy determines the nitrite/nitrate concentration. The Qmini spectrometer with adjusted starting wavelengths at approximately 189 nm enables real-time monitoring in line and at the line without taking samples.

image

Figure 7: Detection of nitride and nitrate content in waste and fresh water using the Qmini spectrometer

Detection of Pathogens in Food and Feed with the Qwave Spectrometer

Optical spectroscopy can also detect harmful pathogens contaminating food and feed in a processing line. Spectroscopy is very effective in the bioanalysis of samples, and can perform this analysis without destroying the sample. With absorbance spectroscopy, the Qwave AFBR-S20W2XX series spectrometer can detect the existence and concentration of labeled pathogens. The Qmini WIDE (220 -1000 nm) can also be used, due to its broad spectral range and the fact that it covers various measurement tasks with a single device in an analyzer system.

image

Figure 8: Detection of pathogens in food and feed using Qwave or Qmini spectrometers

Environmental Analysis with Qneo Spectrometer

The spectral analysis of environmental and geological irradiance is a spectrometer application where optical spectrometers are used to identify spectrally and physically distinctive features of different surface materials and rock types. Environmental analysis includes environmental moisture, solar radiation, and temperature. Qneo NIR (AFBR-S20N1N256) and Qmini (AFBR-S20M2XX) spectrometers are ideal for such applications, because they can measure the amplitude and wavelengths of light emitted in the near-infrared and visible range, and are easily integrated into handheld solutions. Broadcom provides the SDK that guides communication with the spectrometer using various digital interfaces, programming languages for software development, and facilitates communication with embedded microcontrollers.

image

Figure 9: Spectrometer in geological and environmental applications using Qmini or Qneo spectrometers

image Charge Coupled Device (CCD):  a light sensitive integrated circuit capable of converting light into electronic data.

image Diffraction Grating:  a type of monochromator that separates light into a range of individual wavelengths, using a number of parallel, closely spaced slits.

image Electromagnetic (EM) Radiation:  a form of energy traveling in waves at the speed of light, spanning a broad spectrum.

image Infrared (IR):  the range of frequencies of radiant energy or light invisible to the human eye, but able to be felt as heat. Infrared is divided into 3 spectral regions: near-infrared (750 – 1300 nm), mid-infrared (1300 – 3000 nm), and far-infrared (3000 – 1mm).

image Monochromator:  an optical device that separates light into a range of individual wavelengths. Examples of monochromators are prisms and diffraction grating.

image Nuclear Magnetic Resonance (NMR):  a phenomenon where molecules react to a magnetic field by producing an electromagnetic signal with a frequency characteristic of the magnetic field at its nucleus.

image Photon Multiplier Tube (PMT):  a type of vacuum tube capable of detecting light in the UV, visible, and near-infrared ranges of the electromagnetic spectrum.

image Serial Peripheral Interface (SPI):  a synchronous communication interface for short distance communication, typically used to send data between microcontrollers and small peripherals.

image Spectrometer:  an optical instrument used to measure the variation of physical characteristics over a frequency range in a given spectrum of light.

image Visible (VIS): refers to the range of frequencies of light visible to the human eye. The range starts at around 380 nm (violet) and extends to approximately 750 nm (red).

image Ultraviolet (UV):  the range of frequencies of radiant energy or light that falls between the visible spectrum and X-rays. UV is generally divided into 3 spectral regions: UVA (315-400 nm), UVB (280-315 nm), and UVC (180-280 nm).

image Universal Asynchronous Receiver/Transmitter (UART): a hardware communication protocol that provides asynchronous communication between devices.

image Universal Serial Bus (USB): an industry standard for connectors and communication protocols, widely used for connecting peripherals to computers.

*Trademark. Broadcom is a trademark of Broadcom Inc. Other logos, product and/or company names may be trademarks of their respective owners.

Related ComponentsBack to Top

image

The element14 ESSENTIALS of Optical Spectrometers discusses different kinds of spectrometers, the basic concepts underlying the operation of optical spectrometers, and various use cases. To extend the knowledge covered in the main module, this supplementary guide discusses the types of Broadcom Q-Series spectrometers.

Spectrometers

The Qneo AFBR-S20N1N256 Near NIR spectrometer is designed for industrial integration. Equipped with an uncooled InGaAs sensor array, the Qneo enables professional measurement between 950 nm and 1700 nm. On a footprint smaller than a credit card, the Qneo features a rugged setup that combines high resistance in industrial environments and high optical performance.

 

image

AFBR-S20N1N256, Spectrometer, 950 nm, 1700 nm, 8 nm, NIR, 40 mm, SMA Connector

Buy Now

image Wavelength range: 950-1700 nm

image Spectral resolution (FWHM): 8nm

image Dynamic Range: 12000:1

image Detector: 256 pixel linear uncooled InGaAs sensor

image Dimensions: 60.0 x 50.0 x 19.0 mm

 

This is a miniature USB spectrometer with on-board electronics and communication interfaces for UV–VIS–NIR measurements. The Qmini spectrometer offers a small design to enable tight integration to suit a large number of OEM requirements.

 

image

QMINI WIDE-UV Spectrometer, 225 nm, 1000 nm, 1.5 nm, CCD, 50 mm, SMA Connector

Buy Now

image Six wavelength configurations from 190 nm–1100 nm

image Spectral resolution from 0.3–1.5 nm

image Miniature size

image Powerful on-board electronics with processing and evaluation

image Customizable wavelength range, sensitivity, resolution and interfaces

image Application software and Software Development Kit

image Dimensions: 64.0 x 42.0 x 14.5 mm

 

Qmini AFBR-S20M2XX is a Miniature Spectrometer with Onboard Processing for Mobile Applications and Industrial Integration. Its compact design enables tight integration in applications where space is limited, like mobile analysis devices. The Qmini includes a powerful electronics board that enables:

 

image

QMINI VIS, Spectrometer, 370 nm, 750 nm, 0.7 nm, CCD, 50 mm, SMA Connector

Buy Now

image Full processing of spectra in the device (offset, nonlinearity, dark spectrum, and spectral sensitivity)

image Averaging and smoothing

image Binning and buffering of spectra

image A replaceable entrance slit, reduced stray light, and lower power consumption.

 

Within a very small design, the Qmini delivers technical specifications that are unprecedented at this size. Its compact design enables tight integration in applications where space is limited, like mobile analysis devices. The Qmini includes a powerful electronics board that enables:

 

image

QMINI UV, Spectrometer, 220 nm, 400 nm, 0.3 nm, CCD, 50 mm, SMA Connector

Buy Now

image Wavelength range: 220 nm to 400 nm

image Spectral Resolution: 0.3 nm

image Full processing of spectra in the device (offset, nonlinearity, dark spectrum, and spectral sensitivity)

image Averaging and smoothing

image Binning and buffering of spectra

image A replaceable entrance slit, reduced stray light, and lower power consumption.

 

Within a very small design, the Qmini delivers technical specifications that are unprecedented at this size. Its compact design enables tight integration in applications where space is limited, like mobile analysis devices. The Qmini includes a powerful electronics board that enables:

 

image

QMINI NIR, Spectrometer, 730 nm, 1080 nm, 0.7 nm, CCD, 50 mm, SMA Connector

Buy Now

image Wavelength range: 730 nm to 1080 nm

image Spectral Resolution: 0.7 nm

image Full processing of spectra in the device (offset, nonlinearity, dark spectrum, and spectral sensitivity)

image Averaging and smoothing

image Binning and buffering of spectra

image A replaceable entrance slit, reduced stray light, and lower power consumption.

Spectrometer Accessory

 

image

AFBR-S20SK-V2, Test Equipment Kit, SMA 905 Connector, Hexagon Socket Screw Key

Buy Now

AFBR-S20SK-V2 is a Slit Evaluation Kit for Broadcom spectrometers, simplifying the spectrometer evaluation process with interchangeable slits. This kit enables the quick changing of slit sizes when evaluating the spectral performance of Qmini or Qwave in the field.

For more available products Shop Now


Test Your KnowledgeBack to Top

image

Are you ready to demonstrate your knowledge of Optical Spectrometers? Then take a quick 10-question quiz to see how much you've learned. To earn the Tools & Test Equipment III Badge, read through the learning module, attain 100% on the Quiz, leave us some feedback in the comments section, and give the learning module a star rating.

Attachments:
image Tools&TestEquipment3.pdf

element14 Learning Center

image
Tools & Test Equipment III: Optical Spectrometers

Sponsored byimage


1. Introduction | 2. Objectives | 3.Scope | 4.  Basic Concepts | 5. Analysis | Related Components | Test Your Knowledge image
  • spectrometer calibration
  • light measurement tools
  • optical spectrometer applications
  • spectrometer test equipment
  • spectrometer basics
  • optical spectrum analyzer
  • optical spectrum analysis
  • bcom-e14
  • spectrometer tools
  • spectrometer wavelength analysis
  • optical spectrometers
  • spectrometer essentials
  • spectrometer technology
  • optical testing equipment
  • optical measurement tools
  • tools_and_test_equipment
  • optical_spectrometer
  • ess_module
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • beacon_dave
    beacon_dave over 5 years ago +5
    An interesting subject area. They may be pocket-sized but at circa £5k a time you had perhaps better double-check your pockets before doing the laundry...
  • fmilburn
    fmilburn over 5 years ago +3
    If you follow my posts on element14 you know I like optical spectrometers. How could I have missed number 8?
  • dougw
    dougw over 5 years ago +3
    For a few years this type of stuff was an everyday topic at my work.
Parents
  • will06
    will06 over 1 year ago

    Interesting subject

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • will06
    will06 over 1 year ago

    Interesting subject