555 Timers
  • Technologies
  • More
555 Timers
Forum Understanding 555 timer in astable mode but stuck on capacitors
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 555 Timers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 14 replies
  • Answers 7 answers
  • Subscribers 53 subscribers
  • Views 9264 views
  • Users 0 members are here
  • capacitor
  • 555 timer
Related

Understanding 555 timer in astable mode but stuck on capacitors

opalko
opalko over 5 years ago

So I am still plowing my way through Platt's Make: Electronics and into chapter 4 working with the 555 timer IC.  The astable mode of the timer is giving me trouble as I don't understand how

 

When C1 acquires 2/3 of the positive voltage powering the circuit, the 555 reverses its output on Pin 3 from positive to negative and forces C1 to discharge itself through R2.

(This last sentence is actually from Make Magazine issue 10 where Platt is explaining the same thing as in chapter 4 of his book - see image below)

 

image

 

What I am confused about is the discharging through R2.  I am obviously stuck on what is going on with C1. As I understand it, it first gains a positive charge on what I will call the top plate in the picture above, and a negative charge on the bottom plate (next to where the label C1 is).  Maybe I have read too many analogies of water with electricity but I think of the capacitor as a balloon (in fact there are many analogies in Platt's book like this).  So how is the balloon releasing the pressure in what seems like a reverse direction back through R2?  Here is a similar circuit I found on circuitlab albeit the pins arranged differently and it shows that reversing of "flow":

 

image

 

Is there not +5V into R2 from R1 at the same time C1 is discharging??

Finally here is Platt's "internal" view of the 555 timer in astable mode.  I assume pin 7 gets grounded to pin 3 but I am still confused about the seemingly reversal of flow through R2.

 

image

I've read through this many times and still stuck. Any additional help is appreciated!

 

Cheers

 

Message was edited by: Robert Opalko same day

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 5 years ago +6 verified
    Hi Robert, During the discharge part of the cycle the Pin 7 is attached to ground. (see the blue - in the last picture). Once pin 7 is connected to Ground the electricity in C1 starts to move through R2…
  • jw0752
    jw0752 over 5 years ago in reply to opalko +6 suggested
    Hi Robert, The polarized capacitors must be used in the correct polarity as they will fail if more than a token voltage is applied in the reverse direction. The polarity on the capacitor is not like that…
  • jw0752
    jw0752 over 5 years ago +5
    PS you are doing an excellent job of presenting your questions. I would bet that several times you have actually answered them yourself in the process of preparing the question. John
Parents
  • jw0752
    0 jw0752 over 5 years ago

    Hi Robert,

     

    During the discharge part of the cycle the Pin 7 is attached to ground. (see the blue - in the last picture). Once pin 7 is connected to Ground the electricity in C1 starts to move through R2 and into the Ground. The grounding of Pin 7 does also connect R-1 to Ground but this has nothing to do with R2 and C1 at this time since there is a ground between them. The last picture also shows that Pin 3 is connected to ground at this time but here again it has nothing to do with R2 and C1 since there is a ground between them.

     

    image

     

    See if this helps? Keep in mind that the ground that I drew outside of Pin 7 is actually inside the chip and it is temporary. As soon as the charge on C1 hits 1/3 of Vcc it once again goes open and allows the current coming from R1 to recharge C1 through R2.

     

    John

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • opalko
    0 opalko over 5 years ago in reply to jw0752

    Thank you that makes it more obvious now with your diagram.  I should have realized R1 would flow the same way into ground.  See my question below to Jon about polarized vs non-polarized caps..would that matter? 

     

    I wish I could mark 2 answers as correct here, both are such good explanations.


    Cheers

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 5 years ago in reply to opalko

    Hi Robert,

     

    The polarized capacitors must be used in the correct polarity as they will fail if more than a token voltage is applied in the reverse direction. The polarity on the capacitor  is not like that of a diode. In the case of the polarized capacitor if you hook it up in the proper polarity it will work and if you hook it up in the incorrect polarity it will conduct  current, get hot and potentially explode provided there is enough energy available in the circuit. Generally speaking the electrolytic capacitors have higher values of capacitance for their size than do the non-polarized types. There are other differences too but probably not important to this application. The number and variety of components that can be used to make any particular circuit application is what makes electronics an art. The 555 that you are working with is a great example. There are literally hundreds of different applications that it can be applied to. Check out:

     

    http://www.talkingelectronics.com/projects/50%20-%20555%20Circuits/50%20-%20555%20Circuits.html

     

    If there is ever any conflict between what I am telling you and what jc2048  is telling you your best bet is to listen to him. He is a real expert while i am just an enthusiast.

     

    John

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 5 years ago in reply to opalko

    Hi Robert,

     

    The polarized capacitors must be used in the correct polarity as they will fail if more than a token voltage is applied in the reverse direction. The polarity on the capacitor  is not like that of a diode. In the case of the polarized capacitor if you hook it up in the proper polarity it will work and if you hook it up in the incorrect polarity it will conduct  current, get hot and potentially explode provided there is enough energy available in the circuit. Generally speaking the electrolytic capacitors have higher values of capacitance for their size than do the non-polarized types. There are other differences too but probably not important to this application. The number and variety of components that can be used to make any particular circuit application is what makes electronics an art. The 555 that you are working with is a great example. There are literally hundreds of different applications that it can be applied to. Check out:

     

    http://www.talkingelectronics.com/projects/50%20-%20555%20Circuits/50%20-%20555%20Circuits.html

     

    If there is ever any conflict between what I am telling you and what jc2048  is telling you your best bet is to listen to him. He is a real expert while i am just an enthusiast.

     

    John

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer