STEM Academy
  • Learn
  • Learning Center
  • STEM Academy
  • More
  • Cancel
STEM Academy
Blog LEDs: What Types There are, How they’re Manufactured and How to Choose Which is Right for You
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join STEM Academy to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 9 Mar 2018 5:38 PM Date Created
  • Views 4507 views
  • Likes 7 likes
  • Comments 12 comments
  • learn
  • osram
  • manufacturing
  • primer
  • led
  • cabeatwell
  • learning
  • cree
  • light emitting diode
Related
Recommended

LEDs: What Types There are, How they’re Manufactured and How to Choose Which is Right for You

Catwell
Catwell
9 Mar 2018

image

Light Emitting Diodes... LEDs - we interact with them on a daily basis and can be found in or on nearly every piece of electronics or electronic devices from SBCs (Single Board Computers) to street lighting and everything in between. The technology isn’t exactly new, in fact, they’ve been around since their modern inception in 1927 by Russian inventor Oleg Losev with no practical purpose in mind. Only decades later would they find function in communications, indicators, illuminators, displays, and machine vision systems among a host of others.

 

These tiny light-emitting diodes have come a long way regarding technology and come in many different kinds, types, and shapes, all of which are manufactured in different ways and for a myriad of applications. Advancements in LED technology have led to more efficient and brighter illumination, longer service life (25,000 hours or more) and lowered power consumption over their incandescent predecessors. With all these different parameters, it may be daunting or even overwhelming when deciding which type is right for a particular application. As such, this article will attempt to provide a brief overview of all things LED- from manufacturing, types and which are best for certain applications.

 

Types and kinds of LEDs-

 

  image

Various types and sizes of LEDs. (Image credit Afrank99 via Wikimedia)

 

There are many types of LEDs current available on the market, which come in many different shapes and sizes. However they can be broken down into three separate categories- miniature, high-power and AC driven, two of which have subsequent sub-categories

 

   1: Miniature- These are the most common types that can be found and are usually single-die LEDs and range in size from 2mm to 8mm. Although there are RGB versions of in this category, they’re usually available in a single color format and are widely used for indicators on devices such as calculators, cell phones and remote controls. These types are also common on circuit boards for use as status indicators such as power flow and diagnostic applications. There are three subcategories for this type-

         A: They are often low-current and rated at 2mA at around 2V and therefore don’t require a separate heat sink to dissipate heat.

         B: The Standard version miniature LEDs are usually rated at 20mA and range in voltage depending on the color- 1.9/2.1V (red, orange, yellow and green), 3/3.4V (pure green and blue) and 2.9/4.2V (pink, violet, purple and white.

         C: The Ultra-High output versions are rated at 20mA with a voltage range of 2 to 5V and are outfitted with a suitable series resistor for a direct connection to a power supply (5-12V)

 

    2: High-Power- Advanced diode technology has given rise to this version as they offer higher illumination output over the Standard series. These can be driven at currents ranging from hundreds of mA to an ampere, with some emitting over a thousand lumens. As a result, these must be connected to a heat sink or their bright life would be cut short (think seconds). These LEDs are commonly found in vehicle headlights, flashlights and industrial applications due to their high-lumen output.

 

    3: AC Driven- These can operate on AC power without the need for a DC converter, meaning part of the LED is lit, and part of it is dark during each half-cycle, which is reversed for the other half. The benefits of this type allow it to function with a simple controlling circuit with low-power dissipation.

 

    4: Surface Mounted- SMDs are a special type of LED that feature wire leads but instead, have a pair of tiny metallic contacts that can be soldered directly onto circuit boards. These types are typically smaller than traditional LEDs, making them perfect for space-limited boards and other electronics. SMDs are also highly robust as well, able to handle shock and vibration with negligible impact on performance. These types of LEDs are often found in mobile devices, RF and low-power applications.

 

Manufacturing LEDs-

 

image

Semiconductor materials, chemical elements, and impurities are required to manufacture LEDs. (Image credit Flickr)

 

While there are many different LEDs regarding size, shape, output, and color, they are all manufactured nearly the same way with differences lying in the materials used to create them. That being said, they all begin life in the form of raw materials, such as gallium, arsenic and/or phosphor, which are all mixed together inside of an enclosed chamber and forced into a solution. The solution is heated and usually covered with a liquid layer of boron oxide to keep it from escaping and mixing with the pressurized gas in the chamber.

 

A rod is then lowered into the solution and slowly removed, after which the solution cools and crystallizes as it’s removed from the chamber forming a crystal ingot, which is then sliced into thin (approximately 10 mils thick or larger) wafers. Impurities (also known as doping, usually with zinc, silicon, germanium, nitrogen, etc.,) are introduced (grown as additional wafer layers) during this process to create density for electrons to easily flow back and forth and make the LED function correctly. The semiconductor substrate and the impurities used determine the color of the LED being produced.

 

To complete the manufacturing process, wires are then introduced to the wafer, usually in the form of gold or silver as they bond to the substrate exceedingly well, making them ready for soldering into a circuit. The LEDs are then usually coated in a transparent polymer that varies depending on the optical properties required- diffusive, transparent, tinted can all be applied depending on the LED design and application needs. Of course, this is the simple explanation of how an LED is born but for those looking for a complete in-depth production process, complete with various analysis should look the Department of Energy’s Lifecycle Assessment of LED Products report.

 

Choosing the best LED for applications-

 

  image

Choosing the right LEDs depends on the application. (Image credit Kevin Savetz via Wikimedia)

 

Choosing the right LEDs for any number of projects can be a daunting endeavor and essentially boils down to the application they are being used for. Does it need to be mounted to a circuit board, does that board have specific heat or voltage restrictions? What about power requirements, do you need constant current or constant voltage, then you will need a driver to provide variable voltage. Does the project require a single LED or a chain, how about color and lumen output?

 

Are the LEDs for industrial use, signage or displays? Perhaps your project is centered on communication and needs an IR bulb? These are just a few of the factors that will help you decide which LED is right for the application as there is no easy answer, outline or PDF that can guide you to the ideal solution from start to finish. It begins with your project goal, transitions to the requirements needed and then gives you a direction on what best to use.

 

Online help from a myriad of different companies can also help determine which is best for the application. Cree, Osram Opto Semiconductors, Everlight, and Samsung are a few leading manufacturers that have a wealth of repositories to help guide you in your search. They even offer data-rich information on the myriad of products they offer, further helping you to refine your choices. With that being said, it all boils down to your requirements and expected results, which is the first step in finding the right bulb for you.  

 

See more LEDs in the element14 store!

 

Have a story tip? Message me at: cabe(at)element14(dot)com

http://twitter.com/Cabe_Atwell

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 8 years ago +6
    I have found consumer LED lighting notoriously unreliable. I don't get anything close to the 15 years Sadly I think we'll be in this area for a while due to costs v customers expectations. When I designed…
  • shabaz
    shabaz over 8 years ago in reply to beacon_dave +5
    I think it's just hard producing something with the same form-factor as incandescent and managing the heat, as Gene mentions. At home we've got two bulb types in use predominantly, Edison E14 thread: Sylvania…
  • shabaz
    shabaz over 8 years ago in reply to beacon_dave +5
    The E14 bulbs at home are in this type of arrangement: I'm guessing this may be helping the life of them, since heat can escape more easily. It also hides the metal body. I purchased some spare E14 because…
Parents
  • shabaz
    shabaz over 8 years ago

    Interestingly Avnet pioneered some interesting ways of working with manufacturers. They realized some time ago that the creators of fixtures/luminaires were not necessarily geared up to replacing incandescent with LED, so Avnet invested heavily in the ability to provide advice, light measurements, drivers, etc., to help those designers/manufacturers develop better products. Quite a novel idea, reaching out to help designers in such a deep way in this field.

    It is covered in one of Bob Johnstone's books (he writes great books).

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 8 years ago in reply to shabaz

    So what went wrong ?!  image

     

    I have found consumer LED lighting notoriously unreliable. I don't get anything close to the 15 years (at 2.74hours per day in the small print). More like 15months if I'm really lucky.

     

    I suspect it is either down to supply voltage in the UK with lamps primarily being manufactured for Europe for a slightly lower voltage or the heat build up in lamp housings which are mainly designed for the older incandescent lamps.

     

    Has anyone investigated this I wonder. I recall that jw0752 did a post mortem on some of the CFL lamps which are also notorious for not meeting their longevity claims.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 8 years ago in reply to beacon_dave

    Hi Dave,

     

    I have only started using LED bulbs about 6 months ago. So far I have bought only cheapos from the dollar store. Half of the bulbs I have cost me $0.50 each and the rest cost me $1.00 each. All are in open air fixtures and none have failed. Needless to say I don't have very high expectations. Other people I have talked to though do indicate that the bulbs are susceptible to the heat build up in enclosed fixtures.

     

    John

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 8 years ago in reply to jw0752

    So far I have bought only cheapos from the dollar store

    In the kids room we had fixtures that took 230v MR16 type lamps, and someone brought some cheap store no brand version.

    They lasted a very short time compared with the ones I purchased from a reputable supplier for a dollar more.

     

    I couldn't recommend these unless they are for very occasional use.

     

    mark

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 8 years ago in reply to mcb1

    So far I've found the 12v MR16 type lamp LED replacements to be the worst.

     

    The first ones I tried were the 20x 5mm LED type which was great for the first few days but then the individual LEDs started flashing and dying. The dying wasn't so bad as they were overly bright anyway but the strobing effects weren't much fun. Within two weeks over half the LEDs had failed and the strobing was too much to put up with any longer.

     

    Then I tried a 3 LED type which lasted a bit longer but after about a month it would turn on and off intermittently.

     

    Finally I tried a single LED type and that died after about two months.

     

    In comparison the MR16 halogens I was trying to replace, typically lasted around 12 months.

     

     

    The best results I've so far in general are with a E14 SES type single SMD LED lamp. They however had a whopping big heatsink wrapped around them (and were expensive). One was used in an arty open frame light fitting, and the other was in an enclosed metal light fitting. Although good light output both failed within the fist year though. The enclosed one (desk lamp) was used much more heavily than the open one (bedside reading lamp) which suggests that heat build up wasn't necessarily the prime issue here. I'm currently trialling a supermarket brand 6x SMD LED type E14 SES lamp in the enclosed fitting which has lasted around 6 months so far. The quality of the light isn't so good but  usable.

     

    Ironically I've got four 60w incandescent candle wall lights which have been used every evening for the past 16 years. The main difference is that they are fed via a fade on/off dimmer switch.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 8 years ago in reply to beacon_dave

    The E14 bulbs at home are in this type of arrangement:

    image

     

    I'm guessing this may be helping the life of them, since heat can escape more easily. It also hides the metal body. I purchased some spare E14 because I too anticipated some failing, but I've not had to replace any of them in 10 months so far. I'm guessing downward spots could be a much harder challenge if they are retrofit replacements (as opposed to a purpose-built LED fixture with integrated LEDs and heat sink).

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 8 years ago in reply to beacon_dave
    So far I've found the 12v MR16 type lamp LED replacements to be the worst.

    Interesting ... I haven't bothered trying.

     

    As I said many of mine are different angles to suit the application and range from 12 deg to 60 deg.

    Most are 38 deg but many of the LED replacements have some other weird angle, and I haven't found anything close to the 12 deg ones.

     

    Mark

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mcb1
    mcb1 over 8 years ago in reply to beacon_dave
    So far I've found the 12v MR16 type lamp LED replacements to be the worst.

    Interesting ... I haven't bothered trying.

     

    As I said many of mine are different angles to suit the application and range from 12 deg to 60 deg.

    Most are 38 deg but many of the LED replacements have some other weird angle, and I haven't found anything close to the 12 deg ones.

     

    Mark

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • mcb1
    mcb1 over 8 years ago in reply to mcb1

    Just while we're discussing LED's

     

    I mentioned these in this post.What went wrong

     

    image

     

    They are a 12v replacement tailight and manufactured by Phillips (via China it seems) and have a number of individual leds (5 per side) arranged to simulate the light from an incandescent lamp.

    They seem to be much better than the others I've seen with various smd leds attached around a central core.

    Most automotive lamp holders have the reflector behind the lamp which is where these direct their light output.

     

    They do claim a certain life, but anything associated with a moving object, subjected to vibrations, knocks, temperature fluctuations and voltage ranges, has to be considered as one step away from failing.

    I suspect the strange patterns in the housing are for other variations, as they serve no useful purpose.

     

    Cheers

    Mark