STEM Academy
  • Learn
  • Learning Center
  • STEM Academy
  • More
  • Cancel
STEM Academy
Blog Simple Science Experiment with the Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join STEM Academy to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: mikedavis
  • Date Created: 2 Sep 2014 6:13 PM Date Created
  • Views 3091 views
  • Likes 1 like
  • Comments 8 comments
  • science
  • temperature
  • raspberrypi
  • probe
  • fair
  • sensor
  • stem space
Related
Recommended

Simple Science Experiment with the Raspberry Pi

mikedavis
mikedavis
2 Sep 2014

Since I got my first Raspberry Pi, I have been struggling to find a simple science experiment that I could do around the house.  I wanted to do something interesting, that used something I was familiar with.  It also had to involve temperature since that was the only probe I owned at the time.

 

I have a glass beaker mug that I got from a conference.  I don't remember the conference, but that was a highly coveted piece of swag from the exhibition floor, and I felt that I was luck to have it.  As cool as it looks, it is the worst mug I own.  Drinking coffee from that mug is like a drinking contest; it cools down so fast!  So I decided to see what coffee mug acts as the best insulator.

 

This has all of the core components of a classic science fair project.

  • Observation:  My coffee gets cold too quickly in this mug.
  • Hypothesis:  I bet other mugs might be better.
  • Experiment:  I can measure the temperature of water as it cools down over a long period of time using a temperature probe.
    • Heat 300mL of water (the beaker mug has graduation marks, so it isn't totally worthless) for 2 minutes in the microwave.
    • Pour the hot water into the mug of choice.
    • Stick in the temperature probe.
    • Watch the temperature drop as it cools down.
  • Conclusion:  None yet, but my travel mug seems to be doing the best.

 

image

I am a little surprised by this.  I thought my ceramic mugs were better than my glass mug.  According to this, there is little to no difference.

 

I also leads me to other questions:

  • Are there other better ceramic mugs in my house.
  • Will a lid help?
  • What about a travel mug without a lid?
  • What is the optimal drinking temperature - the best mug should be there the longest?

 

It took most of Labor Day to collect this data, and I did most of it while I was doing other things.  I have posted on the temperature probe before.  Again, because the RPi is a dedicated computer, I can dedicate it to watching temperatures for a long time, and do some calculations with it.

 

I wish I were young enough to enter it in the Science Fair!

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 12 years ago +1
    This is a very good experiment and a good science application of the temperature probe and the Raspberry Pi. You can't however go back and use it as a school science experiment. Fortunately, now you have…
  • shabaz
    shabaz over 12 years ago +1
    These kinds of experiments are always the most fun,since one learns a lot not just about the desired experiment itself, but also about the methods used to perform the tests, like what probes are good,…
  • michaelwylie
    michaelwylie over 12 years ago +1
    I think you should try to determine the heat transfer coefficients for each of the materials.
  • mikedavis
    mikedavis over 12 years ago in reply to jw0752

    I plan to do a styrofoam cup (with and without lid).  I also want to do a single paper (Starbucks) cup, and a pair of nested cups.  I don't know if more cups leads to better insulation, but this is a good way to find out.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 12 years ago

    These kinds of experiments are always the most fun,since one learns a lot not just about the desired experiment itself, but also about the methods used to perform the tests, like what probes are good, where and when to perform such experiments, and so on. Stuff that may be hard to learn in any other way!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 12 years ago

    This is a very good experiment and a good science application of the temperature probe and the Raspberry Pi. You can't however go back and use it as a school science experiment. Fortunately, now you have Element 14 to do the experiment for. I want to see the result for a styrofoam cup.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<